<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How do I login to my i.MX6ULL evk board? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-login-to-my-i-MX6ULL-evk-board/m-p/677958#M104583</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Hello, &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I just bought this board recently and I've compiled the kernel for the first time ever because I wanted to use Debian on my board, so I followed the instructions found here &lt;A href="https://community.nxp.com/docs/DOC-334274"&gt;Install Debian 8 Jessie Rootfs on NXP i.MX6ULL EVK board&lt;/A&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I compiled u-boot and the kernel without any problems. And I used release 17.02 instead of using the one listed in the instructions (16.04 if I'm not mistaken) because for some reason it was downloading about 10 times slower than the one I used. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I was able t do everything correctly and I can and I can see "Debian GNU/Linux 8 linaro-alip ttymxc0 " after booting everything but when it tries to autologin with root it sends an authentication failure. It tries 3 times and after that I get the following text. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"fec 2188000.ethernet eth1: Link is Up - 100Mbps/Full - flow control rx/tx&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;random: nonblocking pool is initialized"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Obviously the first is telling me that if is up (I even tried sshing into my board), but the last line is a mistery to me.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Obs: I tried the following passwords: "root",&amp;nbsp;&amp;nbsp; "linaro",&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "",&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "debian" and none of them worked.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Just in case you need it, I'll post the entire debug message I got from the serial port. But I guess that the only thing I'm missing is a password. OBS: I was getting an error when unpacking rootfs (simply said an error occurred even though the content unpacked was the same as the one in the tar ball), so I tried unpacking without the -v flag and then I noticed many errors due to not having the permissions so I chmod 777 it. That and the newer version of the rootfs are the only things I modified. I'm using mint on a VM to compile everything&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2016.03 (May 26 2017 - 09:14:55 -0300)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6ULL rev1.0 528 MHz (running at 396 MHz)&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; Commercial temperature grade (0C to 95C) at 32C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6ULL 14x14 EVK&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp; 512 MiB&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Display: TFT43AB (480x272)&lt;BR /&gt;Video: 480x272x24&lt;BR /&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Net:&amp;nbsp;&amp;nbsp; FEC1&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;reading boot.scr&lt;BR /&gt;** Unable to read file boot.scr **&lt;BR /&gt;reading zImage&lt;BR /&gt;6673232 bytes read in 301 ms (21.1 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;reading imx6ull-14x14-evk.dtb&lt;BR /&gt;35969 bytes read in 21 ms (1.6 MiB/s)&lt;BR /&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x65d350 ]&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Booting using the fdt blob at 0x83000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Using Device Tree in place at 83000000, end 8300bc80&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Booting Linux on physical CPU 0x0&lt;BR /&gt;Linux version 4.1.15 (pablo@pablo-VirtualBox) (gcc version 5.4.0 20160609 (Ubuntu/Linaro 5.4.0-6ubuntu1~16.04.4) ) #1 SMP PREEMPT Fri May 26 10:07:21 BRT 2017&lt;BR /&gt;CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d&lt;BR /&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;Machine model: Freescale i.MX6 ULL 14x14 EVK Board&lt;BR /&gt;Reserved memory: created CMA memory pool at 0x8c000000, size 320 MiB&lt;BR /&gt;Reserved memory: initialized node linux,cma, compatible id shared-dma-pool&lt;BR /&gt;Memory policy: Data cache writealloc&lt;BR /&gt;PERCPU: Embedded 12 pages/cpu @8bb32000 s16908 r8192 d24052 u49152&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 130048&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw&lt;BR /&gt;PID hash table entries: 2048 (order: 1, 8192 bytes)&lt;BR /&gt;Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;BR /&gt;Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;BR /&gt;Memory: 178564K/524288K available (8404K kernel code, 443K rwdata, 2932K rodata, 444K init, 450K bss, 18044K reserved, 327680K cma-reserved, 0K highmem)&lt;BR /&gt;Virtual kernel memory layout:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xffc00000 - 0xfff00000&amp;nbsp;&amp;nbsp; (3072 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0xa0800000 - 0xff000000&amp;nbsp;&amp;nbsp; (1512 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0x80000000 - 0xa0000000&amp;nbsp;&amp;nbsp; ( 512 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pkmap&amp;nbsp;&amp;nbsp; : 0x7fe00000 - 0x80000000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 2 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0x7f000000 - 0x7fe00000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 14 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0x80008000 - 0x80b1a434&amp;nbsp;&amp;nbsp; (11338 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0x80b1b000 - 0x80b8a000&amp;nbsp;&amp;nbsp; ( 444 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0x80b8a000 - 0x80bf8c20&amp;nbsp;&amp;nbsp; ( 444 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bss : 0x80bfb000 - 0x80c6b880&amp;nbsp;&amp;nbsp; ( 451 kB)&lt;BR /&gt;SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1&lt;BR /&gt;Preemptible hierarchical RCU implementation.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Additional per-CPU info printed with stalls.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.&lt;BR /&gt;RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1&lt;BR /&gt;NR_IRQS:16 nr_irqs:16 16&lt;BR /&gt;mxc_clocksource_init 3000000&lt;BR /&gt;Switching to timer-based delay loop, resolution 333ns&lt;BR /&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns&lt;BR /&gt;clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns&lt;BR /&gt;Console: colour dummy device 80x30&lt;BR /&gt;Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)&lt;BR /&gt;pid_max: default: 32768 minimum: 301&lt;BR /&gt;Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;BR /&gt;Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;BR /&gt;CPU: Testing write buffer coherency: ok&lt;BR /&gt;/cpus/cpu@0 missing clock-frequency property&lt;BR /&gt;CPU0: thread -1, cpu 0, socket 0, mpidr 80000000&lt;BR /&gt;Setting up static identity map for 0x80008280 - 0x800082d8&lt;BR /&gt;Brought up 1 CPUs&lt;BR /&gt;SMP: Total of 1 processors activated (6.00 BogoMIPS).&lt;BR /&gt;CPU: All CPU(s) started in SVC mode.&lt;BR /&gt;devtmpfs: initialized&lt;BR /&gt;device-tree: Duplicate name in lcdif@021c8000, renamed to "display#1"&lt;BR /&gt;VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5&lt;BR /&gt;clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns&lt;BR /&gt;pinctrl core: initialized pinctrl subsystem&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;DMA: preallocated 256 KiB pool for atomic coherent allocations&lt;BR /&gt;cpuidle: using governor ladder&lt;BR /&gt;cpuidle: using governor menu&lt;BR /&gt;hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.&lt;BR /&gt;hw-breakpoint: maximum watchpoint size is 8 bytes.&lt;BR /&gt;imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver&lt;BR /&gt;imx6ul-pinctrl 2290000.iomuxc-snvs: initialized IMX pinctrl driver&lt;BR /&gt;mxs-dma 1804000.dma-apbh: initialized&lt;BR /&gt;SCSI subsystem initialized&lt;BR /&gt;usbcore: registered new interface driver usbfs&lt;BR /&gt;usbcore: registered new interface driver hub&lt;BR /&gt;usbcore: registered new device driver usb&lt;BR /&gt;i2c i2c-0: IMX I2C adapter registered&lt;BR /&gt;i2c i2c-0: can't use DMA&lt;BR /&gt;i2c i2c-1: IMX I2C adapter registered&lt;BR /&gt;i2c i2c-1: can't use DMA&lt;BR /&gt;Linux video capture interface: v2.00&lt;BR /&gt;pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;&lt;SPAN&gt;pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:giometti@linux.it"&gt;giometti@linux.it&lt;/A&gt;&lt;SPAN&gt;&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;PTP clock support registered&lt;BR /&gt;MIPI CSI2 driver module loaded&lt;BR /&gt;Advanced Linux Sound Architecture Driver Initialized.&lt;BR /&gt;Bluetooth: Core ver 2.20&lt;BR /&gt;NET: Registered protocol family 31&lt;BR /&gt;Bluetooth: HCI device and connection manager initialized&lt;BR /&gt;Bluetooth: HCI socket layer initialized&lt;BR /&gt;Bluetooth: L2CAP socket layer initialized&lt;BR /&gt;Bluetooth: SCO socket layer initialized&lt;BR /&gt;Switched to clocksource mxc_timer1&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;TCP established hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;TCP bind hash table entries: 4096 (order: 3, 32768 bytes)&lt;BR /&gt;TCP: Hash tables configured (established 4096 bind 4096)&lt;BR /&gt;UDP hash table entries: 256 (order: 1, 8192 bytes)&lt;BR /&gt;UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;RPC: Registered named UNIX socket transport module.&lt;BR /&gt;RPC: Registered udp transport module.&lt;BR /&gt;RPC: Registered tcp transport module.&lt;BR /&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;imx rpmsg driver is registered.&lt;BR /&gt;Bus freq driver module loaded&lt;BR /&gt;futex hash table entries: 256 (order: 2, 16384 bytes)&lt;BR /&gt;VFS: Disk quotas dquot_6.6.0&lt;BR /&gt;VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)&lt;BR /&gt;NFS: Registering the id_resolver key type&lt;BR /&gt;Key type id_resolver registered&lt;BR /&gt;Key type id_legacy registered&lt;BR /&gt;jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;BR /&gt;fuse init (API version 7.23)&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered (default)&lt;BR /&gt;imx-weim 21b8000.weim: Driver registered.&lt;BR /&gt;backlight supply power not found, using dummy regulator&lt;BR /&gt;MIPI DSI driver module loaded&lt;BR /&gt;MIPI DSI driver module loaded&lt;BR /&gt;21c8000.lcdif supply lcd not found, using dummy regulator&lt;BR /&gt;mxsfb 21c8000.lcdif: failed to find mxc display driver&lt;BR /&gt;Console: switching to colour frame buffer device 60x34&lt;BR /&gt;mxsfb 21c8000.lcdif: initialized&lt;BR /&gt;imx-sdma 20ec000.sdma: no event needs to be remapped&lt;BR /&gt;imx-sdma 20ec000.sdma: loaded firmware 3.3&lt;BR /&gt;imx-sdma 20ec000.sdma: initialized&lt;BR /&gt;2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 18, base_baud = 5000000) is a IMX&lt;BR /&gt;console [ttymxc0] enabled&lt;BR /&gt;21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 235, base_baud = 5000000) is a IMX&lt;BR /&gt;imx-rng 2284000.rngb: iMX RNG Registered.&lt;BR /&gt;imx sema4 driver is registered.&lt;BR /&gt;[drm] Initialized drm 1.1.0 20060810&lt;BR /&gt;[drm] Initialized vivante 1.0.0 20120216 on minor 0&lt;BR /&gt;brd: module loaded&lt;BR /&gt;loop: module loaded&lt;BR /&gt;fsl-quadspi 21e0000.qspi: n25q256a (32768 Kbytes)&lt;BR /&gt;spi_gpio spi4: gpio-miso property not found, switching to no-rx mode&lt;BR /&gt;CAN device driver interface&lt;BR /&gt;flexcan 2090000.can: device registered (reg_base=a09f8000, irq=27)&lt;BR /&gt;flexcan 2094000.can: device registered (reg_base=a0a00000, irq=28)&lt;BR /&gt;20b4000.ethernet supply phy not found, using dummy regulator&lt;BR /&gt;pps pps0: new PPS source ptp0&lt;BR /&gt;libphy: fec_enet_mii_bus: probed&lt;BR /&gt;fec 20b4000.ethernet eth0: registered PHC device 0&lt;BR /&gt;2188000.ethernet supply phy not found, using dummy regulator&lt;BR /&gt;pps pps1: new PPS source ptp1&lt;BR /&gt;fec 2188000.ethernet eth1: registered PHC device 1&lt;BR /&gt;usbcore: registered new interface driver asix&lt;BR /&gt;usbcore: registered new interface driver ax88179_178a&lt;BR /&gt;usbcore: registered new interface driver cdc_ether&lt;BR /&gt;usbcore: registered new interface driver net1080&lt;BR /&gt;usbcore: registered new interface driver cdc_subset&lt;BR /&gt;usbcore: registered new interface driver zaurus&lt;BR /&gt;usbcore: registered new interface driver cdc_ncm&lt;BR /&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;BR /&gt;ehci-mxc: Freescale On-Chip EHCI Host driver&lt;BR /&gt;usbcore: registered new interface driver usb-storage&lt;BR /&gt;usbcore: registered new interface driver usb_ehset_test&lt;BR /&gt;2184800.usbmisc supply vbus-wakeup not found, using dummy regulator&lt;BR /&gt;2184000.usb supply vbus not found, using dummy regulator&lt;BR /&gt;2184200.usb supply vbus not found, using dummy regulator&lt;BR /&gt;ci_hdrc ci_hdrc.1: EHCI Host Controller&lt;BR /&gt;ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1&lt;BR /&gt;ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00&lt;BR /&gt;hub 1-0:1.0: USB hub found&lt;BR /&gt;hub 1-0:1.0: 1 port detected&lt;BR /&gt;mousedev: PS/2 mouse device common for all mice&lt;BR /&gt;input: 20cc000.snvs:snvs-powerkey as /devices/platform/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0&lt;BR /&gt;input: iMX6UL TouchScreen Controller as /devices/platform/soc/2000000.aips-bus/2040000.tsc/input/input1&lt;BR /&gt;input: FreescaleAccelerometer as /devices/virtual/input/input2&lt;BR /&gt;fxls8471 device driver probe successfully&lt;BR /&gt;snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;IR NEC protocol handler initialized&lt;BR /&gt;IR RC5(x/sz) protocol handler initialized&lt;BR /&gt;IR RC6 protocol handler initialized&lt;BR /&gt;IR JVC protocol handler initialized&lt;BR /&gt;IR Sony protocol handler initialized&lt;BR /&gt;IR SANYO protocol handler initialized&lt;BR /&gt;IR Sharp protocol handler initialized&lt;BR /&gt;IR MCE Keyboard/mouse protocol handler initialized&lt;BR /&gt;IR XMP protocol handler initialized&lt;BR /&gt;pxp-v4l2 pxp_v4l2: initialized&lt;BR /&gt;0-000e supply vdd not found, using dummy regulator&lt;BR /&gt;0-000e supply vddio not found, using dummy regulator&lt;BR /&gt;mag3110 0-000e: check mag3110 chip ID&lt;BR /&gt;input: mag3110 as /devices/virtual/input/input3&lt;BR /&gt;mag3110 0-000e: mag3110 is probed&lt;BR /&gt;imx2-wdt 20bc000.wdog: use WDOG_B to reboot.&lt;BR /&gt;imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)&lt;BR /&gt;Bluetooth: HCI UART driver ver 2.3&lt;BR /&gt;Bluetooth: HCI UART protocol H4 registered&lt;BR /&gt;Bluetooth: HCI UART protocol BCSP registered&lt;BR /&gt;Bluetooth: HCI UART protocol ATH3K registered&lt;BR /&gt;usbcore: registered new interface driver bcm203x&lt;BR /&gt;usbcore: registered new interface driver btusb&lt;BR /&gt;usbcore: registered new interface driver ath3k&lt;BR /&gt;sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified&lt;BR /&gt;sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO&lt;BR /&gt;sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found&lt;BR /&gt;mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA&lt;BR /&gt;/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on normal mode&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found&lt;BR /&gt;mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA&lt;BR /&gt;usbcore: registered new interface driver usbhid&lt;BR /&gt;usbhid: USB HID core driver&lt;BR /&gt;fsl-asrc 2034000.asrc: driver registered&lt;BR /&gt;mmc1: host does not support reading read-only switch, assuming write-enable&lt;BR /&gt;imx-wm8960 sound: wm8960-hifi &amp;lt;-&amp;gt; 202c000.sai mapping ok&lt;BR /&gt;mmc1: new high speed SDHC card at address 0001&lt;BR /&gt;imx-wm8960 sound: snd-soc-dummy-dai &amp;lt;-&amp;gt; 2034000.asrc mapping ok&lt;BR /&gt;mmcblk1: mmc1:0001 SD8GB 7.24 GiB&lt;BR /&gt;imx-wm8960 sound: wm8960-hifi &amp;lt;-&amp;gt; 202c000.sai mapping ok&lt;BR /&gt;&amp;nbsp;mmcblk1: p1 p2&lt;BR /&gt;NET: Registered protocol family 26&lt;BR /&gt;NET: Registered protocol family 10&lt;BR /&gt;sit: IPv6 over IPv4 tunneling driver&lt;BR /&gt;NET: Registered protocol family 17&lt;BR /&gt;can: controller area network core (rev 20120528 abi 9)&lt;BR /&gt;NET: Registered protocol family 29&lt;BR /&gt;can: raw protocol (rev 20120528)&lt;BR /&gt;can: broadcast manager protocol (rev 20120528 t)&lt;BR /&gt;can: netlink gateway (rev 20130117) max_hops=1&lt;BR /&gt;Bluetooth: RFCOMM TTY layer initialized&lt;BR /&gt;Bluetooth: RFCOMM socket layer initialized&lt;BR /&gt;Bluetooth: RFCOMM ver 1.11&lt;BR /&gt;Bluetooth: BNEP (Ethernet Emulation) ver 1.3&lt;BR /&gt;Bluetooth: BNEP filters: protocol multicast&lt;BR /&gt;Bluetooth: BNEP socket layer initialized&lt;BR /&gt;Bluetooth: HIDP (Human Interface Emulation) ver 1.2&lt;BR /&gt;Bluetooth: HIDP socket layer initialized&lt;BR /&gt;8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;Key type dns_resolver registered&lt;BR /&gt;dhd_module_init in&lt;BR /&gt;snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:15:16 UTC (916)&lt;BR /&gt;gpio_dvfs: disabling&lt;BR /&gt;VSD_3V3: disabling&lt;BR /&gt;can-3v3: disabling&lt;BR /&gt;ALSA device list:&lt;BR /&gt;&amp;nbsp; #0: wm8960-audio&lt;BR /&gt;kjournald starting.&amp;nbsp; Commit interval 5 seconds&lt;BR /&gt;EXT3-fs (mmcblk1p2): using internal journal&lt;BR /&gt;EXT3-fs (mmcblk1p2): recovery complete&lt;BR /&gt;EXT3-fs (mmcblk1p2): mounted filesystem with ordered data mode&lt;BR /&gt;VFS: Mounted root (ext3 filesystem) on device 179:2.&lt;BR /&gt;devtmpfs: mounted&lt;BR /&gt;Freeing unused kernel memory: 444K (80b1b000 - 80b8a000)&lt;BR /&gt;systemd[1]: Failed to insert module 'kdbus': Function not implemented&lt;BR /&gt;random: systemd urandom read with 23 bits of entropy available&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Welcome to Debian GNU/Linux 8 (jessie)!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[&amp;nbsp; OK&amp;nbsp; ] Created slice User and Session Slice.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on Journal Socket (/dev/log).&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on /dev/initctl Compatibility Named Pipe.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Forward Password Requests to Wall Directory Watch.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Created slice System Slice.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Created slice system-serial\x2dgetty.slice.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Encrypted Volumes.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on udev Kernel Socket.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Slices.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Set up automount Arbitrary Executab...ats File System Automount Point.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on udev Control Socket.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Swap.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on Journal Socket.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Load Kernel Modules...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Create Static Device Nodes in /dev...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mounting Debug File System...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Nameserver information manager...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Created slice system-getty.slice.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on Syslog Socket.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Journal Service...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Remote File Systems (Pre).&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Remote File Systems.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: Prepare console...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Load Kernel Modules.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Apply Kernel Variables...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mounting FUSE Control File System...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Mounted Debug File System.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Create Static Device Nodes in /dev.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Apply Kernel Variables.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Mounted FUSE Control File System.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Nameserver information manager.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Journal Service.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: Prepare console.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: Set console font and keymap...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting udev Kernel Device Manager...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started udev Kernel Device Manager.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: Set preliminary keymap...&lt;BR /&gt;cfg80211: World regulatory domain updated:&lt;BR /&gt;cfg80211:&amp;nbsp; DFS Master region: unset&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (2402000 KHz - 2472000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (2457000 KHz - 2482000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (2474000 KHz - 2494000 KHz @ 20000 KHz), (N/A, 2000 mBm), (N/A)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (5170000 KHz - 5250000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (N/A)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (5250000 KHz - 5330000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (0 s)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (5490000 KHz - 5730000 KHz @ 160000 KHz), (N/A, 2000 mBm), (0 s)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (5735000 KHz - 5835000 KHz @ 80000 KHz), (N/A, 2000 mBm), (N/A)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (57240000 KHz - 63720000 KHz @ 2160000 KHz), (N/A, 0 mBm), (N/A)&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: Set preliminary keymap.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: Set console font and keymap.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Remount Root and Kernel File Systems...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Remount Root and Kernel File Systems.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Flush Journal to Persistent Storage...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting udev Coldplug all Devices...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Local File Systems (Pre).&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Local File Systems.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Tell Plymouth To Write Out Runtime Data...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Load/Save Random Seed...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Tell Plymouth To Write Out Runtime Data.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Load/Save Random Seed.&lt;BR /&gt;systemd-journald[107]: Received request to flush runtime journal from PID 1&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Flush Journal to Persistent Storage.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Create Volatile Files and Directories...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: Raise network interfaces....&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Create Volatile Files and Directories.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Network Time Synchronization...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Update UTMP about System Boot/Shutdown...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Network Time Synchronization.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Update UTMP about System Boot/Shutdown.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target System Time Synchronized.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: Raise network interfaces..&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started udev Coldplug all Devices.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Found device /dev/ttymxc0.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Dispatch Password Requests to Console Directory Watch.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Created slice system-systemd\x2dbacklight.slice.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Load/Save Screen Backlight...htness of backlight:backlight...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Network.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Network is Online.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Load/Save Screen Backlight Brightness of backlight:backlight.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target System Initialization.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Daily Cleanup of Temporary Directories.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Timers.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on D-Bus System Message Bus Socket.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on ACPID Listen Socket.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Sockets.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Trigger resolvconf update for networkd DNS.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started ACPI Events Check.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Paths.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Basic System.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started D-Bus System Message Bus.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Network Manager...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Initialize hardware monitoring sensors...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Login Service...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started OpenBSD Secure Shell server.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: Advanced IEEE 802.11 management daemon...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting System Logging Service...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Run anacron jobs.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting /etc/rc.local Compatibility...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: Load kernel modules needed to enable cpufreq scaling...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started ACPI event daemon.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: network benchmark...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Permit User Sessions...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: Advanced IEEE 802.11 management daemon.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started /etc/rc.local Compatibility.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Permit User Sessions.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started System Logging Service.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: network benchmark.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Initialize hardware monitoring sensors.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: Load kernel modules needed to enable cpufreq scaling.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Login Service.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Authenticate and Authorize Users to Run Privileged Tasks...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Sound Card.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: set CPUFreq kernel parameters...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Light Display Manager...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Terminate Plymouth Boot Screen...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Wait for Plymouth Boot Screen to Quit...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Terminate Plymouth Boot Screen.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Wait for Plymouth Boot Screen to Quit.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: set CPUFreq kernel parameters.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Authenticate and Authorize Users to Run Privileged Tasks.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Light Display Manager.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Network Manager.&lt;BR /&gt;fec 20b4000.ethernet eth0: Freescale FEC PHY driver [Micrel KSZ8081 or KSZ8091] (mii_bus:phy_addr=20b4000.ethernet:01, irq=-1)&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Getty on tty1.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Serial Getty on ttymxc0.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Login Prompts.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Multi-User System.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Graphical Interface.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Update UTMP about System Runlevel Changes...&lt;BR /&gt;fec 2188000.ethernet eth1: Freescale FEC PHY driver [Micrel KSZ8081 or KSZ8091] (mii_bus:phy_addr=20b4000.ethernet:02, irq=-1)&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Update UTMP about System Runlevel Changes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debian GNU/Linux 8 linaro-alip ttymxc0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linaro-alip login: root (automatic login)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Authentication failure&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debian GNU/Linux 8 linaro-alip ttymxc0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linaro-alip login: root (automatic login)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Authentication failure&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debian GNU/Linux 8 linaro-alip ttymxc0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linaro-alip login: root (automatic login)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Authentication failure&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debian GNU/Linux 8 linaro-alip ttymxc0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linaro-alip login: root (automatic login)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Authentication failure&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debian GNU/Linux 8 linaro-alip ttymxc0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linaro-alip login: root (automatic login)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Authentication failure&lt;BR /&gt;fec 2188000.ethernet eth1: Link is Up - 100Mbps/Full - flow control rx/tx&lt;BR /&gt;random: nonblocking pool is initialized&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Jun 2017 01:39:19 GMT</pubDate>
    <dc:creator>pablocottens</dc:creator>
    <dc:date>2017-06-07T01:39:19Z</dc:date>
    <item>
      <title>How do I login to my i.MX6ULL evk board?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-login-to-my-i-MX6ULL-evk-board/m-p/677958#M104583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Hello, &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I just bought this board recently and I've compiled the kernel for the first time ever because I wanted to use Debian on my board, so I followed the instructions found here &lt;A href="https://community.nxp.com/docs/DOC-334274"&gt;Install Debian 8 Jessie Rootfs on NXP i.MX6ULL EVK board&lt;/A&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I compiled u-boot and the kernel without any problems. And I used release 17.02 instead of using the one listed in the instructions (16.04 if I'm not mistaken) because for some reason it was downloading about 10 times slower than the one I used. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I was able t do everything correctly and I can and I can see "Debian GNU/Linux 8 linaro-alip ttymxc0 " after booting everything but when it tries to autologin with root it sends an authentication failure. It tries 3 times and after that I get the following text. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"fec 2188000.ethernet eth1: Link is Up - 100Mbps/Full - flow control rx/tx&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;random: nonblocking pool is initialized"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Obviously the first is telling me that if is up (I even tried sshing into my board), but the last line is a mistery to me.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Obs: I tried the following passwords: "root",&amp;nbsp;&amp;nbsp; "linaro",&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "",&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "debian" and none of them worked.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Just in case you need it, I'll post the entire debug message I got from the serial port. But I guess that the only thing I'm missing is a password. OBS: I was getting an error when unpacking rootfs (simply said an error occurred even though the content unpacked was the same as the one in the tar ball), so I tried unpacking without the -v flag and then I noticed many errors due to not having the permissions so I chmod 777 it. That and the newer version of the rootfs are the only things I modified. I'm using mint on a VM to compile everything&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2016.03 (May 26 2017 - 09:14:55 -0300)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6ULL rev1.0 528 MHz (running at 396 MHz)&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; Commercial temperature grade (0C to 95C) at 32C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6ULL 14x14 EVK&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp; 512 MiB&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Display: TFT43AB (480x272)&lt;BR /&gt;Video: 480x272x24&lt;BR /&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Net:&amp;nbsp;&amp;nbsp; FEC1&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;reading boot.scr&lt;BR /&gt;** Unable to read file boot.scr **&lt;BR /&gt;reading zImage&lt;BR /&gt;6673232 bytes read in 301 ms (21.1 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;reading imx6ull-14x14-evk.dtb&lt;BR /&gt;35969 bytes read in 21 ms (1.6 MiB/s)&lt;BR /&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x65d350 ]&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Booting using the fdt blob at 0x83000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Using Device Tree in place at 83000000, end 8300bc80&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Booting Linux on physical CPU 0x0&lt;BR /&gt;Linux version 4.1.15 (pablo@pablo-VirtualBox) (gcc version 5.4.0 20160609 (Ubuntu/Linaro 5.4.0-6ubuntu1~16.04.4) ) #1 SMP PREEMPT Fri May 26 10:07:21 BRT 2017&lt;BR /&gt;CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d&lt;BR /&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;Machine model: Freescale i.MX6 ULL 14x14 EVK Board&lt;BR /&gt;Reserved memory: created CMA memory pool at 0x8c000000, size 320 MiB&lt;BR /&gt;Reserved memory: initialized node linux,cma, compatible id shared-dma-pool&lt;BR /&gt;Memory policy: Data cache writealloc&lt;BR /&gt;PERCPU: Embedded 12 pages/cpu @8bb32000 s16908 r8192 d24052 u49152&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 130048&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw&lt;BR /&gt;PID hash table entries: 2048 (order: 1, 8192 bytes)&lt;BR /&gt;Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;BR /&gt;Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;BR /&gt;Memory: 178564K/524288K available (8404K kernel code, 443K rwdata, 2932K rodata, 444K init, 450K bss, 18044K reserved, 327680K cma-reserved, 0K highmem)&lt;BR /&gt;Virtual kernel memory layout:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xffc00000 - 0xfff00000&amp;nbsp;&amp;nbsp; (3072 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0xa0800000 - 0xff000000&amp;nbsp;&amp;nbsp; (1512 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0x80000000 - 0xa0000000&amp;nbsp;&amp;nbsp; ( 512 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pkmap&amp;nbsp;&amp;nbsp; : 0x7fe00000 - 0x80000000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 2 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0x7f000000 - 0x7fe00000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 14 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0x80008000 - 0x80b1a434&amp;nbsp;&amp;nbsp; (11338 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0x80b1b000 - 0x80b8a000&amp;nbsp;&amp;nbsp; ( 444 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0x80b8a000 - 0x80bf8c20&amp;nbsp;&amp;nbsp; ( 444 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bss : 0x80bfb000 - 0x80c6b880&amp;nbsp;&amp;nbsp; ( 451 kB)&lt;BR /&gt;SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1&lt;BR /&gt;Preemptible hierarchical RCU implementation.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Additional per-CPU info printed with stalls.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.&lt;BR /&gt;RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1&lt;BR /&gt;NR_IRQS:16 nr_irqs:16 16&lt;BR /&gt;mxc_clocksource_init 3000000&lt;BR /&gt;Switching to timer-based delay loop, resolution 333ns&lt;BR /&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns&lt;BR /&gt;clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns&lt;BR /&gt;Console: colour dummy device 80x30&lt;BR /&gt;Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)&lt;BR /&gt;pid_max: default: 32768 minimum: 301&lt;BR /&gt;Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;BR /&gt;Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;BR /&gt;CPU: Testing write buffer coherency: ok&lt;BR /&gt;/cpus/cpu@0 missing clock-frequency property&lt;BR /&gt;CPU0: thread -1, cpu 0, socket 0, mpidr 80000000&lt;BR /&gt;Setting up static identity map for 0x80008280 - 0x800082d8&lt;BR /&gt;Brought up 1 CPUs&lt;BR /&gt;SMP: Total of 1 processors activated (6.00 BogoMIPS).&lt;BR /&gt;CPU: All CPU(s) started in SVC mode.&lt;BR /&gt;devtmpfs: initialized&lt;BR /&gt;device-tree: Duplicate name in lcdif@021c8000, renamed to "display#1"&lt;BR /&gt;VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5&lt;BR /&gt;clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns&lt;BR /&gt;pinctrl core: initialized pinctrl subsystem&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;DMA: preallocated 256 KiB pool for atomic coherent allocations&lt;BR /&gt;cpuidle: using governor ladder&lt;BR /&gt;cpuidle: using governor menu&lt;BR /&gt;hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.&lt;BR /&gt;hw-breakpoint: maximum watchpoint size is 8 bytes.&lt;BR /&gt;imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver&lt;BR /&gt;imx6ul-pinctrl 2290000.iomuxc-snvs: initialized IMX pinctrl driver&lt;BR /&gt;mxs-dma 1804000.dma-apbh: initialized&lt;BR /&gt;SCSI subsystem initialized&lt;BR /&gt;usbcore: registered new interface driver usbfs&lt;BR /&gt;usbcore: registered new interface driver hub&lt;BR /&gt;usbcore: registered new device driver usb&lt;BR /&gt;i2c i2c-0: IMX I2C adapter registered&lt;BR /&gt;i2c i2c-0: can't use DMA&lt;BR /&gt;i2c i2c-1: IMX I2C adapter registered&lt;BR /&gt;i2c i2c-1: can't use DMA&lt;BR /&gt;Linux video capture interface: v2.00&lt;BR /&gt;pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;&lt;SPAN&gt;pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:giometti@linux.it"&gt;giometti@linux.it&lt;/A&gt;&lt;SPAN&gt;&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;PTP clock support registered&lt;BR /&gt;MIPI CSI2 driver module loaded&lt;BR /&gt;Advanced Linux Sound Architecture Driver Initialized.&lt;BR /&gt;Bluetooth: Core ver 2.20&lt;BR /&gt;NET: Registered protocol family 31&lt;BR /&gt;Bluetooth: HCI device and connection manager initialized&lt;BR /&gt;Bluetooth: HCI socket layer initialized&lt;BR /&gt;Bluetooth: L2CAP socket layer initialized&lt;BR /&gt;Bluetooth: SCO socket layer initialized&lt;BR /&gt;Switched to clocksource mxc_timer1&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;TCP established hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;TCP bind hash table entries: 4096 (order: 3, 32768 bytes)&lt;BR /&gt;TCP: Hash tables configured (established 4096 bind 4096)&lt;BR /&gt;UDP hash table entries: 256 (order: 1, 8192 bytes)&lt;BR /&gt;UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;RPC: Registered named UNIX socket transport module.&lt;BR /&gt;RPC: Registered udp transport module.&lt;BR /&gt;RPC: Registered tcp transport module.&lt;BR /&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;imx rpmsg driver is registered.&lt;BR /&gt;Bus freq driver module loaded&lt;BR /&gt;futex hash table entries: 256 (order: 2, 16384 bytes)&lt;BR /&gt;VFS: Disk quotas dquot_6.6.0&lt;BR /&gt;VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)&lt;BR /&gt;NFS: Registering the id_resolver key type&lt;BR /&gt;Key type id_resolver registered&lt;BR /&gt;Key type id_legacy registered&lt;BR /&gt;jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;BR /&gt;fuse init (API version 7.23)&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered (default)&lt;BR /&gt;imx-weim 21b8000.weim: Driver registered.&lt;BR /&gt;backlight supply power not found, using dummy regulator&lt;BR /&gt;MIPI DSI driver module loaded&lt;BR /&gt;MIPI DSI driver module loaded&lt;BR /&gt;21c8000.lcdif supply lcd not found, using dummy regulator&lt;BR /&gt;mxsfb 21c8000.lcdif: failed to find mxc display driver&lt;BR /&gt;Console: switching to colour frame buffer device 60x34&lt;BR /&gt;mxsfb 21c8000.lcdif: initialized&lt;BR /&gt;imx-sdma 20ec000.sdma: no event needs to be remapped&lt;BR /&gt;imx-sdma 20ec000.sdma: loaded firmware 3.3&lt;BR /&gt;imx-sdma 20ec000.sdma: initialized&lt;BR /&gt;2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 18, base_baud = 5000000) is a IMX&lt;BR /&gt;console [ttymxc0] enabled&lt;BR /&gt;21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 235, base_baud = 5000000) is a IMX&lt;BR /&gt;imx-rng 2284000.rngb: iMX RNG Registered.&lt;BR /&gt;imx sema4 driver is registered.&lt;BR /&gt;[drm] Initialized drm 1.1.0 20060810&lt;BR /&gt;[drm] Initialized vivante 1.0.0 20120216 on minor 0&lt;BR /&gt;brd: module loaded&lt;BR /&gt;loop: module loaded&lt;BR /&gt;fsl-quadspi 21e0000.qspi: n25q256a (32768 Kbytes)&lt;BR /&gt;spi_gpio spi4: gpio-miso property not found, switching to no-rx mode&lt;BR /&gt;CAN device driver interface&lt;BR /&gt;flexcan 2090000.can: device registered (reg_base=a09f8000, irq=27)&lt;BR /&gt;flexcan 2094000.can: device registered (reg_base=a0a00000, irq=28)&lt;BR /&gt;20b4000.ethernet supply phy not found, using dummy regulator&lt;BR /&gt;pps pps0: new PPS source ptp0&lt;BR /&gt;libphy: fec_enet_mii_bus: probed&lt;BR /&gt;fec 20b4000.ethernet eth0: registered PHC device 0&lt;BR /&gt;2188000.ethernet supply phy not found, using dummy regulator&lt;BR /&gt;pps pps1: new PPS source ptp1&lt;BR /&gt;fec 2188000.ethernet eth1: registered PHC device 1&lt;BR /&gt;usbcore: registered new interface driver asix&lt;BR /&gt;usbcore: registered new interface driver ax88179_178a&lt;BR /&gt;usbcore: registered new interface driver cdc_ether&lt;BR /&gt;usbcore: registered new interface driver net1080&lt;BR /&gt;usbcore: registered new interface driver cdc_subset&lt;BR /&gt;usbcore: registered new interface driver zaurus&lt;BR /&gt;usbcore: registered new interface driver cdc_ncm&lt;BR /&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;BR /&gt;ehci-mxc: Freescale On-Chip EHCI Host driver&lt;BR /&gt;usbcore: registered new interface driver usb-storage&lt;BR /&gt;usbcore: registered new interface driver usb_ehset_test&lt;BR /&gt;2184800.usbmisc supply vbus-wakeup not found, using dummy regulator&lt;BR /&gt;2184000.usb supply vbus not found, using dummy regulator&lt;BR /&gt;2184200.usb supply vbus not found, using dummy regulator&lt;BR /&gt;ci_hdrc ci_hdrc.1: EHCI Host Controller&lt;BR /&gt;ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1&lt;BR /&gt;ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00&lt;BR /&gt;hub 1-0:1.0: USB hub found&lt;BR /&gt;hub 1-0:1.0: 1 port detected&lt;BR /&gt;mousedev: PS/2 mouse device common for all mice&lt;BR /&gt;input: 20cc000.snvs:snvs-powerkey as /devices/platform/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0&lt;BR /&gt;input: iMX6UL TouchScreen Controller as /devices/platform/soc/2000000.aips-bus/2040000.tsc/input/input1&lt;BR /&gt;input: FreescaleAccelerometer as /devices/virtual/input/input2&lt;BR /&gt;fxls8471 device driver probe successfully&lt;BR /&gt;snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;IR NEC protocol handler initialized&lt;BR /&gt;IR RC5(x/sz) protocol handler initialized&lt;BR /&gt;IR RC6 protocol handler initialized&lt;BR /&gt;IR JVC protocol handler initialized&lt;BR /&gt;IR Sony protocol handler initialized&lt;BR /&gt;IR SANYO protocol handler initialized&lt;BR /&gt;IR Sharp protocol handler initialized&lt;BR /&gt;IR MCE Keyboard/mouse protocol handler initialized&lt;BR /&gt;IR XMP protocol handler initialized&lt;BR /&gt;pxp-v4l2 pxp_v4l2: initialized&lt;BR /&gt;0-000e supply vdd not found, using dummy regulator&lt;BR /&gt;0-000e supply vddio not found, using dummy regulator&lt;BR /&gt;mag3110 0-000e: check mag3110 chip ID&lt;BR /&gt;input: mag3110 as /devices/virtual/input/input3&lt;BR /&gt;mag3110 0-000e: mag3110 is probed&lt;BR /&gt;imx2-wdt 20bc000.wdog: use WDOG_B to reboot.&lt;BR /&gt;imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)&lt;BR /&gt;Bluetooth: HCI UART driver ver 2.3&lt;BR /&gt;Bluetooth: HCI UART protocol H4 registered&lt;BR /&gt;Bluetooth: HCI UART protocol BCSP registered&lt;BR /&gt;Bluetooth: HCI UART protocol ATH3K registered&lt;BR /&gt;usbcore: registered new interface driver bcm203x&lt;BR /&gt;usbcore: registered new interface driver btusb&lt;BR /&gt;usbcore: registered new interface driver ath3k&lt;BR /&gt;sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified&lt;BR /&gt;sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO&lt;BR /&gt;sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found&lt;BR /&gt;mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA&lt;BR /&gt;/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on normal mode&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found&lt;BR /&gt;mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA&lt;BR /&gt;usbcore: registered new interface driver usbhid&lt;BR /&gt;usbhid: USB HID core driver&lt;BR /&gt;fsl-asrc 2034000.asrc: driver registered&lt;BR /&gt;mmc1: host does not support reading read-only switch, assuming write-enable&lt;BR /&gt;imx-wm8960 sound: wm8960-hifi &amp;lt;-&amp;gt; 202c000.sai mapping ok&lt;BR /&gt;mmc1: new high speed SDHC card at address 0001&lt;BR /&gt;imx-wm8960 sound: snd-soc-dummy-dai &amp;lt;-&amp;gt; 2034000.asrc mapping ok&lt;BR /&gt;mmcblk1: mmc1:0001 SD8GB 7.24 GiB&lt;BR /&gt;imx-wm8960 sound: wm8960-hifi &amp;lt;-&amp;gt; 202c000.sai mapping ok&lt;BR /&gt;&amp;nbsp;mmcblk1: p1 p2&lt;BR /&gt;NET: Registered protocol family 26&lt;BR /&gt;NET: Registered protocol family 10&lt;BR /&gt;sit: IPv6 over IPv4 tunneling driver&lt;BR /&gt;NET: Registered protocol family 17&lt;BR /&gt;can: controller area network core (rev 20120528 abi 9)&lt;BR /&gt;NET: Registered protocol family 29&lt;BR /&gt;can: raw protocol (rev 20120528)&lt;BR /&gt;can: broadcast manager protocol (rev 20120528 t)&lt;BR /&gt;can: netlink gateway (rev 20130117) max_hops=1&lt;BR /&gt;Bluetooth: RFCOMM TTY layer initialized&lt;BR /&gt;Bluetooth: RFCOMM socket layer initialized&lt;BR /&gt;Bluetooth: RFCOMM ver 1.11&lt;BR /&gt;Bluetooth: BNEP (Ethernet Emulation) ver 1.3&lt;BR /&gt;Bluetooth: BNEP filters: protocol multicast&lt;BR /&gt;Bluetooth: BNEP socket layer initialized&lt;BR /&gt;Bluetooth: HIDP (Human Interface Emulation) ver 1.2&lt;BR /&gt;Bluetooth: HIDP socket layer initialized&lt;BR /&gt;8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;Key type dns_resolver registered&lt;BR /&gt;dhd_module_init in&lt;BR /&gt;snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:15:16 UTC (916)&lt;BR /&gt;gpio_dvfs: disabling&lt;BR /&gt;VSD_3V3: disabling&lt;BR /&gt;can-3v3: disabling&lt;BR /&gt;ALSA device list:&lt;BR /&gt;&amp;nbsp; #0: wm8960-audio&lt;BR /&gt;kjournald starting.&amp;nbsp; Commit interval 5 seconds&lt;BR /&gt;EXT3-fs (mmcblk1p2): using internal journal&lt;BR /&gt;EXT3-fs (mmcblk1p2): recovery complete&lt;BR /&gt;EXT3-fs (mmcblk1p2): mounted filesystem with ordered data mode&lt;BR /&gt;VFS: Mounted root (ext3 filesystem) on device 179:2.&lt;BR /&gt;devtmpfs: mounted&lt;BR /&gt;Freeing unused kernel memory: 444K (80b1b000 - 80b8a000)&lt;BR /&gt;systemd[1]: Failed to insert module 'kdbus': Function not implemented&lt;BR /&gt;random: systemd urandom read with 23 bits of entropy available&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Welcome to Debian GNU/Linux 8 (jessie)!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[&amp;nbsp; OK&amp;nbsp; ] Created slice User and Session Slice.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on Journal Socket (/dev/log).&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on /dev/initctl Compatibility Named Pipe.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Forward Password Requests to Wall Directory Watch.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Created slice System Slice.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Created slice system-serial\x2dgetty.slice.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Encrypted Volumes.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on udev Kernel Socket.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Slices.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Set up automount Arbitrary Executab...ats File System Automount Point.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on udev Control Socket.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Swap.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on Journal Socket.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Load Kernel Modules...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Create Static Device Nodes in /dev...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mounting Debug File System...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Nameserver information manager...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Created slice system-getty.slice.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on Syslog Socket.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Journal Service...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Remote File Systems (Pre).&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Remote File Systems.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: Prepare console...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Load Kernel Modules.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Apply Kernel Variables...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mounting FUSE Control File System...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Mounted Debug File System.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Create Static Device Nodes in /dev.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Apply Kernel Variables.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Mounted FUSE Control File System.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Nameserver information manager.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Journal Service.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: Prepare console.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: Set console font and keymap...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting udev Kernel Device Manager...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started udev Kernel Device Manager.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: Set preliminary keymap...&lt;BR /&gt;cfg80211: World regulatory domain updated:&lt;BR /&gt;cfg80211:&amp;nbsp; DFS Master region: unset&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (2402000 KHz - 2472000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (2457000 KHz - 2482000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (2474000 KHz - 2494000 KHz @ 20000 KHz), (N/A, 2000 mBm), (N/A)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (5170000 KHz - 5250000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (N/A)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (5250000 KHz - 5330000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (0 s)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (5490000 KHz - 5730000 KHz @ 160000 KHz), (N/A, 2000 mBm), (0 s)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (5735000 KHz - 5835000 KHz @ 80000 KHz), (N/A, 2000 mBm), (N/A)&lt;BR /&gt;cfg80211:&amp;nbsp;&amp;nbsp; (57240000 KHz - 63720000 KHz @ 2160000 KHz), (N/A, 0 mBm), (N/A)&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: Set preliminary keymap.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: Set console font and keymap.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Remount Root and Kernel File Systems...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Remount Root and Kernel File Systems.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Flush Journal to Persistent Storage...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting udev Coldplug all Devices...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Local File Systems (Pre).&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Local File Systems.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Tell Plymouth To Write Out Runtime Data...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Load/Save Random Seed...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Tell Plymouth To Write Out Runtime Data.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Load/Save Random Seed.&lt;BR /&gt;systemd-journald[107]: Received request to flush runtime journal from PID 1&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Flush Journal to Persistent Storage.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Create Volatile Files and Directories...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: Raise network interfaces....&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Create Volatile Files and Directories.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Network Time Synchronization...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Update UTMP about System Boot/Shutdown...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Network Time Synchronization.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Update UTMP about System Boot/Shutdown.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target System Time Synchronized.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: Raise network interfaces..&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started udev Coldplug all Devices.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Found device /dev/ttymxc0.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Dispatch Password Requests to Console Directory Watch.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Created slice system-systemd\x2dbacklight.slice.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Load/Save Screen Backlight...htness of backlight:backlight...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Network.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Network is Online.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Load/Save Screen Backlight Brightness of backlight:backlight.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target System Initialization.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Daily Cleanup of Temporary Directories.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Timers.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on D-Bus System Message Bus Socket.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Listening on ACPID Listen Socket.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Sockets.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Trigger resolvconf update for networkd DNS.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started ACPI Events Check.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Paths.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Basic System.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started D-Bus System Message Bus.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Network Manager...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Initialize hardware monitoring sensors...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Login Service...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started OpenBSD Secure Shell server.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: Advanced IEEE 802.11 management daemon...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting System Logging Service...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Run anacron jobs.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting /etc/rc.local Compatibility...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: Load kernel modules needed to enable cpufreq scaling...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started ACPI event daemon.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: network benchmark...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Permit User Sessions...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: Advanced IEEE 802.11 management daemon.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started /etc/rc.local Compatibility.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Permit User Sessions.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started System Logging Service.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: network benchmark.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Initialize hardware monitoring sensors.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: Load kernel modules needed to enable cpufreq scaling.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Login Service.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Authenticate and Authorize Users to Run Privileged Tasks...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Sound Card.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting LSB: set CPUFreq kernel parameters...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Light Display Manager...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Terminate Plymouth Boot Screen...&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Wait for Plymouth Boot Screen to Quit...&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Terminate Plymouth Boot Screen.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Wait for Plymouth Boot Screen to Quit.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started LSB: set CPUFreq kernel parameters.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Authenticate and Authorize Users to Run Privileged Tasks.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Light Display Manager.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Network Manager.&lt;BR /&gt;fec 20b4000.ethernet eth0: Freescale FEC PHY driver [Micrel KSZ8081 or KSZ8091] (mii_bus:phy_addr=20b4000.ethernet:01, irq=-1)&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Getty on tty1.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Serial Getty on ttymxc0.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Login Prompts.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Multi-User System.&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Reached target Graphical Interface.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Starting Update UTMP about System Runlevel Changes...&lt;BR /&gt;fec 2188000.ethernet eth1: Freescale FEC PHY driver [Micrel KSZ8081 or KSZ8091] (mii_bus:phy_addr=20b4000.ethernet:02, irq=-1)&lt;BR /&gt;[&amp;nbsp; OK&amp;nbsp; ] Started Update UTMP about System Runlevel Changes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debian GNU/Linux 8 linaro-alip ttymxc0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linaro-alip login: root (automatic login)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Authentication failure&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debian GNU/Linux 8 linaro-alip ttymxc0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linaro-alip login: root (automatic login)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Authentication failure&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debian GNU/Linux 8 linaro-alip ttymxc0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linaro-alip login: root (automatic login)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Authentication failure&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debian GNU/Linux 8 linaro-alip ttymxc0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linaro-alip login: root (automatic login)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Authentication failure&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debian GNU/Linux 8 linaro-alip ttymxc0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linaro-alip login: root (automatic login)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Authentication failure&lt;BR /&gt;fec 2188000.ethernet eth1: Link is Up - 100Mbps/Full - flow control rx/tx&lt;BR /&gt;random: nonblocking pool is initialized&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 01:39:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-login-to-my-i-MX6ULL-evk-board/m-p/677958#M104583</guid>
      <dc:creator>pablocottens</dc:creator>
      <dc:date>2017-06-07T01:39:19Z</dc:date>
    </item>
    <item>
      <title>Re: How do I login to my i.MX6ULL evk board?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-login-to-my-i-MX6ULL-evk-board/m-p/677959#M104584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can login without password.&lt;/P&gt;&lt;P style="color: #000000; background-color: #ffffff; border: 0px;"&gt;You need to add "--autologin root" parameter&lt;/P&gt;&lt;P style="color: #000000; background-color: #ffffff; border: 0px;"&gt;into the line with "respawn:/sbin/getty" option in /etc/inittab.&lt;/P&gt;&lt;P style="color: #000000; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #000000; background-color: #ffffff; border: 0px;"&gt;Regards,&lt;/P&gt;&lt;P style="color: #000000; background-color: #ffffff; border: 0px;"&gt;Aravinth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 05:56:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-login-to-my-i-MX6ULL-evk-board/m-p/677959#M104584</guid>
      <dc:creator>aravinthkumarja</dc:creator>
      <dc:date>2017-06-07T05:56:30Z</dc:date>
    </item>
    <item>
      <title>Re: How do I login to my i.MX6ULL evk board?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-login-to-my-i-MX6ULL-evk-board/m-p/677960#M104585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;But I can't login to change the file. I tried editing the file in the rootfs folder, but as I'm using mint (I think it's because of this) I didn't get a /etc/inittab file ... as of now I'm searching for a way to do the "--autologin root" this on mint and then reflash&amp;nbsp; to the SD card. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Aside from that, any other suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 11:35:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-login-to-my-i-MX6ULL-evk-board/m-p/677960#M104585</guid>
      <dc:creator>pablocottens</dc:creator>
      <dc:date>2017-06-07T11:35:14Z</dc:date>
    </item>
    <item>
      <title>Re: How do I login to my i.MX6ULL evk board?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-login-to-my-i-MX6ULL-evk-board/m-p/677961#M104586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nevermind. The problem was in the distro I was using. I thought that since Mint was based on Debian (or Ubuntu ... don't recall now) then it wouldn't be a problem. But still...today I downloaded and installed ubuntu and&amp;nbsp;did the steps for the rootfs again and everything worked perfectly.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2017 02:06:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-login-to-my-i-MX6ULL-evk-board/m-p/677961#M104586</guid>
      <dc:creator>pablocottens</dc:creator>
      <dc:date>2017-06-08T02:06:56Z</dc:date>
    </item>
  </channel>
</rss>