<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FlexCAN in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN/m-p/677838#M104560</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FlexCAN is just the name for the CAN controller IP of the i.MX6 series processors, and, yes, it supports both CAN 2.0 Part A and CAN 2.0 Part B specifications.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Jun 2017 05:35:34 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2017-06-29T05:35:34Z</dc:date>
    <item>
      <title>FlexCAN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN/m-p/677837#M104559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to use CAN 2.0A and 2.0B to communicate the external device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, IMX6UL is FIexCAN type. Can the FlexCAN supports CAN 2.0A and 2.0B?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it does not support, Could you please recommend me what adding external IC?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jun 2017 03:52:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN/m-p/677837#M104559</guid>
      <dc:creator>nuttakorntrirat</dc:creator>
      <dc:date>2017-06-29T03:52:48Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN/m-p/677838#M104560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FlexCAN is just the name for the CAN controller IP of the i.MX6 series processors, and, yes, it supports both CAN 2.0 Part A and CAN 2.0 Part B specifications.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jun 2017 05:35:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN/m-p/677838#M104560</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-06-29T05:35:34Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN/m-p/677839#M104561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petukhov,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Mang thanks for your answer.&lt;/P&gt;&lt;P&gt;Nuttakorn&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jun 2017 06:00:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN/m-p/677839#M104561</guid>
      <dc:creator>nuttakorntrirat</dc:creator>
      <dc:date>2017-06-29T06:00:52Z</dc:date>
    </item>
  </channel>
</rss>