<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: usb upgrade in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/usb-upgrade/m-p/677785#M104555</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can use the mfgtool nxp provide to download the new linux images to your board. Via the usb-otg line connect your board to PC to download.&lt;BR /&gt;Have a great day,&lt;BR /&gt; Rita&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Jul 2017 02:51:58 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2017-07-21T02:51:58Z</dc:date>
    <item>
      <title>usb upgrade</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/usb-upgrade/m-p/677784#M104554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;two imx6d board connetc with usb, one run android and the other run linux. i want upgrade linux board through usb, is there a proper way to do this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jul 2017 02:02:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/usb-upgrade/m-p/677784#M104554</guid>
      <dc:creator>yufe</dc:creator>
      <dc:date>2017-07-21T02:02:50Z</dc:date>
    </item>
    <item>
      <title>Re: usb upgrade</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/usb-upgrade/m-p/677785#M104555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can use the mfgtool nxp provide to download the new linux images to your board. Via the usb-otg line connect your board to PC to download.&lt;BR /&gt;Have a great day,&lt;BR /&gt; Rita&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jul 2017 02:51:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/usb-upgrade/m-p/677785#M104555</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2017-07-21T02:51:58Z</dc:date>
    </item>
    <item>
      <title>Re: usb upgrade</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/usb-upgrade/m-p/677786#M104556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;my hardware is not support this mode, boot conf pins are fixed. host android board and salve linux borad connect through usb only.&lt;/P&gt;&lt;P&gt;is there a way to upgrade uboot, kernel or fs? i see tplink route and other product support internet online upgrade, can usb do the same thing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 02:16:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/usb-upgrade/m-p/677786#M104556</guid>
      <dc:creator>yufe</dc:creator>
      <dc:date>2017-07-24T02:16:30Z</dc:date>
    </item>
  </channel>
</rss>