<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.mx6ull DVFS</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6ull-DVFS/m-p/677768#M104549</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;these numbers are very rough estimation, just for reference according to&lt;/P&gt;&lt;P&gt;AN5345 Table 4. Dhrystone benchmark measurement results: 157mA@528MHz&lt;BR /&gt;&lt;A href="http://www.nxp.com/docs/en/application-note/AN5345.pdf"&gt;www.nxp.com/docs/en/application-note/AN5345.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Cortex-A7 core power consumption is 100uW/MHz&amp;nbsp;&lt;/P&gt;&lt;P&gt;You are right, there is no industrial 900MHz grade, just 800MHz: MCIMX6Y2CVM08AA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Jul 2017 02:25:13 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-07-21T02:25:13Z</dc:date>
    <item>
      <title>i.mx6ull DVFS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6ull-DVFS/m-p/677767#M104548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear &amp;nbsp;Expert:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the IMX6ULLCEC (Rev. 1.1, 05/2017)document，there is a table below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26374i7F30BE3BC4C96A77/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But in the&amp;nbsp;Rev. 0, 09/2016,there is a table below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26496i384D4582D6A239DD/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;About VDD_SOC_IN,one's condition is 900Mhz,another is 528MHz,but the Max Current is the same,that is correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Futhermore,in the&amp;nbsp;IMX6ULLIEC document,I can not find the 900MHz version,is there i.mx6ull 900Mhz industry version?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please help,thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jul 2017 01:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6ull-DVFS/m-p/677767#M104548</guid>
      <dc:creator>strive</dc:creator>
      <dc:date>2017-07-21T01:40:46Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6ull DVFS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6ull-DVFS/m-p/677768#M104549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;these numbers are very rough estimation, just for reference according to&lt;/P&gt;&lt;P&gt;AN5345 Table 4. Dhrystone benchmark measurement results: 157mA@528MHz&lt;BR /&gt;&lt;A href="http://www.nxp.com/docs/en/application-note/AN5345.pdf"&gt;www.nxp.com/docs/en/application-note/AN5345.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Cortex-A7 core power consumption is 100uW/MHz&amp;nbsp;&lt;/P&gt;&lt;P&gt;You are right, there is no industrial 900MHz grade, just 800MHz: MCIMX6Y2CVM08AA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jul 2017 02:25:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6ull-DVFS/m-p/677768#M104549</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-21T02:25:13Z</dc:date>
    </item>
  </channel>
</rss>