<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6DL, ONOFF Button press causes RESTART instead of POWER OFF if booting from eMMC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-ONOFF-Button-press-causes-RESTART-instead-of-POWER-OFF-if/m-p/677375#M104475</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The IMX6dl reference manual states that a 5 second press of the ONOFF button should power down the device. &amp;nbsp;If we boot from an SD card, then everything works correctly and the device powers down. &amp;nbsp;If we boot from eMMC, then the system going down correctly, but then immediately starts back up. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone have an idea why the boot location would affect the performance? &amp;nbsp;Are the settings for the eMMC that need to be set in order to enable power down instead of reset? &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Jun 2017 21:31:04 GMT</pubDate>
    <dc:creator>dcolon</dc:creator>
    <dc:date>2017-06-06T21:31:04Z</dc:date>
    <item>
      <title>IMX6DL, ONOFF Button press causes RESTART instead of POWER OFF if booting from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-ONOFF-Button-press-causes-RESTART-instead-of-POWER-OFF-if/m-p/677375#M104475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The IMX6dl reference manual states that a 5 second press of the ONOFF button should power down the device. &amp;nbsp;If we boot from an SD card, then everything works correctly and the device powers down. &amp;nbsp;If we boot from eMMC, then the system going down correctly, but then immediately starts back up. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone have an idea why the boot location would affect the performance? &amp;nbsp;Are the settings for the eMMC that need to be set in order to enable power down instead of reset? &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jun 2017 21:31:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-ONOFF-Button-press-causes-RESTART-instead-of-POWER-OFF-if/m-p/677375#M104475</guid>
      <dc:creator>dcolon</dc:creator>
      <dc:date>2017-06-06T21:31:04Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6DL, ONOFF Button press causes RESTART instead of POWER OFF if booting from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-ONOFF-Button-press-causes-RESTART-instead-of-POWER-OFF-if/m-p/677376#M104476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Small extra tidbit of information. &amp;nbsp;If we interrupt Uboot and get to the Uboot terminal, and then try to shutdown, it still restarts if we booted from eMMC and shuts down if we booted from SD card. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Whatever is causing this issue does not seem to be related to loading the Kernel&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 19:08:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-ONOFF-Button-press-causes-RESTART-instead-of-POWER-OFF-if/m-p/677376#M104476</guid>
      <dc:creator>dcolon</dc:creator>
      <dc:date>2017-06-07T19:08:18Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6DL, ONOFF Button press causes RESTART instead of POWER OFF if booting from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-ONOFF-Button-press-causes-RESTART-instead-of-POWER-OFF-if/m-p/677377#M104477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which version BSP are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jun 2017 03:22:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-ONOFF-Button-press-causes-RESTART-instead-of-POWER-OFF-if/m-p/677377#M104477</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2017-06-30T03:22:13Z</dc:date>
    </item>
  </channel>
</rss>