<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6 internal thermal sensor safe values in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-internal-thermal-sensor-safe-values/m-p/677233#M104467</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;What is the actual location of i.MX6 internal thermal sensor ? How the temperature values are different from Tj. What are the recommended safe limits of temperature to throttle down the frequency or shutdown the processor?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Jun 2017 12:28:10 GMT</pubDate>
    <dc:creator>himanshu_gupta</dc:creator>
    <dc:date>2017-06-28T12:28:10Z</dc:date>
    <item>
      <title>i.MX6 internal thermal sensor safe values</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-internal-thermal-sensor-safe-values/m-p/677233#M104467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;What is the actual location of i.MX6 internal thermal sensor ? How the temperature values are different from Tj. What are the recommended safe limits of temperature to throttle down the frequency or shutdown the processor?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jun 2017 12:28:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-internal-thermal-sensor-safe-values/m-p/677233#M104467</guid>
      <dc:creator>himanshu_gupta</dc:creator>
      <dc:date>2017-06-28T12:28:10Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 internal thermal sensor safe values</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-internal-thermal-sensor-safe-values/m-p/677234#M104468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Himanshu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thermal sensor is described on app notes :&lt;/P&gt;&lt;P&gt;AN5215 i.MX 6 Temperature Sensor Module&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN5215.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/docs/en/application-note/AN5215.pdf&lt;/A&gt;&lt;BR /&gt;AN4579 i.MX 6 Series Thermal Management Guidelines &lt;BR /&gt;&lt;A href="http://cache.nxp.com/docs/en/application-note/AN4579.pdf"&gt;http://cache.nxp.com/docs/en/application-note/AN4579.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Actual location of i.MX6 internal thermal sensor is not available, &lt;/P&gt;&lt;P&gt;one can consider that it measures Tj.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jun 2017 23:18:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-internal-thermal-sensor-safe-values/m-p/677234#M104468</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-28T23:18:27Z</dc:date>
    </item>
  </channel>
</rss>