<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX6ULG0 kernel booting stuck</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULG0-kernel-booting-stuck/m-p/677165#M104459</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;Thanks for the quick reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp;am using same u-boot.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Only difference is kernel zImage, dtb files and modules.&lt;/P&gt;&lt;P&gt;One more thing FSLC linux is booting on IMX6ULG2 board. Same kernel(sdcard) stuck on IMX6ULG0 board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you suggest&amp;nbsp;me what exactly i have to check for&amp;nbsp;memory initialization in u-boot for IMX6ULG2 &amp;amp; IMX6ULG0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yuvi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 May 2017 09:45:40 GMT</pubDate>
    <dc:creator>yuvrajdodia</dc:creator>
    <dc:date>2017-05-12T09:45:40Z</dc:date>
    <item>
      <title>IMX6ULG0 kernel booting stuck</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULG0-kernel-booting-stuck/m-p/677163#M104457</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using custom imx6ul board.&lt;/P&gt;&lt;P&gt;I have 2 type of boards, 1 with MCIMX6UL&lt;STRONG&gt;G2&lt;/STRONG&gt; &amp;amp; 1 with MCIMX6UL&lt;STRONG&gt;G0 &lt;/STRONG&gt;other than controller everything is same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using linux-fslc-4.1-2.0.x-imx kernel.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;kernel is working with MCIMX6UL&lt;/SPAN&gt;&lt;STRONG&gt;G2&amp;nbsp;&lt;/STRONG&gt;board and i am able to boot board.&lt;/P&gt;&lt;P&gt;same kernel is not working with MCIMX6ULG0 board.&lt;/P&gt;&lt;P&gt;After u-boot message kernel booting stuck at&amp;nbsp;&lt;SPAN&gt;Starting kernel/booting the kernel.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I&amp;nbsp;change controller from IMX6ULG2 to IMX6ULG0, Is there anything i have to modify?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On same IMX6ULG0 board i am able to boot custom linux kernel compiled using&lt;/P&gt;&lt;P&gt;&lt;A class="jivelink1" href="https://eewiki.net/display/linuxonarm/MCIMX6UL-EVK" title="https://eewiki.net/display/linuxonarm/MCIMX6UL-EVK"&gt;https://eewiki.net/display/linuxonarm/MCIMX6UL-EVK&lt;/A&gt;&lt;/P&gt;&lt;P&gt;So board/hardware is working fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Boot log:&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;U-Boot SPL 2016.07-rc2-dirty (Mar 01 2017 - 15:26:37)&lt;BR /&gt;Trying to boot from MMC1&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2016.07-rc2-dirty (Mar 01 2017 - 15:26:37 +0530)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6UL rev1.0 528 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 30C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6UL 14x14 EVK&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Net: CPU Net Initialization Failed&lt;BR /&gt;No ethernet found.&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;SD/MMC found on device 1&lt;BR /&gt;Checking for: /uEnv.txt ...&lt;BR /&gt;Checking for: /boot/uEnv.txt ...&lt;BR /&gt;24 bytes read in 77 ms (0 Bytes/s)&lt;BR /&gt;Loaded environment from /boot/uEnv.txt&lt;BR /&gt;Checking if uname_r is set in /boot/uEnv.txt...&lt;BR /&gt;Running uname_boot ...&lt;BR /&gt;loading /boot/vmlinuz-4.1.39-armv7-x5 ...&lt;BR /&gt;6719848 bytes read in 386 ms (16.6 MiB/s)&lt;BR /&gt;loading /boot/dtbs/4.1.39-armv7-x5/imx6ul-14x14-evk.dtb ...&lt;BR /&gt;36042 bytes read in 162 ms (216.8 KiB/s)&lt;BR /&gt;debug: [console=ttymxc0,115200 root=/dev/mmcblk1p2 ro rootfstype=ext4 rootwait] ...&lt;BR /&gt;debug: [bootz 0x82000000 - 0x83000000] ...&lt;BR /&gt;Kernel image @ 0x82000000 [ 0x000000 - 0x668968 ]&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt; Booting using the fdt blob at 0x83000000&lt;BR /&gt; Using Device Tree in place at 83000000, end 8300bcc9&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;Uncompressing Linux... done, booting the kernel.&lt;/P&gt;&lt;P&gt;--------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me to fix/modify&amp;nbsp;&lt;SPAN&gt;linux-fslc-4.1-2.0.x-imx kernel for IMX6ULG0 controller.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Yuvi&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 May 2017 15:16:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6ULG0-kernel-booting-stuck/m-p/677163#M104457</guid>
      <dc:creator>yuvrajdodia</dc:creator>
      <dc:date>2017-05-11T15:16:12Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6ULG0 kernel booting stuck</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULG0-kernel-booting-stuck/m-p/677164#M104458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please check if memory initialization of Your U-boot is the same as for working case.&lt;/P&gt;&lt;P&gt;Also the following may be helpful&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/838547"&gt;https://community.nxp.com/message/838547&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 May 2017 07:41:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6ULG0-kernel-booting-stuck/m-p/677164#M104458</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-05-12T07:41:22Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6ULG0 kernel booting stuck</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULG0-kernel-booting-stuck/m-p/677165#M104459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;Thanks for the quick reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp;am using same u-boot.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Only difference is kernel zImage, dtb files and modules.&lt;/P&gt;&lt;P&gt;One more thing FSLC linux is booting on IMX6ULG2 board. Same kernel(sdcard) stuck on IMX6ULG0 board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you suggest&amp;nbsp;me what exactly i have to check for&amp;nbsp;memory initialization in u-boot for IMX6ULG2 &amp;amp; IMX6ULG0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yuvi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 May 2017 09:45:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6ULG0-kernel-booting-stuck/m-p/677165#M104459</guid>
      <dc:creator>yuvrajdodia</dc:creator>
      <dc:date>2017-05-12T09:45:40Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6ULG0 kernel booting stuck</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULG0-kernel-booting-stuck/m-p/677166#M104460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; What are exact part numbers of &amp;nbsp;the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;IMX6ULG2 &amp;amp; IMX6ULG0 ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 May 2017 06:57:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6ULG0-kernel-booting-stuck/m-p/677166#M104460</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-05-18T06:57:09Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6ULG0 kernel booting stuck</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULG0-kernel-booting-stuck/m-p/677167#M104461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to boot&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;linux-fslc-4.1-2.0.x-imx kernel on my MCIMX6ULG0 board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Initially i was using gcc-linaro-5.4.1-2017.01, I try with gcc-linaro-5.3.1-2016.05 and it start working.&lt;/P&gt;&lt;P&gt;I am not sure.&amp;nbsp;What is changed between 2 compiler versions and how kernel booting issue is fixed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FYI, exact part numbers are MCIMX6G2DVM05AA &amp;amp; MCIMX6G0DVM05AA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for you support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Yuvi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 May 2017 07:17:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6ULG0-kernel-booting-stuck/m-p/677167#M104461</guid>
      <dc:creator>yuvrajdodia</dc:creator>
      <dc:date>2017-05-18T07:17:11Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6ULG0 kernel booting stuck</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULG0-kernel-booting-stuck/m-p/677168#M104462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Is it possible to try NXP Linux ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 May 2017 08:53:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6ULG0-kernel-booting-stuck/m-p/677168#M104462</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-05-26T08:53:05Z</dc:date>
    </item>
  </channel>
</rss>