<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX7D Regarding TEMPMON without RTC XTAL　</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-Regarding-TEMPMON-without-RTC-XTAL/m-p/677052#M104450</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Support-team.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our customer do not use RTC(32KHz).&lt;BR /&gt;But customer want to use TEMPMON(Temperature Monitor).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even if we do not use the 32 KHz RTC, it looks like i.MX7D can be used with 40 KHz RingOSC.&lt;BR /&gt;-------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;(i.MX7DRM.pdf) Rev. 0.1&lt;BR /&gt;5.1.3.2 Oscillator&lt;/P&gt;&lt;P&gt;Either the 32KHz XTAL or the 40KHz RingOSC can be used as the source of the 32KHz&lt;BR /&gt;clock to CCM and then get delivered to the rest of the SoC. Due to the 32KHz XTAL&lt;BR /&gt;start up time, 40KHz RingOSC is selected as the default clock source during SoC power&lt;BR /&gt;up. Once the 32KHz XTAL starts up, the clock source will be switched to it&lt;BR /&gt;automatically and the 40KHz RingOSC will be shut off. If the 32KHz XTAL stops in&lt;BR /&gt;some case, the 40KHz RingOSC will be enabled and selected as the source. The enable/&lt;BR /&gt;disable of the 40KHz RingOSC and the clock source switching is done automatically in&lt;BR /&gt;HW and there is no programmable register for SW to select the clock source. There is&lt;BR /&gt;only one read-only register to show the current clock source.&lt;BR /&gt;-------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can we use TEMPMON without 32 KHz RTC?&lt;BR /&gt;If yes,&lt;BR /&gt;1) Do we need any special setting?&lt;BR /&gt;2) Please also let me know if you have any caveats.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Jun 2017 05:53:27 GMT</pubDate>
    <dc:creator>tomohisa_sakamo</dc:creator>
    <dc:date>2017-06-07T05:53:27Z</dc:date>
    <item>
      <title>i.MX7D Regarding TEMPMON without RTC XTAL　</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-Regarding-TEMPMON-without-RTC-XTAL/m-p/677052#M104450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Support-team.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our customer do not use RTC(32KHz).&lt;BR /&gt;But customer want to use TEMPMON(Temperature Monitor).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even if we do not use the 32 KHz RTC, it looks like i.MX7D can be used with 40 KHz RingOSC.&lt;BR /&gt;-------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;(i.MX7DRM.pdf) Rev. 0.1&lt;BR /&gt;5.1.3.2 Oscillator&lt;/P&gt;&lt;P&gt;Either the 32KHz XTAL or the 40KHz RingOSC can be used as the source of the 32KHz&lt;BR /&gt;clock to CCM and then get delivered to the rest of the SoC. Due to the 32KHz XTAL&lt;BR /&gt;start up time, 40KHz RingOSC is selected as the default clock source during SoC power&lt;BR /&gt;up. Once the 32KHz XTAL starts up, the clock source will be switched to it&lt;BR /&gt;automatically and the 40KHz RingOSC will be shut off. If the 32KHz XTAL stops in&lt;BR /&gt;some case, the 40KHz RingOSC will be enabled and selected as the source. The enable/&lt;BR /&gt;disable of the 40KHz RingOSC and the clock source switching is done automatically in&lt;BR /&gt;HW and there is no programmable register for SW to select the clock source. There is&lt;BR /&gt;only one read-only register to show the current clock source.&lt;BR /&gt;-------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can we use TEMPMON without 32 KHz RTC?&lt;BR /&gt;If yes,&lt;BR /&gt;1) Do we need any special setting?&lt;BR /&gt;2) Please also let me know if you have any caveats.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 05:53:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-Regarding-TEMPMON-without-RTC-XTAL/m-p/677052#M104450</guid>
      <dc:creator>tomohisa_sakamo</dc:creator>
      <dc:date>2017-06-07T05:53:27Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7D Regarding TEMPMON without RTC XTAL　</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-Regarding-TEMPMON-without-RTC-XTAL/m-p/677053#M104451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomohisa&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Can we use TEMPMON without 32 KHz RTC?&lt;BR /&gt;yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;1) Do we need any special setting?&lt;/P&gt;&lt;P&gt;no&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;gt;2) Please also let me know if you have any caveats.&lt;/P&gt;&lt;P&gt;there are no caveats for using TEMPMON without 32 KHz RTC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 09:59:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-Regarding-TEMPMON-without-RTC-XTAL/m-p/677053#M104451</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-07T09:59:15Z</dc:date>
    </item>
  </channel>
</rss>