<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: BLE interfacing with i.MX6 over UART in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/BLE-interfacing-with-i-MX6-over-UART/m-p/676724#M104388</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rahul&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in general it is not necessary to use all 4 pins of UART, but flow control&lt;/P&gt;&lt;P&gt;allows to achieve more fast and reliable communication with peripheral.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 May 2017 23:20:10 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-05-11T23:20:10Z</dc:date>
    <item>
      <title>BLE interfacing with i.MX6 over UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BLE-interfacing-with-i-MX6-over-UART/m-p/676723#M104387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;We have a device in which we are using MCIMX6L8DVN10AA processor.We want to add BLE functionality into the device.For this, we are planning to use CC2640 Bluetooth Smart IC.&lt;/P&gt;&lt;P&gt;In CC2640 only 2 UART lines (RX and TX) are available for communication.&lt;/P&gt;&lt;P&gt;In processor, we have free UART (J19,J21,T20, T21) for UART (Tx, Rx, RTS &amp;amp; CTS lines) to communicate with CC2640 Smart IC.&lt;/P&gt;&lt;P&gt;My Query is:&lt;/P&gt;&lt;P&gt;Is UART 3 HCI Based?&lt;/P&gt;&lt;P&gt;Is there any necessary to use all 4 pins of UART for communicating with CC2640 or we can go for only 2 pins of UART (Tx &amp;amp; Rx) for communication by disabling Flow control&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 May 2017 11:16:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BLE-interfacing-with-i-MX6-over-UART/m-p/676723#M104387</guid>
      <dc:creator>rahulsoni</dc:creator>
      <dc:date>2017-05-11T11:16:50Z</dc:date>
    </item>
    <item>
      <title>Re: BLE interfacing with i.MX6 over UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BLE-interfacing-with-i-MX6-over-UART/m-p/676724#M104388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rahul&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in general it is not necessary to use all 4 pins of UART, but flow control&lt;/P&gt;&lt;P&gt;allows to achieve more fast and reliable communication with peripheral.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 May 2017 23:20:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BLE-interfacing-with-i-MX6-over-UART/m-p/676724#M104388</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-05-11T23:20:10Z</dc:date>
    </item>
  </channel>
</rss>