<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Device tree setup for BCM4343W</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Device-tree-setup-for-BCM4343W/m-p/676586#M104356</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jaya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at imx6sl-evk-btwifi.dts&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6sl-evk-btwifi.dts?h=imx_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6sl-evk-btwifi.dts?h=imx_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.0.0_ga"&gt;linux-imx.git - i.MX Linux Kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Broadcom firmware packages&lt;BR /&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=BCMDHD-L4.1.15&amp;amp;amp;appType=license&amp;amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType=" title="https://www.nxp.com/webapp/Download?colCode=BCMDHD-L4.1.15&amp;amp;amp;appType=license&amp;amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType="&gt;https://www.nxp.com/webapp/Download?colCode=BCMDHD-L4.1.15&amp;amp;amp;appType=license&amp;amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&amp;amp;…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Chapter 46 Wi-Fi BCM4339 Driver attached Linux Manual.&lt;/P&gt;&lt;P&gt;also one can apply to Murata support link&lt;BR /&gt;wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Jul 2017 10:33:05 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-07-20T10:33:05Z</dc:date>
    <item>
      <title>Device tree setup for BCM4343W</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-tree-setup-for-BCM4343W/m-p/676585#M104355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a new board using i.mx6sololite interfaced via SD3 (mmc2) to a BCM4343W wifi/bluetooth chip. I'm using Linux 4.1.15. I'm running into a bit of trouble getting the chip detected. I wanted to check if anyone else has a working device tree setup that is similar so that I can compare if I've made some mistakes in the configuration. My current configuration is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;wlan_en_reg: fixedregulator {&lt;BR /&gt; compatible = "regulator-fixed";&lt;BR /&gt; regulator-min-microvolt = &amp;lt;5000000&amp;gt;;&lt;BR /&gt; regulator-max-microvolt = &amp;lt;5000000&amp;gt;;&lt;BR /&gt; regulator-name = "wlan_enable_regulator";&lt;BR /&gt; gpio = &amp;lt;&amp;amp;gpio5 10&amp;gt;; //active high /* this is WL_REG_ON/WIFI_REG_ON/SD1_DAT7/GPIO5_IO10 */&lt;BR /&gt; enable-active-high;&lt;BR /&gt; startup-delay-us = &amp;lt;100&amp;gt;;&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;amp;usdhc3 {&lt;BR /&gt; pinctrl-names = "default";&lt;BR /&gt; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_usdhc3&amp;gt;;&lt;BR /&gt; no-1-8-v;&lt;BR /&gt; non-removable;&lt;BR /&gt; cd-post;&lt;BR /&gt; pm-ignore-notify;&lt;BR /&gt; bus-width = &amp;lt;4&amp;gt;;&lt;BR /&gt; vmmc-supply = &amp;lt;&amp;amp;wlan_en_reg&amp;gt;;&lt;BR /&gt; keep-power-in-suspend;&lt;BR /&gt; enable-sdio-wakeup;&lt;BR /&gt; needs-special-hs-handling;&lt;BR /&gt; status = "okay";&lt;BR /&gt; wifi-host;&lt;/P&gt;&lt;P&gt;bcmdhd_wlan_0: bcmdhd_wlan@0 {&lt;BR /&gt; compatible = "android,bcmdhd_wlan";&lt;BR /&gt; wlreg_on-supply = &amp;lt;&amp;amp;wlan_en_reg&amp;gt;;&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;pinctrl_usdhc3: usdhc3grp {&lt;BR /&gt; fsl,pins = &amp;lt;&lt;BR /&gt; MX6SL_PAD_SD3_CMD__SD3_CMD 0x17059&lt;BR /&gt; MX6SL_PAD_SD3_CLK__SD3_CLK 0x10059&lt;BR /&gt; MX6SL_PAD_SD3_DAT0__SD3_DATA0 0x17059&lt;BR /&gt; MX6SL_PAD_SD3_DAT1__SD3_DATA1 0x17059&lt;BR /&gt; MX6SL_PAD_SD3_DAT2__SD3_DATA2 0x17059&lt;BR /&gt; MX6SL_PAD_SD3_DAT3__SD3_DATA3 0x17059&lt;BR /&gt; MX6SL_PAD_SD1_DAT6__GPIO5_IO07 0x13059 /* wlan irq for solace */&lt;BR /&gt; MX6SL_PAD_SD1_DAT7__GPIO5_IO10 0x13059 /* wlan en for solace */&lt;BR /&gt; &amp;gt;;&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With these settings, I'm getting the following bootup output:&lt;/P&gt;&lt;P&gt;sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified&lt;BR /&gt;sdhci-esdhc-imx 2190000.usdhc: No vmmc regulator found&lt;BR /&gt;sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found&lt;BR /&gt;mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using DMA&lt;BR /&gt;/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found&lt;BR /&gt;mmc0: host does not support reading read-only switch, assuming write-enable&lt;BR /&gt;mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using DMA&lt;BR /&gt;/soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified&lt;BR /&gt;sdhci-esdhc-imx 2198000.usdhc: assigned as wifi host&lt;BR /&gt;sdhci-esdhc-imx 2198000.usdhc: Failed getting OCR mask: 0&lt;BR /&gt;mmc0: new high speed SDHC card at address 0007&lt;BR /&gt;sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found&lt;BR /&gt;mmcblk0: mmc0:0007 Y008B 7.42 GiB&lt;BR /&gt;sdhci-esdhc-imx 2198000.usdhc: could not set regulator OCR (-22)&lt;BR /&gt; mmcblk0: p1 p2&lt;BR /&gt;sdhci-esdhc-imx 2198000.usdhc: could not set regulator OCR (-22)&lt;BR /&gt;mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using DMA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The other SD/MMC interfaces on mmc0 and mmc1 are working fine. But mmc2 is not detecting the chip. It is a 5V chip so I thought&amp;nbsp;my regulator settings are correct. As an experiment, I also tried:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;wlan_en_reg: fixedregulator {&lt;BR /&gt; compatible = "regulator-fixed";&lt;BR /&gt; regulator-min-microvolt = &amp;lt;1800000&amp;gt;;&lt;BR /&gt; regulator-max-microvolt = &amp;lt;1800000&amp;gt;;&lt;BR /&gt; regulator-name = "wlan_enable_regulator";&lt;BR /&gt; gpio = &amp;lt;&amp;amp;gpio5 10 GPIO_ACTIVE_HIGH&amp;gt;; //active high /* this is WL_REG_ON/WIFI_REG_ON/SD1_DAT7/GPIO5_IO10 */&lt;BR /&gt; output-high;&lt;BR /&gt; enable-active-high;&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;amp;usdhc3 {&lt;BR /&gt; non-removable;&lt;BR /&gt; no-1-8-v;&lt;BR /&gt; bus-width = &amp;lt;4&amp;gt;;&lt;BR /&gt; cap-power-off-card;&lt;BR /&gt; vmmc-supply = &amp;lt;&amp;amp;wlan_en_reg&amp;gt;;&lt;BR /&gt; pinctrl-names = "default";&lt;BR /&gt; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_usdhc3&amp;gt;;&lt;BR /&gt; keep-power-in-suspend;&lt;BR /&gt; enable-sdio-wakeup;&lt;BR /&gt; needs-special-hs-handling;&lt;BR /&gt; status = "okay";&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and I got a similar&amp;nbsp;set of errors:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified&lt;BR /&gt;sdhci-esdhc-imx 2190000.usdhc: No vmmc regulator found&lt;BR /&gt;sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found&lt;BR /&gt;mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using DMA&lt;BR /&gt;/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found&lt;BR /&gt;mmc0: host does not support reading read-only switch, assuming write-enable&lt;BR /&gt;mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using DMA&lt;BR /&gt;/soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified&lt;BR /&gt;sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found&lt;BR /&gt;mmc0: new high speed SDHC card at address 0007&lt;BR /&gt;mmcblk0: mmc0:0007 Y008B 7.42 GiB&lt;BR /&gt; mmcblk0: p1 p2&lt;BR /&gt;mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using DMA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for any suggestions / feedback.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jul 2017 06:09:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-tree-setup-for-BCM4343W/m-p/676585#M104355</guid>
      <dc:creator>jayakumar2</dc:creator>
      <dc:date>2017-07-20T06:09:31Z</dc:date>
    </item>
    <item>
      <title>Re: Device tree setup for BCM4343W</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-tree-setup-for-BCM4343W/m-p/676586#M104356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jaya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at imx6sl-evk-btwifi.dts&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6sl-evk-btwifi.dts?h=imx_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6sl-evk-btwifi.dts?h=imx_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.0.0_ga"&gt;linux-imx.git - i.MX Linux Kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Broadcom firmware packages&lt;BR /&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=BCMDHD-L4.1.15&amp;amp;amp;appType=license&amp;amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType=" title="https://www.nxp.com/webapp/Download?colCode=BCMDHD-L4.1.15&amp;amp;amp;appType=license&amp;amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType="&gt;https://www.nxp.com/webapp/Download?colCode=BCMDHD-L4.1.15&amp;amp;amp;appType=license&amp;amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&amp;amp;…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Chapter 46 Wi-Fi BCM4339 Driver attached Linux Manual.&lt;/P&gt;&lt;P&gt;also one can apply to Murata support link&lt;BR /&gt;wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jul 2017 10:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-tree-setup-for-BCM4343W/m-p/676586#M104356</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-20T10:33:05Z</dc:date>
    </item>
  </channel>
</rss>