<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Linux iMX6 PCIe driver, Linux 4.4  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-iMX6-PCIe-driver-Linux-4-4/m-p/676429#M104326</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even though the Hummingboard does not use an external PCIe clock, it seems that this issue isn't a clocking problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After discussing this issue with SolidRun, they suggested testing the VMX-200 PCIe video card with the PCIe driver in latest Linux 4.4 kernel.&amp;nbsp;&amp;nbsp; Sure enough, the card initializes correctly with the 4.4 PCIe driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Although the PCIe support seems much improved in the 4.4 kernel, much of the iMX6 support for the Vivante GPU, IPU, and VPU is missing in the 4.4 kernel.&amp;nbsp; I located an iMX6 kernel at&amp;nbsp; &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://github.com/patrykk/linux-udoo.git" rel="nofollow"&gt;https://github.com/patrykk/linux-udoo.git&lt;/A&gt;&lt;SPAN&gt;, however I haven't had much luck getting the 5.0.11.p7.1-hfp imx-gpu-viv OpenGL libraries working with this kernel.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does Freescale have any plans to release updates for the 4.4 LTS kernel or to backport a more reliable PCIe driver back to the 3.14 kernel?&amp;nbsp; Are there updated Vivante OpenGL drivers which can run with a 4.4 kernel?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan Olson&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Feb 2016 04:25:05 GMT</pubDate>
    <dc:creator>jonathanolson</dc:creator>
    <dc:date>2016-02-24T04:25:05Z</dc:date>
    <item>
      <title>Linux iMX6 PCIe driver, Linux 4.4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-iMX6-PCIe-driver-Linux-4-4/m-p/676429#M104326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even though the Hummingboard does not use an external PCIe clock, it seems that this issue isn't a clocking problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After discussing this issue with SolidRun, they suggested testing the VMX-200 PCIe video card with the PCIe driver in latest Linux 4.4 kernel.&amp;nbsp;&amp;nbsp; Sure enough, the card initializes correctly with the 4.4 PCIe driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Although the PCIe support seems much improved in the 4.4 kernel, much of the iMX6 support for the Vivante GPU, IPU, and VPU is missing in the 4.4 kernel.&amp;nbsp; I located an iMX6 kernel at&amp;nbsp; &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://github.com/patrykk/linux-udoo.git" rel="nofollow"&gt;https://github.com/patrykk/linux-udoo.git&lt;/A&gt;&lt;SPAN&gt;, however I haven't had much luck getting the 5.0.11.p7.1-hfp imx-gpu-viv OpenGL libraries working with this kernel.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does Freescale have any plans to release updates for the 4.4 LTS kernel or to backport a more reliable PCIe driver back to the 3.14 kernel?&amp;nbsp; Are there updated Vivante OpenGL drivers which can run with a 4.4 kernel?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan Olson&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Feb 2016 04:25:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-iMX6-PCIe-driver-Linux-4-4/m-p/676429#M104326</guid>
      <dc:creator>jonathanolson</dc:creator>
      <dc:date>2016-02-24T04:25:05Z</dc:date>
    </item>
    <item>
      <title>Re: Linux iMX6 PCIe driver, Linux 4.4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-iMX6-PCIe-driver-Linux-4-4/m-p/676430#M104327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; You may try using the following. &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;&amp;lt; &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Flgfiles%2FNMG%2FMAD%2FYOCTO%2Fimx-gpu-viv-5.0.11.p8.4-hfp.bin" rel="nofollow" target="_blank"&gt;http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-gpu-viv-5.0.11.p8.4-hfp.bin&lt;/A&gt;&lt;SPAN&gt; &amp;gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329918"&gt;GPU Driver and Tools&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Linux 4.9 is expected soon.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jun 2017 06:38:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-iMX6-PCIe-driver-Linux-4-4/m-p/676430#M104327</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-06-28T06:38:38Z</dc:date>
    </item>
  </channel>
</rss>