<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Kernel Version for iMX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Version-for-iMX6/m-p/675809#M104206</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it may be difficult to define a best version. Naturally the newest version should be the best option, but there are always patches required, then after some time the latest version is released it becomes stable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that there are BSPs for i.MX processors developed by NXP and there are also BSPs created by a community external to NXP such as the one you are referring to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can find the NXP BSPs releases here: git.freescale.com &amp;gt; fsl-arm-yocto-bsp.git&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;On the other hand the BSPs releases developed by the external community can be found here: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fgithub.com%2FFreescale%2F" rel="nofollow" target="_blank"&gt;https://github.com/Freescale/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using a board based on our Reference Designs and Evaluation Boards you may use our BSP, in this case &lt;A href="http://git.freescale.com/git/cgit.cgi/imx/fsl-arm-yocto-bsp.git/log/?h=imx-4.1-krogoth"&gt;imx-4.1-krogoth&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But if you are using a custom board and it is not based on our reference Designs you may use a BSP developed by the community, in this case branch Morty would be the indicated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;just please be aware that NXP provides support of the BSPs developed by NXP, but unfortunately the releases of the external community are out of our scope.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Jun 2017 20:28:43 GMT</pubDate>
    <dc:creator>Carlos_Musich</dc:creator>
    <dc:date>2017-06-05T20:28:43Z</dc:date>
    <item>
      <title>Kernel Version for iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Version-for-iMX6/m-p/675808#M104205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Freescale has several kernel versions that support iMX6. &amp;nbsp;What is the best kernel version to use as far as support for iMX6 features?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jun 2017 16:39:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Version-for-iMX6/m-p/675808#M104205</guid>
      <dc:creator>richogrady</dc:creator>
      <dc:date>2017-06-05T16:39:53Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel Version for iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Version-for-iMX6/m-p/675809#M104206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it may be difficult to define a best version. Naturally the newest version should be the best option, but there are always patches required, then after some time the latest version is released it becomes stable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that there are BSPs for i.MX processors developed by NXP and there are also BSPs created by a community external to NXP such as the one you are referring to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can find the NXP BSPs releases here: git.freescale.com &amp;gt; fsl-arm-yocto-bsp.git&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;On the other hand the BSPs releases developed by the external community can be found here: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fgithub.com%2FFreescale%2F" rel="nofollow" target="_blank"&gt;https://github.com/Freescale/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using a board based on our Reference Designs and Evaluation Boards you may use our BSP, in this case &lt;A href="http://git.freescale.com/git/cgit.cgi/imx/fsl-arm-yocto-bsp.git/log/?h=imx-4.1-krogoth"&gt;imx-4.1-krogoth&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But if you are using a custom board and it is not based on our reference Designs you may use a BSP developed by the community, in this case branch Morty would be the indicated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;just please be aware that NXP provides support of the BSPs developed by NXP, but unfortunately the releases of the external community are out of our scope.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jun 2017 20:28:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Version-for-iMX6/m-p/675809#M104206</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-06-05T20:28:43Z</dc:date>
    </item>
  </channel>
</rss>