<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPI interface with IMX6 solo processor in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPI-interface-with-IMX6-solo-processor/m-p/675337#M104152</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one can refer to the link as below&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/808351?commentID=808351#comment-808351" title="https://community.nxp.com/message/808351?commentID=808351#comment-808351"&gt;https://community.nxp.com/message/808351?commentID=808351#comment-808351&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Jun 2017 07:39:25 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2017-06-06T07:39:25Z</dc:date>
    <item>
      <title>SPI interface with IMX6 solo processor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-interface-with-IMX6-solo-processor/m-p/675336#M104151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to interface MCP2515 (CAN Controller) with IMX6 solo processor via SPI .&lt;/P&gt;&lt;P&gt;what is the procedure to do this?&lt;/P&gt;&lt;P&gt;Can anyone help me on this ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jun 2017 07:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-interface-with-IMX6-solo-processor/m-p/675336#M104151</guid>
      <dc:creator>subhashreechand</dc:creator>
      <dc:date>2017-06-05T07:12:52Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface with IMX6 solo processor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-interface-with-IMX6-solo-processor/m-p/675337#M104152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one can refer to the link as below&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/808351?commentID=808351#comment-808351" title="https://community.nxp.com/message/808351?commentID=808351#comment-808351"&gt;https://community.nxp.com/message/808351?commentID=808351#comment-808351&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jun 2017 07:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-interface-with-IMX6-solo-processor/m-p/675337#M104152</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-06-06T07:39:25Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface with IMX6 solo processor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-interface-with-IMX6-solo-processor/m-p/675338#M104153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Joan Xie , &lt;/P&gt;&lt;P&gt;Thanks for the reply .&lt;/P&gt;&lt;P&gt;But that post speaks about the Kernel version.&lt;/P&gt;&lt;P&gt;I am trying to write the &amp;nbsp;code , build it and copy&amp;nbsp;the bin &amp;nbsp;to the SD card and then flash the bin to the processor.&lt;/P&gt;&lt;P&gt;My question : what are the steps to code to make the MCP2515 transmit/receive a CAN signal to the i.MX6 SoloX processor ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2017 12:32:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-interface-with-IMX6-solo-processor/m-p/675338#M104153</guid>
      <dc:creator>subhashreechand</dc:creator>
      <dc:date>2017-06-14T12:32:19Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface with IMX6 solo processor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-interface-with-IMX6-solo-processor/m-p/675339#M104154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.mx6 SoloX has a built in CAN controller (Flexcan) so using the MCP2515 is overkill. You can use a CAN transceiver eg SN65HVD232 with Flexcan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2017 13:12:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-interface-with-IMX6-solo-processor/m-p/675339#M104154</guid>
      <dc:creator>mtx512</dc:creator>
      <dc:date>2017-06-14T13:12:26Z</dc:date>
    </item>
  </channel>
</rss>