<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Can Raw Nand Flash be programmed using JTAG programmer</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-Raw-Nand-Flash-be-programmed-using-JTAG-programmer/m-p/674990#M104060</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I checked the section 1.4.1 , it mentions the case of debugging uboot using JTAG . But my question is , can I program the uboot&amp;nbsp; over the Raw Nand Flash using JTAG programmer ? Please suggest.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 May 2017 06:46:31 GMT</pubDate>
    <dc:creator>adityanagal</dc:creator>
    <dc:date>2017-05-11T06:46:31Z</dc:date>
    <item>
      <title>Can Raw Nand Flash be programmed using JTAG programmer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Raw-Nand-Flash-be-programmed-using-JTAG-programmer/m-p/674988#M104058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working over IMX6solo based target board. In my desing IMX6 is connected to the Raw Nand Flash over GPMI interface. Can we program the Raw Nand FLash using JTAG programmer. Please suggest.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 May 2017 15:14:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Raw-Nand-Flash-be-programmed-using-JTAG-programmer/m-p/674988#M104058</guid>
      <dc:creator>adityanagal</dc:creator>
      <dc:date>2017-05-10T15:14:35Z</dc:date>
    </item>
    <item>
      <title>Re: Can Raw Nand Flash be programmed using JTAG programmer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Raw-Nand-Flash-be-programmed-using-JTAG-programmer/m-p/674989#M104059</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer chapter 1.4.1 "Using JTAG Tool for Debugging" of i.MX BSP Porting Guide I attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 May 2017 03:49:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Raw-Nand-Flash-be-programmed-using-JTAG-programmer/m-p/674989#M104059</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-05-11T03:49:56Z</dc:date>
    </item>
    <item>
      <title>Re: Can Raw Nand Flash be programmed using JTAG programmer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Raw-Nand-Flash-be-programmed-using-JTAG-programmer/m-p/674990#M104060</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I checked the section 1.4.1 , it mentions the case of debugging uboot using JTAG . But my question is , can I program the uboot&amp;nbsp; over the Raw Nand Flash using JTAG programmer ? Please suggest.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 May 2017 06:46:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Raw-Nand-Flash-be-programmed-using-JTAG-programmer/m-p/674990#M104060</guid>
      <dc:creator>adityanagal</dc:creator>
      <dc:date>2017-05-11T06:46:31Z</dc:date>
    </item>
    <item>
      <title>Re: Can Raw Nand Flash be programmed using JTAG programmer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Raw-Nand-Flash-be-programmed-using-JTAG-programmer/m-p/674991#M104061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You can use a JTAG debugger for flashing as much as You have an application, that can be &lt;BR /&gt;loaded to i.MX6 target and run there (using JTAG).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 May 2017 06:37:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Raw-Nand-Flash-be-programmed-using-JTAG-programmer/m-p/674991#M104061</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-05-16T06:37:58Z</dc:date>
    </item>
    <item>
      <title>Re: Can Raw Nand Flash be programmed using JTAG programmer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Raw-Nand-Flash-be-programmed-using-JTAG-programmer/m-p/674992#M104062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Yuri , &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I really doubt that we can directly program the Raw Nand Flash using the JTAG. As the Raw Nand is interfaced with the Nand Controller of the IMX6 processor. We cannot write anything on the Raw Nand Flash unless Nand Controller is properly initialized. Flashing application over IMX6 and Flashing over Nand&amp;nbsp; using JTAG is a different thing .&amp;nbsp; Please correct me if I am wrong. Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 May 2017 08:09:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Raw-Nand-Flash-be-programmed-using-JTAG-programmer/m-p/674992#M104062</guid>
      <dc:creator>adityanagal</dc:creator>
      <dc:date>2017-05-16T08:09:55Z</dc:date>
    </item>
    <item>
      <title>Re: Can Raw Nand Flash be programmed using JTAG programmer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Raw-Nand-Flash-be-programmed-using-JTAG-programmer/m-p/674993#M104063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; You are right, we have no a host application, that can write the flash directly via JTAG.&lt;/P&gt;&lt;P&gt;I meant, it is possible to init the i.MX6 system via JTAG debugger and run special (target)&lt;/P&gt;&lt;P&gt;application to flash the NAND in the same manner as, say, bare metal code for i.MX6 can run&lt;/P&gt;&lt;P&gt;under JTAG debugger. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 May 2017 08:33:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Raw-Nand-Flash-be-programmed-using-JTAG-programmer/m-p/674993#M104063</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-05-16T08:33:24Z</dc:date>
    </item>
  </channel>
</rss>