<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RS232 connection not working in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RS232-connection-not-working/m-p/196043#M10406</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've just received the i.MX53 QSB board. I've inserted the supplied SD card, and RS232 cable and power up the board. I can see uboot booting and counting down 3s before booting up the kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately I can't prevent uboot from booting the kernel as uboot doesn't accept any input from my keyboard. I'm using minicom. I'm sure my connection to PC is working fine as if I just swap the 53QSB board for a i.mx51 EVK it works as it should.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The same happens if I let the kernel boot up. When it comes to entering the username and password I just can't enter anything through the RS232 connection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this a know issue with i.mx53QSB ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Marko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Dec 2011 09:08:45 GMT</pubDate>
    <dc:creator>MarkoPanger</dc:creator>
    <dc:date>2011-12-15T09:08:45Z</dc:date>
    <item>
      <title>RS232 connection not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RS232-connection-not-working/m-p/196043#M10406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've just received the i.MX53 QSB board. I've inserted the supplied SD card, and RS232 cable and power up the board. I can see uboot booting and counting down 3s before booting up the kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately I can't prevent uboot from booting the kernel as uboot doesn't accept any input from my keyboard. I'm using minicom. I'm sure my connection to PC is working fine as if I just swap the 53QSB board for a i.mx51 EVK it works as it should.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The same happens if I let the kernel boot up. When it comes to entering the username and password I just can't enter anything through the RS232 connection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this a know issue with i.mx53QSB ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Marko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 09:08:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RS232-connection-not-working/m-p/196043#M10406</guid>
      <dc:creator>MarkoPanger</dc:creator>
      <dc:date>2011-12-15T09:08:45Z</dc:date>
    </item>
    <item>
      <title>Re: RS232 connection not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RS232-connection-not-working/m-p/196044#M10407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Got it working. It was a soldering problem on the connector. Thank, Marko.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 09:49:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RS232-connection-not-working/m-p/196044#M10407</guid>
      <dc:creator>MarkoPanger</dc:creator>
      <dc:date>2011-12-15T09:49:32Z</dc:date>
    </item>
    <item>
      <title>Re: RS232 connection not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RS232-connection-not-working/m-p/196045#M10408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The RS232 interface on the QSB should work in both directions. You should check that you've got the right RS232 cable and that minicom is configured correctly - in particular there's no hardware handshaking.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 09:54:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RS232-connection-not-working/m-p/196045#M10408</guid>
      <dc:creator>AlanLevy</dc:creator>
      <dc:date>2011-12-15T09:54:42Z</dc:date>
    </item>
  </channel>
</rss>