<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックproblem with MAC57D54 interrupt receive in UART</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-MAC57D54-interrupt-receive-in-UART/m-p/673865#M103843</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I use PC communicate with MAC57D54 through UART ,the MAC57D54 can transmit&lt;BR /&gt;message to PC but can't receive message from PC by interrupt .can you help me about it and &lt;BR /&gt;Do you have a Example_code about MAC57D54 receive message by interrupt use USART .Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 May 2017 09:13:29 GMT</pubDate>
    <dc:creator>gqzhang</dc:creator>
    <dc:date>2017-05-10T09:13:29Z</dc:date>
    <item>
      <title>problem with MAC57D54 interrupt receive in UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-MAC57D54-interrupt-receive-in-UART/m-p/673865#M103843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I use PC communicate with MAC57D54 through UART ,the MAC57D54 can transmit&lt;BR /&gt;message to PC but can't receive message from PC by interrupt .can you help me about it and &lt;BR /&gt;Do you have a Example_code about MAC57D54 receive message by interrupt use USART .Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 May 2017 09:13:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problem-with-MAC57D54-interrupt-receive-in-UART/m-p/673865#M103843</guid>
      <dc:creator>gqzhang</dc:creator>
      <dc:date>2017-05-10T09:13:29Z</dc:date>
    </item>
    <item>
      <title>Re: problem with MAC57D54 interrupt receive in UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-MAC57D54-interrupt-receive-in-UART/m-p/673866#M103844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;You are using the MAC57D54, you should create thread in the &lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/community/s32/s32ds/content" title="https://community.nxp.com/community/s32/s32ds/content"&gt;S32 Design Studio&lt;/A&gt; community. Here is i.MX community, so no support for MAC57D54.&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Rita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 May 2017 08:42:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problem-with-MAC57D54-interrupt-receive-in-UART/m-p/673866#M103844</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2017-05-12T08:42:20Z</dc:date>
    </item>
  </channel>
</rss>