<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIssues with serial on iMX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issues-with-serial-on-iMX6/m-p/673823#M103830</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello we use&amp;nbsp;iMX6DP4AVT1AA &amp;nbsp;devices in a hardware setup running on windows7 32bit&amp;nbsp;and libusbx-1.0.15-win&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We face some problems on the serial hardware, where we have a FTDI232RL + 3.3V level translation &amp;nbsp;to comunicate with the iMX chip &amp;nbsp;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sometimes the test system fails when waiting &amp;nbsp;for &amp;nbsp;iMX boot console response.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any hardware alternative to ftdi232rl chip for comunication with imx?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We tryied a alternative using the native COM1 &amp;nbsp;via a max232 + optical isolation and level translation, but the results where worst&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any sugestions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 May 2017 04:54:53 GMT</pubDate>
    <dc:creator>bogdananton</dc:creator>
    <dc:date>2017-05-10T04:54:53Z</dc:date>
    <item>
      <title>Issues with serial on iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issues-with-serial-on-iMX6/m-p/673823#M103830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello we use&amp;nbsp;iMX6DP4AVT1AA &amp;nbsp;devices in a hardware setup running on windows7 32bit&amp;nbsp;and libusbx-1.0.15-win&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We face some problems on the serial hardware, where we have a FTDI232RL + 3.3V level translation &amp;nbsp;to comunicate with the iMX chip &amp;nbsp;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sometimes the test system fails when waiting &amp;nbsp;for &amp;nbsp;iMX boot console response.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any hardware alternative to ftdi232rl chip for comunication with imx?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We tryied a alternative using the native COM1 &amp;nbsp;via a max232 + optical isolation and level translation, but the results where worst&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any sugestions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 May 2017 04:54:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issues-with-serial-on-iMX6/m-p/673823#M103830</guid>
      <dc:creator>bogdananton</dc:creator>
      <dc:date>2017-05-10T04:54:53Z</dc:date>
    </item>
    <item>
      <title>Re: Issues with serial on iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issues-with-serial-on-iMX6/m-p/673824#M103831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi bogdan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from i.MX6 side there are no restrictions, one can use any rs232&lt;/P&gt;&lt;P&gt;converter or USB to serial UART interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 May 2017 07:57:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issues-with-serial-on-iMX6/m-p/673824#M103831</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-05-10T07:57:04Z</dc:date>
    </item>
  </channel>
</rss>