<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX7 Wi-Fi Support in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Wi-Fi-Support/m-p/673812#M103827</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, it is not possible to configure the WiFi interface of the Variscite iMX7 SoM the way you describe.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Jun 2017 11:36:14 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2017-06-28T11:36:14Z</dc:date>
    <item>
      <title>i.MX7 Wi-Fi Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Wi-Fi-Support/m-p/673811#M103826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For the Variscite iMX7 SoM, can the Wi-fi be configured to work in AP+station mode? .&lt;/P&gt;&lt;P&gt;ie it can act as access point and simultaneously connect to other access point.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2017 12:17:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Wi-Fi-Support/m-p/673811#M103826</guid>
      <dc:creator>sourabhzunke090</dc:creator>
      <dc:date>2017-06-26T12:17:40Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7 Wi-Fi Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Wi-Fi-Support/m-p/673812#M103827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, it is not possible to configure the WiFi interface of the Variscite iMX7 SoM the way you describe.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jun 2017 11:36:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Wi-Fi-Support/m-p/673812#M103827</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-06-28T11:36:14Z</dc:date>
    </item>
  </channel>
</rss>