<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Kernel starting problem in imx6q custom board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-starting-problem-in-imx6q-custom-board/m-p/673124#M103723</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check boundary devices&amp;nbsp;imx6q-nitrogen6_max dts files&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.1.15_2.0.0_ga/arch/arm/boot/dts/imx6q-nitrogen6_max.dts" title="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.1.15_2.0.0_ga/arch/arm/boot/dts/imx6q-nitrogen6_max.dts"&gt;linux-imx6/imx6q-nitrogen6_max.dts at boundary-imx_4.1.15_2.0.0_ga · boundarydevices/linux-imx6 · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 25 Jun 2017 22:53:24 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-06-25T22:53:24Z</dc:date>
    <item>
      <title>Kernel starting problem in imx6q custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-starting-problem-in-imx6q-custom-board/m-p/673123#M103722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is regarding imx6q based custom hardware design and it boot from flash correctly and when it start the kernel shows the following error messages.&lt;/P&gt;&lt;P&gt;I have done the changes to all the imx6qdl.dtsi, imx6qd.dtsi and etc files and compiled and generated the dtb file as well. &lt;STRONG&gt;Could you please tell me the reason for following error messages.&lt;/STRONG&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;----------- trying to load /initrd.img&lt;BR /&gt;6556084 bytes read in 637 ms (9.8 MiB/s)&lt;BR /&gt;5791064 bytes read in 663 ms (8.3 MiB/s)&lt;BR /&gt;Kernel image @ 0x10800000 [ 0x000000 - 0x585d58 ]&lt;BR /&gt;## Flattened Device Tree blob at 13000000&lt;BR /&gt; Booting using the fdt blob at 0x13000000&lt;BR /&gt; reserving fdt memory region: addr=13000000 size=b000&lt;BR /&gt; Using Device Tree in place at 13000000, end 1300dfff&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/iomuxc-imx6q-nitrogen6-maxgrp/audmuxgrp&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/iomuxc-imx6q-nitrogen6-maxgrp/hoggrp&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/iomuxc-imx6q-nitrogen6-maxgrp/i2c1-sgtl5000grp&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/iomuxc-imx6q-nitrogen6-maxgrp/i2c2muxgrp&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/iomuxc-imx6q-nitrogen6-maxgrp/i2c3muxgrp&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: no fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/iomuxc-imx6q-nitrogen6-maxgrp/i2c3-ov5640grp&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/iomuxc-imx6q-nitrogen6-maxgrp/reg-wlan-engrp&lt;BR /&gt;i2c-mux-gpio i2cmux@2: Missing mux-gpios property in the DT.&lt;BR /&gt;i2c-mux-gpio i2cmux@3: Missing mux-gpios property in the DT.&lt;BR /&gt;ldb 2000000.aips-bus:ldb@020e0008: failed to find valid LVDS channel&lt;BR /&gt;m25p80 spi0.0: unrecognized JEDEC id bytes: bf, 26, 42&lt;BR /&gt;imx-sgtl5000 sound: ASoC: CODEC DAI sgtl5000 not registered&lt;BR /&gt;imx-sgtl5000 sound: snd_soc_register_card failed (-517)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Jun 2017 06:08:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-starting-problem-in-imx6q-custom-board/m-p/673123#M103722</guid>
      <dc:creator>peteramond</dc:creator>
      <dc:date>2017-06-24T06:08:21Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel starting problem in imx6q custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-starting-problem-in-imx6q-custom-board/m-p/673124#M103723</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check boundary devices&amp;nbsp;imx6q-nitrogen6_max dts files&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.1.15_2.0.0_ga/arch/arm/boot/dts/imx6q-nitrogen6_max.dts" title="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.1.15_2.0.0_ga/arch/arm/boot/dts/imx6q-nitrogen6_max.dts"&gt;linux-imx6/imx6q-nitrogen6_max.dts at boundary-imx_4.1.15_2.0.0_ga · boundarydevices/linux-imx6 · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 25 Jun 2017 22:53:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-starting-problem-in-imx6q-custom-board/m-p/673124#M103723</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-25T22:53:24Z</dc:date>
    </item>
  </channel>
</rss>