<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FSL_shw returns error code 1 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FSL-shw-returns-error-code-1/m-p/195793#M10371</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Never mind&amp;nbsp;I got it figured out. I just needed to setup everything right, meaning load the modules.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Dec 2011 19:23:17 GMT</pubDate>
    <dc:creator>MichaelMcCarty</dc:creator>
    <dc:date>2011-12-14T19:23:17Z</dc:date>
    <item>
      <title>FSL_shw returns error code 1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FSL-shw-returns-error-code-1/m-p/195792#M10370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a custom iMX.51 board that uses the digi connect core (Wi-iMX51).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to use the sahara api and linux. I've reduced the code down to the bare minimum but it always returns a 1 which is unspecified error. I define the platform as "CONFIG_ARCH_MX5"&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;code = fsl_shw_register_user(my_ctx);&lt;/P&gt;&lt;P&gt;printf("Finished, Code: 0x%X", code);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone have a clue ?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2011 15:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FSL-shw-returns-error-code-1/m-p/195792#M10370</guid>
      <dc:creator>MichaelMcCarty</dc:creator>
      <dc:date>2011-12-14T15:37:28Z</dc:date>
    </item>
    <item>
      <title>Re: FSL_shw returns error code 1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FSL-shw-returns-error-code-1/m-p/195793#M10371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Never mind&amp;nbsp;I got it figured out. I just needed to setup everything right, meaning load the modules.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2011 19:23:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FSL-shw-returns-error-code-1/m-p/195793#M10371</guid>
      <dc:creator>MichaelMcCarty</dc:creator>
      <dc:date>2011-12-14T19:23:17Z</dc:date>
    </item>
    <item>
      <title>Re: FSL_shw returns error code 1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FSL-shw-returns-error-code-1/m-p/195794#M10372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to test sahara on imx51.&lt;/P&gt;&lt;P&gt;I referred the PDF file at below location,&lt;/P&gt;&lt;P&gt;read.pudn.com/downloads137/sourcecode/embed/588140/mx27_linux.pdf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But i am not able to get "User-Mode API Library (and test code)".&lt;/P&gt;&lt;P&gt;It is mentioned that it is located at location "LINUX2.6/misc/lib/sahara2", but i can not find it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you guide me from where can i get this test_code?&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;How can i test or use sahara driver for encryption?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Shashank.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2015 11:00:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FSL-shw-returns-error-code-1/m-p/195794#M10372</guid>
      <dc:creator>shashankpathak</dc:creator>
      <dc:date>2015-01-07T11:00:36Z</dc:date>
    </item>
  </channel>
</rss>