<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Bitbaking Linux-Wandboard ? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Bitbaking-Linux-Wandboard/m-p/672439#M103602</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello;&lt;/P&gt;&lt;P&gt;I have a made the changes on the mxc_mipi_csi2.c file to adjust right clock configuration in the&amp;nbsp; linux-wandboard&amp;nbsp; directory.&lt;/P&gt;&lt;P&gt;I think I using bitbake command ,which is&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;bitbake -c compile -f virtual/kernel then&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;then&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;bitbake -c deploy virtual/kernel&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;after that&amp;nbsp; I am using ;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;bitbake core-image-base &amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;to create my image but I think I am doing wrong , so I couldnt get the csi_mclk .&lt;/P&gt;&lt;P&gt;What am I doing wrong with this command ? Can you help me .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mustafa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Jul 2017 14:52:14 GMT</pubDate>
    <dc:creator>mustafabakircio</dc:creator>
    <dc:date>2017-07-17T14:52:14Z</dc:date>
    <item>
      <title>Bitbaking Linux-Wandboard ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bitbaking-Linux-Wandboard/m-p/672439#M103602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello;&lt;/P&gt;&lt;P&gt;I have a made the changes on the mxc_mipi_csi2.c file to adjust right clock configuration in the&amp;nbsp; linux-wandboard&amp;nbsp; directory.&lt;/P&gt;&lt;P&gt;I think I using bitbake command ,which is&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;bitbake -c compile -f virtual/kernel then&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;then&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;bitbake -c deploy virtual/kernel&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;after that&amp;nbsp; I am using ;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;bitbake core-image-base &amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;to create my image but I think I am doing wrong , so I couldnt get the csi_mclk .&lt;/P&gt;&lt;P&gt;What am I doing wrong with this command ? Can you help me .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mustafa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jul 2017 14:52:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bitbaking-Linux-Wandboard/m-p/672439#M103602</guid>
      <dc:creator>mustafabakircio</dc:creator>
      <dc:date>2017-07-17T14:52:14Z</dc:date>
    </item>
    <item>
      <title>Re: Bitbaking Linux-Wandboard ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bitbaking-Linux-Wandboard/m-p/672440#M103603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mustafa&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95003"&gt;i.MX Yocto Project: How can I (quickly) modify the kernel and test it?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jul 2017 23:23:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bitbaking-Linux-Wandboard/m-p/672440#M103603</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-17T23:23:38Z</dc:date>
    </item>
  </channel>
</rss>