<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow Do I use the V4L2 interface for video output?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195590#M10354</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One of the best sources of information and example source code for using the V4L2 interface in the Linux BSP are the unit tests provided by Freescale. &amp;nbsp;This code provides a concise example of how to accomplish basic functionalities which can be used a building blocks for your more complex use cases. The unit test source code can be accessed using the following ltib command:&lt;/P&gt;&lt;P&gt;./ltib -m prep -p imx-test&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Afterward, the source code will be located in your ltib project directory in the following location:&lt;/P&gt;&lt;P&gt;&amp;lt;ltib install dir&amp;gt;/rpm/BUILD/imx-test-&amp;lt;version&amp;gt;/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This source code contains a wealth of information that hopefully will help you shorten the time it takes to get up and running with these sometimes complicated APIs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Dec 2011 13:31:06 GMT</pubDate>
    <dc:creator>Philip_FSL</dc:creator>
    <dc:date>2011-12-13T13:31:06Z</dc:date>
    <item>
      <title>How Do I use the V4L2 interface for video output?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195590#M10354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One of the best sources of information and example source code for using the V4L2 interface in the Linux BSP are the unit tests provided by Freescale. &amp;nbsp;This code provides a concise example of how to accomplish basic functionalities which can be used a building blocks for your more complex use cases. The unit test source code can be accessed using the following ltib command:&lt;/P&gt;&lt;P&gt;./ltib -m prep -p imx-test&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Afterward, the source code will be located in your ltib project directory in the following location:&lt;/P&gt;&lt;P&gt;&amp;lt;ltib install dir&amp;gt;/rpm/BUILD/imx-test-&amp;lt;version&amp;gt;/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This source code contains a wealth of information that hopefully will help you shorten the time it takes to get up and running with these sometimes complicated APIs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2011 13:31:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195590#M10354</guid>
      <dc:creator>Philip_FSL</dc:creator>
      <dc:date>2011-12-13T13:31:06Z</dc:date>
    </item>
    <item>
      <title>Re: How Do I use the V4L2 interface for video output?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195591#M10355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you, indeed these might be useful building blocks.&lt;/P&gt;&lt;P&gt;What are the prerequisites for the graphics related test tools?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx-test-11.09.01/test/mxc_fb_test/&lt;/P&gt;&lt;P&gt;imx-test-11.09.01/test/mxc_ipudev_test/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am building the software from scratch, not running the supplied image, and would like to learn what I need to bring up in order to run these tests.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Same question for the Freescale supplied GStreamer components; do these require the X Windows to be up and running on the target?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2011 21:42:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195591#M10355</guid>
      <dc:creator>sidebranch</dc:creator>
      <dc:date>2011-12-13T21:42:18Z</dc:date>
    </item>
    <item>
      <title>Re: How Do I use the V4L2 interface for video output?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195592#M10356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For the fb test, you just need to have the framebuffer driver in the system. &amp;nbsp;For ipudev, libipu is necessary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;GStreamer does not require X Windows. &amp;nbsp;You can directly use the ipulib sink or the v4l2 sink plug-in for rendering video in a non-X environment.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 09:32:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195592#M10356</guid>
      <dc:creator>Philip_FSL</dc:creator>
      <dc:date>2011-12-15T09:32:08Z</dc:date>
    </item>
    <item>
      <title>Re: How Do I use the V4L2 interface for video output?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195593#M10357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does Freescale provide the source code for imx-test anymore? I finally found it here. Is there an official version?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/288297"&gt;https://community.freescale.com/thread/288297&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2012 02:41:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195593#M10357</guid>
      <dc:creator>fcs</dc:creator>
      <dc:date>2012-10-17T02:41:43Z</dc:date>
    </item>
    <item>
      <title>Re: How Do I use the V4L2 interface for video output?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195594#M10358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes.&amp;nbsp; Getting the source is the same process as before.&amp;nbsp; Using LTIB perform the following: ./ltib -m prep imx-test .&amp;nbsp; This will unpack the sources in the rpm/BUILD/ directory of your LTIB project.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2012 06:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195594#M10358</guid>
      <dc:creator>Philip_FSL</dc:creator>
      <dc:date>2012-10-17T06:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: How Do I use the V4L2 interface for video output?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195595#M10359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I couldn't find the source code for the unit tests anywhere in any package, is it in imx-test-11.09.01-1.arm.rpm?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ ./ltib -m prep imx-test&lt;/P&gt;&lt;P&gt;The options prep, scbuild, scinstall and scdeploy are only allowed when working&lt;/P&gt;&lt;P&gt;on a single package, not a list.&amp;nbsp; You need to supply the option -p|--pkg &amp;lt;pkg&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ ./ltib -p imx-test&lt;/P&gt;&lt;P&gt;Processing platform: Freescale iMX5x Based Boards&lt;BR /&gt;===================================================&lt;BR /&gt;using config/platform/imx/.config&lt;/P&gt;&lt;P&gt;Processing: imx-test&lt;BR /&gt;======================&lt;/P&gt;&lt;P&gt;Started: Tue Oct 16 23:23:24 2012&lt;BR /&gt;Ended:&amp;nbsp;&amp;nbsp; Tue Oct 16 23:23:27 2012&lt;BR /&gt;Elapsed: 3 seconds&lt;/P&gt;&lt;P&gt;Build Succeeded&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:lucid@ubuntu:~/Desktop/B/ltib$"&gt;lucid@ubuntu:~/Desktop/B/ltib$&lt;/A&gt; find . |grep imx-test&lt;BR /&gt;./rpm/BUILD/linux-2.6.35.3/patches/0247-ENGR00131944-Fix-imx-test-build-failure-issue-on-mx2.patch&lt;BR /&gt;./rpm/RPMS/arm/imx-test-11.09.01-1.arm.rpm&lt;BR /&gt;./dist/lfs-5.1/mxc-misc/imx-test.spec&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2012 06:27:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195595#M10359</guid>
      <dc:creator>fcs</dc:creator>
      <dc:date>2012-10-17T06:27:58Z</dc:date>
    </item>
    <item>
      <title>Re: How Do I use the V4L2 interface for video output?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195596#M10360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry about that.&amp;nbsp; There is a command line option missing: &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;./ltib -m prep -p imx-test&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2012 06:48:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195596#M10360</guid>
      <dc:creator>Philip_FSL</dc:creator>
      <dc:date>2012-10-17T06:48:35Z</dc:date>
    </item>
    <item>
      <title>Re: How Do I use the V4L2 interface for video output?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195597#M10361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, that works. I hadn't seen any documentation for that&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2012 07:29:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-Do-I-use-the-V4L2-interface-for-video-output/m-p/195597#M10361</guid>
      <dc:creator>fcs</dc:creator>
      <dc:date>2012-10-17T07:29:57Z</dc:date>
    </item>
  </channel>
</rss>