<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX233 DCDC powerUp problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX233-DCDC-powerUp-problem/m-p/195518#M10352</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is not a problem with the DC/DC or the PSU in general. It more like a problem with you partitions on the MMC&lt;/P&gt;&lt;P&gt;Attached is a file that describes how to properly set partitions on SD/MMC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, check/edit you init memory size in LTIB option&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Dec 2011 10:36:59 GMT</pubDate>
    <dc:creator>danix</dc:creator>
    <dc:date>2011-12-14T10:36:59Z</dc:date>
    <item>
      <title>iMX233 DCDC powerUp problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX233-DCDC-powerUp-problem/m-p/195517#M10351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day dear coforumer! I have a my own board based on iMX233 processor. I want to power up onboard DCDC, as more effective than linregulators. &amp;nbsp;Bootlets source code has been corrected &amp;nbsp;in&amp;nbsp; the way which errata recommends. So, my board is bootable now, but it's work unstable,a lot of times it stops on the linux boot stage. And another one it doesn't work on frequencies higher than 320 Mhz (((. &lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;My current bootlets version is 10.12.01. Any suggestion. Thanks a lot, earlier)) &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;Linux BootLog&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;PowerPrep start initialize power...&lt;/P&gt;&lt;P&gt;Configured for 5v only power source. Battery powered operation disabled.&lt;/P&gt;&lt;P&gt;--------------POWER---------------------&lt;/P&gt;&lt;P&gt;HW_POWER_CTRL 0x00019024&lt;/P&gt;&lt;P&gt;HW_POWER_5VCTRL 0x0003F003&lt;/P&gt;&lt;P&gt;HW_POWER_MINPWR 0x00000020&lt;/P&gt;&lt;P&gt;HW_POWER_CHARGE 0x00410000&lt;/P&gt;&lt;P&gt;HW_POWER_VDDDCTRL 0x00020710&lt;/P&gt;&lt;P&gt;HW_POWER_VDDACTRL 0x0000270A&lt;/P&gt;&lt;P&gt;HW_POWER_VDDIOCTRL 0x00002614&lt;/P&gt;&lt;P&gt;HW_POWER_VDDMEMCTRL 0x0000020C&lt;/P&gt;&lt;P&gt;HW_POWER_DCDC4P2 0xC0C00000&lt;/P&gt;&lt;P&gt;HW_POWER_MISC 0x00000000&lt;/P&gt;&lt;P&gt;HW_POWER_DCLIMITS 0x0000305F&lt;/P&gt;&lt;P&gt;HW_POWER_LOOPCTRL 0x00167021&lt;/P&gt;&lt;P&gt;HW_POWER_STS 0x20038A2E&lt;/P&gt;&lt;P&gt;HW_POWER_SPEED 0x00F40000&lt;/P&gt;&lt;P&gt;HW_POWER_BATTMONITOR 0x0000060F&lt;/P&gt;&lt;P&gt;HW_POWER_RESET 0x3E770000&lt;/P&gt;&lt;P&gt;HW_POWER_DEBUG 0x00000000&lt;/P&gt;&lt;P&gt;HW_POWER_SPECIAL 0x00000000&lt;/P&gt;&lt;P&gt;HW_POWER_VERSION 0x03010000&lt;/P&gt;&lt;P&gt;------------------------------------------&lt;/P&gt;&lt;P&gt;----------------LRADC-------------------&lt;/P&gt;&lt;P&gt;HW_LRADC_CTRL0 0x00000000&lt;/P&gt;&lt;P&gt;HW_LRADC_CTRL1 0x00000080&lt;/P&gt;&lt;P&gt;HW_LRADC_CTRL2 0x00008000&lt;/P&gt;&lt;P&gt;HW_LRADC_CTRL3 0x00000000&lt;/P&gt;&lt;P&gt;HW_LRADC_CTRL4 0x76543210&lt;/P&gt;&lt;P&gt;HW_LRADC_STATUS 0x07FF0000&lt;/P&gt;&lt;P&gt;HW_LRADC_CH6 0x00000000&lt;/P&gt;&lt;P&gt;HW_LRADC_CH7 0x000007AB&lt;/P&gt;&lt;P&gt;HW_LRADC_DELAY0 0x00000000&lt;/P&gt;&lt;P&gt;HW_LRADC_DELAY1 0x00000000&lt;/P&gt;&lt;P&gt;HW_LRADC_DELAY2 0x00000000&lt;/P&gt;&lt;P&gt;HW_LRADC_DELAY3 0x80180064&lt;/P&gt;&lt;P&gt;HW_LRADC_CONVERSION 0x000201C1&lt;/P&gt;&lt;P&gt;------------------------------------------&lt;/P&gt;&lt;P&gt;-------------CLK-----------------------&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_PLLCTRL0 0x00000000&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_PLLCTRL1 0x00000000&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_CPU 0x00010001&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_HBUS 0x00000001&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_XBUS 0x00000001&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_XTAL 0x70000001&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_SSP 0x00000001&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_GPMI 0x80000001&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_EMI 0x80000101&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_SAIF 0x80000001&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_FRAC 0x92929292&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_FRAC1 0x80000000&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_CLKSEQ 0x000001FB&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_RESET 0x00000000&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_STATUS 0x00000000&lt;/P&gt;&lt;P&gt;HW_CLKCTRL_VERSION 0x04000000&lt;/P&gt;&lt;P&gt;------------------------------------------&lt;/P&gt;&lt;P&gt;LLCDec 13 201107:32:16&lt;/P&gt;&lt;P&gt;EMI_CTRL 0x1C084040&lt;/P&gt;&lt;P&gt;FRAC 0x92926192&lt;/P&gt;&lt;P&gt;init_ddr_mt46v32m16_133Mhz&lt;/P&gt;&lt;P&gt;power 0x00020710&lt;/P&gt;&lt;P&gt;Frac 0x92926192&lt;/P&gt;&lt;P&gt;start change cpu freq&lt;/P&gt;&lt;P&gt;hbus 0x00000003&lt;/P&gt;&lt;P&gt;cpu 0x00010001&lt;/P&gt;&lt;P&gt;LLLLLLLFCLJUncompressing Linux... done, booting the kernel.&lt;/P&gt;&lt;P&gt;Linux version 2.6.35.3 (root@abk-d23) (gcc version 4.3.3 (GCC) ) #3 PREEMPT Thu Nov 17 10:15:06 EET 2011&lt;/P&gt;&lt;P&gt;CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177&lt;/P&gt;&lt;P&gt;CPU: VIVT data cache, VIVT instruction cache&lt;/P&gt;&lt;P&gt;Machine: Freescale MX23EVK board&lt;/P&gt;&lt;P&gt;Memory policy: ECC disabled, Data cache writeback&lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on. Total pages: 16256&lt;/P&gt;&lt;P&gt;Kernel command line: console=ttyAM0,115200 ssp1=spi1 ssp2=mmc root=/dev/mmcblk0p2 rootwait&lt;/P&gt;&lt;P&gt;PID hash table entries: 256 (order: -2, 1024 bytes)&lt;/P&gt;&lt;P&gt;Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)&lt;/P&gt;&lt;P&gt;Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;Memory: 64MB = 64MB total&lt;/P&gt;&lt;P&gt;Memory: 60864k/60864k available, 4672k reserved, 0K highmem&lt;/P&gt;&lt;P&gt;Virtual kernel memory layout:&lt;/P&gt;&lt;P&gt;vector : 0xffff0000 - 0xffff1000 ( 4 kB)&lt;/P&gt;&lt;P&gt;fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)&lt;/P&gt;&lt;P&gt;DMA : 0xfde00000 - 0xffe00000 ( 32 MB)&lt;/P&gt;&lt;P&gt;vmalloc : 0xc4800000 - 0xf0000000 ( 696 MB)&lt;/P&gt;&lt;P&gt;lowmem : 0xc0000000 - 0xc4000000 ( 64 MB)&lt;/P&gt;&lt;P&gt;modules : 0xbf000000 - 0xc0000000 ( 16 MB)&lt;/P&gt;&lt;P&gt;.init : 0xc0008000 - 0xc0026000 ( 120 kB)&lt;/P&gt;&lt;P&gt;.text : 0xc0026000 - 0xc03bf000 (3684 kB)&lt;/P&gt;&lt;P&gt;.data : 0xc03c0000 - 0xc03ecb00 ( 179 kB)&lt;/P&gt;&lt;P&gt;SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1&lt;/P&gt;&lt;P&gt;Hierarchical RCU implementation.&lt;/P&gt;&lt;P&gt;RCU-based detection of stalled CPUs is disabled.&lt;/P&gt;&lt;P&gt;Verbose stalled-CPUs detection is disabled.&lt;/P&gt;&lt;P&gt;NR_IRQS:224&lt;/P&gt;&lt;P&gt;Console: colour dummy device 80x30&lt;/P&gt;&lt;P&gt;console [ttyAM0] enabled&lt;/P&gt;&lt;P&gt;Calibrating delay loop... 143.36 BogoMIPS (lpj=716800)&lt;/P&gt;&lt;P&gt;pid_max: default: 32768 minimum: 301&lt;/P&gt;&lt;P&gt;Mount-cache hash table entries: 512&lt;/P&gt;&lt;P&gt;CPU: Testing write buffer coherency: ok&lt;/P&gt;&lt;P&gt;regulator: core version 0.5&lt;/P&gt;&lt;P&gt;regulator: dummy:&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 16&lt;/P&gt;&lt;P&gt;regulator: vddd: 800 &amp;lt;--&amp;gt; 1575 mV at 1550 mV fast normal&lt;/P&gt;&lt;P&gt;regulator: vdddbo: 800 &amp;lt;--&amp;gt; 1575 mV fast normal&lt;/P&gt;&lt;P&gt;regulator: vdda: 1500 &amp;lt;--&amp;gt; 2275 mV at 1750 mV fast normal&lt;/P&gt;&lt;P&gt;regulator: vddio: 2800 &amp;lt;--&amp;gt; 3575 mV at 3300 mV fast normal&lt;/P&gt;&lt;P&gt;regulator: overall_current: fast normal&lt;/P&gt;&lt;P&gt;regulator: mxs-duart-1: fast normal&lt;/P&gt;&lt;P&gt;regulator: mxs-bl-1: fast normal&lt;/P&gt;&lt;P&gt;regulator: mxs-i2c-1: fast normal&lt;/P&gt;&lt;P&gt;regulator: mmc_ssp-1: fast normal&lt;/P&gt;&lt;P&gt;regulator: mmc_ssp-2: fast normal&lt;/P&gt;&lt;P&gt;regulator: charger-1: fast normal&lt;/P&gt;&lt;P&gt;regulator: power-test-1: fast normal&lt;/P&gt;&lt;P&gt;regulator: cpufreq-1: fast normal&lt;/P&gt;&lt;P&gt;i.MX IRAM pool: 28 KB@0xc4808000&lt;/P&gt;&lt;P&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;/P&gt;&lt;P&gt;SCSI subsystem initialized&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbfs&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver hub&lt;/P&gt;&lt;P&gt;usbcore: registered new device driver usb&lt;/P&gt;&lt;P&gt;Advanced Linux Sound Architecture Driver Version 1.0.23.&lt;/P&gt;&lt;P&gt;Switching to clocksource mxs clock source&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 2&lt;/P&gt;&lt;P&gt;IP route cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;/P&gt;&lt;P&gt;TCP established hash table entries: 2048 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;TCP bind hash table entries: 2048 (order: 1, 8192 bytes)&lt;/P&gt;&lt;P&gt;TCP: Hash tables configured (established 2048 bind 2048)&lt;/P&gt;&lt;P&gt;TCP reno registered&lt;/P&gt;&lt;P&gt;UDP hash table entries: 256 (order: 0, 4096 bytes)&lt;/P&gt;&lt;P&gt;UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 1&lt;/P&gt;&lt;P&gt;Bus freq driver module loaded&lt;/P&gt;&lt;P&gt;WARNING : No battery connected !&lt;/P&gt;&lt;P&gt;Aborting power driver initialization&lt;/P&gt;&lt;P&gt;mxs-battery: probe of mxs-battery.0 failed with error 1&lt;/P&gt;&lt;P&gt;mxs_cpu_init: cpufreq init finished&lt;/P&gt;&lt;P&gt;msgmni has been set to 118&lt;/P&gt;&lt;P&gt;alg: No test for stdrng (krng)&lt;/P&gt;&lt;P&gt;cryptodev: driver loaded.&lt;/P&gt;&lt;P&gt;io scheduler noop registered&lt;/P&gt;&lt;P&gt;io scheduler cfq registered (default)&lt;/P&gt;&lt;P&gt;Console: switching to colour frame buffer device 90x30&lt;/P&gt;&lt;P&gt;mxs-duart.0: ttyAM0 at MMIO 0x80070000 (irq = 0) is a DebugUART&lt;/P&gt;&lt;P&gt;brd: module loaded&lt;/P&gt;&lt;P&gt;loop: module loaded&lt;/P&gt;&lt;P&gt;ssp_set_rate: error -110&lt;/P&gt;&lt;P&gt;mxs-spi mxs-spi.0: Max possible speed 96000 = 96000000/2 kHz&lt;/P&gt;&lt;P&gt;mxs-spi mxs-spi.0: at 0x80010000 mapped to 0xF0010000, irq=14, bus 1, DMA ver_major 3&lt;/P&gt;&lt;P&gt;ks8851 spi1.0: message enable is 0&lt;/P&gt;&lt;P&gt;ks8851 spi1.0: eth0: revision 1, MAC 72:db:d7:5d:8c:cf, IRQ 195&lt;/P&gt;&lt;P&gt;tun: Universal TUN/TAP device driver, 1.6&lt;/P&gt;&lt;P&gt;tun: (C) 1999-2004 Max Krasnyansky &amp;lt;maxk@qualcomm.com&amp;gt;&lt;/P&gt;&lt;P&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci: Freescale On-Chip EHCI Host Controller&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci: new USB bus registered, assigned bus number 1&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci: irq 11, io base 0x80080000&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci: USB 2.0 started, EHCI 1.00&lt;/P&gt;&lt;P&gt;hub 1-0:1.0: USB hub found&lt;/P&gt;&lt;P&gt;hub 1-0:1.0: 1 port detected&lt;/P&gt;&lt;P&gt;Initializing USB Mass Storage driver...&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usb-storage&lt;/P&gt;&lt;P&gt;USB Mass Storage support registered.&lt;/P&gt;&lt;P&gt;i2c /dev entries driver&lt;/P&gt;&lt;P&gt;Linux video capture interface: v2.00&lt;/P&gt;&lt;P&gt;mxs-pxp mxs-pxp.0: initialized&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver uvcvideo&lt;/P&gt;&lt;P&gt;USB Video Class driver (v0.1.0)&lt;/P&gt;&lt;P&gt;mxs watchdog: initialized, heartbeat 19 sec&lt;/P&gt;&lt;P&gt;mxs-mmc: MXS SSP Controller MMC Interface driver&lt;/P&gt;&lt;P&gt;mxs-mmc mxs-mmc.0: mmc0: MXS SSP MMC DMAIRQ 20 ERRIRQ 15&lt;/P&gt;&lt;P&gt;dcp dcp.0: DCP crypto enabled.!&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbhid&lt;/P&gt;&lt;P&gt;usbhid: USB HID core driver&lt;/P&gt;&lt;P&gt;mxs-adc-audio mxs-adc-audio.0: MXS ADC/DAC Audio Codec&lt;/P&gt;&lt;P&gt;No device for DAI mxs adc/dac&lt;/P&gt;&lt;P&gt;No device for DAI mxs adc/dac&lt;/P&gt;&lt;P&gt;asoc: mxs adc/dac &amp;lt;-&amp;gt; mxs adc/dac mapping ok&lt;/P&gt;&lt;P&gt;ALSA device list:&lt;/P&gt;&lt;P&gt;#0: MXS EVK (mxs adc/dac)&lt;/P&gt;&lt;P&gt;IPv4 over IPv4 tunneling driver&lt;/P&gt;&lt;P&gt;ip_tables: (C) 2000-2006 Netfilter Core Team&lt;/P&gt;&lt;P&gt;TCP cubic registered&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 10&lt;/P&gt;&lt;P&gt;IPv6 over IPv4 tunneling driver&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 17&lt;/P&gt;&lt;P&gt;Waiting for root device /dev/mmcblk0p2...&lt;/P&gt;&lt;P&gt;mmc0: new high speed SD card at address 0002&lt;/P&gt;&lt;P&gt;mmcblk0: mmc0:0002 00000 954 MiB&lt;/P&gt;&lt;P&gt;mmcblk0: p1 p2&lt;/P&gt;&lt;P&gt;EXT2-fs (mmcblk0p2): warning: mounting unchecked fs, running e2fsck is recommended&lt;/P&gt;&lt;P&gt;VFS: Mounted root (ext2 filesystem) on device 179:2.&lt;/P&gt;&lt;P&gt;Freeing init memory: 120K&lt;/P&gt;&lt;P&gt;EXT2-fs (mmcblk0p2): error: ext2_check_page: bad#7521: : rec_len is smaller than minimal - offset=0, inode=0, rec_len=0, name_len=0&lt;/P&gt;&lt;P&gt;Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.&lt;/P&gt;&lt;P&gt;Backtrace:&lt;/P&gt;&lt;P&gt;[&amp;lt;c002a2dc&amp;gt;] (dump_backtrace+0x0/0x10c) from [&amp;lt;c02e9c48&amp;gt;] (dump_stack+0x18/0x1c)&lt;/P&gt;&lt;P&gt;r7:00000013 r6:c0043150 r5:c0021900 r4:c03ed6c0&lt;/P&gt;&lt;P&gt;[&amp;lt;c02e9c30&amp;gt;] (dump_stack+0x0/0x1c) from [&amp;lt;c02e9cb4&amp;gt;] (panic+0x68/0xec)&lt;/P&gt;&lt;P&gt;[&amp;lt;c02e9c4c&amp;gt;] (panic+0x0/0xec) from [&amp;lt;c0026628&amp;gt;] (init_post+0x124/0x15c)&lt;/P&gt;&lt;P&gt;r3:c3f96900 r2:00000000 r1:c04822c0 r0:c0367442&lt;/P&gt;&lt;P&gt;[&amp;lt;c0026504&amp;gt;] (init_post+0x0/0x15c) from [&amp;lt;c00084f8&amp;gt;] (kernel_init+0x128/0x16c)&lt;/P&gt;&lt;P&gt;r4:c03ecb98&lt;/P&gt;&lt;P&gt;[&amp;lt;c00083d0&amp;gt;] (kernel_init+0x0/0x16c) from [&amp;lt;c0043150&amp;gt;] (do_exit+0x0/0x664)&lt;/P&gt;&lt;P&gt;r5:c00083d0 r4:00000000&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2011 09:29:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX233-DCDC-powerUp-problem/m-p/195517#M10351</guid>
      <dc:creator>s_i_suprun</dc:creator>
      <dc:date>2011-12-13T09:29:39Z</dc:date>
    </item>
    <item>
      <title>Re: iMX233 DCDC powerUp problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX233-DCDC-powerUp-problem/m-p/195518#M10352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is not a problem with the DC/DC or the PSU in general. It more like a problem with you partitions on the MMC&lt;/P&gt;&lt;P&gt;Attached is a file that describes how to properly set partitions on SD/MMC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, check/edit you init memory size in LTIB option&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2011 10:36:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX233-DCDC-powerUp-problem/m-p/195518#M10352</guid>
      <dc:creator>danix</dc:creator>
      <dc:date>2011-12-14T10:36:59Z</dc:date>
    </item>
  </channel>
</rss>