<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX53 QSB audio record problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-audio-record-problem/m-p/195433#M10337</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think the I2S bandwidth should &amp;nbsp;not be a problem, because I2S interface has&amp;nbsp;separated TX and RX signal.&lt;/P&gt;&lt;P&gt;Any ideas, guys?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Jan 2012 06:25:35 GMT</pubDate>
    <dc:creator>JerryFan</dc:creator>
    <dc:date>2012-01-04T06:25:35Z</dc:date>
    <item>
      <title>i.MX53 QSB audio record problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-audio-record-problem/m-p/195432#M10336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have i.MX53 QSB with lucid ubuntu image. At the beginning, I play a mp3 audio file first, in the same time, use "arecord" utility to record the sound from micphone.&amp;nbsp; During the procedure, there are some overrun message is shown, and something is lost in recorded audio file. For example, the record audio should have the sound of number from 1~20, but in the recorded audio, number 8 &amp;amp; 11 is missing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The message is listed below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$totem aaa.mp3 &amp;amp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ arecord -f cd test.wav&lt;/P&gt;&lt;P&gt;Recording WAVE 'test.wav' : Signed 15 bit Little Endian, Rate 44100 Hz, Stereo&lt;/P&gt;&lt;P&gt;overrun!!! (at least -437969.791 ms long)&lt;/P&gt;&lt;P&gt;overrun!!! (at least -437969.798 ms long)&lt;/P&gt;&lt;P&gt;overrun!!! (at least -437969.798 ms long)&lt;/P&gt;&lt;P&gt;^C Aborted by signal Interrupt...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If no audio playback when recording, then this problem is gone. Is it possible I2S bandwidth issue ? Anybody have idea how to solved this problem ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, if I use "gnome-sound-recorder" to test in stead of "arecord", then the saved audio is very poor ( without mp3 playback).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2011 07:31:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-audio-record-problem/m-p/195432#M10336</guid>
      <dc:creator>SamayaLin</dc:creator>
      <dc:date>2011-12-14T07:31:12Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 QSB audio record problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-audio-record-problem/m-p/195433#M10337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think the I2S bandwidth should &amp;nbsp;not be a problem, because I2S interface has&amp;nbsp;separated TX and RX signal.&lt;/P&gt;&lt;P&gt;Any ideas, guys?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jan 2012 06:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-QSB-audio-record-problem/m-p/195433#M10337</guid>
      <dc:creator>JerryFan</dc:creator>
      <dc:date>2012-01-04T06:25:35Z</dc:date>
    </item>
  </channel>
</rss>