<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to remove framebuffer and GPU functions in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-remove-framebuffer-and-GPU-functions/m-p/671226#M103369</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I do not use yocto, when I remove the module " device drivers--&amp;gt;graphics support--&amp;gt;support for frame buffer devices",althought the system can boot up and also can login,but the system died after a few seconds. The system is run in level 3.and I also remove the touchscreen drivers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 May 2017 02:06:08 GMT</pubDate>
    <dc:creator>jiongzhongliu</dc:creator>
    <dc:date>2017-05-11T02:06:08Z</dc:date>
    <item>
      <title>How to remove framebuffer and GPU functions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-remove-framebuffer-and-GPU-functions/m-p/671224#M103367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;my board is IMX6Q-SABRESD,and used linux3.14.52.Now my project do not need display function,so I want to remove the codes about the framebuffer and GPU,and the system can boot as quickly as possible,becauss the fb and gpu initialize consume too much time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;I use make menuconfig to remove the framebuffer moudle and change the device tee to remove ldb node. and the linux image can be lunch, but after the linux system run about a few seconds, the system died! How can it happen?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;If I want to remove framebuffer and GPU functions, is there something I shall do? thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 May 2017 09:08:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-remove-framebuffer-and-GPU-functions/m-p/671224#M103367</guid>
      <dc:creator>jiongzhongliu</dc:creator>
      <dc:date>2017-05-08T09:08:50Z</dc:date>
    </item>
    <item>
      <title>Re: How to remove framebuffer and GPU functions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-remove-framebuffer-and-GPU-functions/m-p/671225#M103368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jiongzhong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please try minimal configuration "core-image-minimal"&lt;/P&gt;&lt;P&gt;described in Table 1. Freescale Yocto project images attached Yocto Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 May 2017 10:07:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-remove-framebuffer-and-GPU-functions/m-p/671225#M103368</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-05-08T10:07:33Z</dc:date>
    </item>
    <item>
      <title>Re: How to remove framebuffer and GPU functions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-remove-framebuffer-and-GPU-functions/m-p/671226#M103369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I do not use yocto, when I remove the module " device drivers--&amp;gt;graphics support--&amp;gt;support for frame buffer devices",althought the system can boot up and also can login,but the system died after a few seconds. The system is run in level 3.and I also remove the touchscreen drivers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 May 2017 02:06:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-remove-framebuffer-and-GPU-functions/m-p/671226#M103369</guid>
      <dc:creator>jiongzhongliu</dc:creator>
      <dc:date>2017-05-11T02:06:08Z</dc:date>
    </item>
  </channel>
</rss>