<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: imx7d PCIe configuration registers</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx7d-PCIe-configuration-registers/m-p/669965#M103173</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you mean that the regs at 0x33800000 are all the same as (just a memory map of) the regs at 0x306d0000?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: 0x33800000 - I got&amp;nbsp;it from the imx7d.dtsi file. From the drivers\pci\host\pci-imx6.c I can see the base address is something like 0xc01d0000 (the value of pp-&amp;gt;dbi_base)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Jun 2017 13:36:32 GMT</pubDate>
    <dc:creator>dmitrykinev</dc:creator>
    <dc:date>2017-06-01T13:36:32Z</dc:date>
    <item>
      <title>imx7d PCIe configuration registers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7d-PCIe-configuration-registers/m-p/669963#M103171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could someone please explain the difference between regiters used in the linux kernel starting at address 0x33800000 and registers decribed in the imx7d Reference Manual (at address 0x306d0000)? Why&amp;nbsp;are the &lt;A href="mailto:regs@0x3380.."&gt;regs at 0x3380&lt;/A&gt;0000 used instead of regs at 0x306d0000? I also can't find a description for regs at 0x33800000.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 May 2017 20:34:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7d-PCIe-configuration-registers/m-p/669963#M103171</guid>
      <dc:creator>dmitrykinev</dc:creator>
      <dc:date>2017-05-31T20:34:19Z</dc:date>
    </item>
    <item>
      <title>Re: imx7d PCIe configuration registers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7d-PCIe-configuration-registers/m-p/669964#M103172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dmitry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linux uses address mapping, only i.MX7D PCIe register descriptions are given&lt;/P&gt;&lt;P&gt;in Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jun 2017 06:29:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7d-PCIe-configuration-registers/m-p/669964#M103172</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-01T06:29:34Z</dc:date>
    </item>
    <item>
      <title>Re: imx7d PCIe configuration registers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7d-PCIe-configuration-registers/m-p/669965#M103173</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you mean that the regs at 0x33800000 are all the same as (just a memory map of) the regs at 0x306d0000?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: 0x33800000 - I got&amp;nbsp;it from the imx7d.dtsi file. From the drivers\pci\host\pci-imx6.c I can see the base address is something like 0xc01d0000 (the value of pp-&amp;gt;dbi_base)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jun 2017 13:36:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7d-PCIe-configuration-registers/m-p/669965#M103173</guid>
      <dc:creator>dmitrykinev</dc:creator>
      <dc:date>2017-06-01T13:36:32Z</dc:date>
    </item>
    <item>
      <title>Re: imx7d PCIe configuration registers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7d-PCIe-configuration-registers/m-p/669966#M103174</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;seems these registers are the same as for i.MX6Q PCIe dtsi 0x1000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2017 03:43:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7d-PCIe-configuration-registers/m-p/669966#M103174</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-02T03:43:02Z</dc:date>
    </item>
  </channel>
</rss>