<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Regarding  i.MX 6UltraLite Processor  Booting</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Regarding-i-MX-6UltraLite-Processor-Booting/m-p/669705#M103123</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using i.MX 6UltraLite Processor in our project , As per reference manual we made BOOT_MODE0 to '1' and BOOT_MODE1 to '0' for serial boot option, in this mode we are able to read &amp;amp; write the data from DDR3 and we can download the imge to eMMC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And later we made BOOT_MODE0 to '0' and BOOT_MODE1 to '1' to enter internalboot (through eMMC ) option eventhough we made these settings we are unable to boot the processor through eMMC. and we observed that processor is in serail boot mode only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can any one suggest us, do we need to make any other settings for internal boot option ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Kumaraswamy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Jul 2017 02:37:12 GMT</pubDate>
    <dc:creator>arvapallykumara</dc:creator>
    <dc:date>2017-07-14T02:37:12Z</dc:date>
    <item>
      <title>Regarding  i.MX 6UltraLite Processor  Booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Regarding-i-MX-6UltraLite-Processor-Booting/m-p/669705#M103123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using i.MX 6UltraLite Processor in our project , As per reference manual we made BOOT_MODE0 to '1' and BOOT_MODE1 to '0' for serial boot option, in this mode we are able to read &amp;amp; write the data from DDR3 and we can download the imge to eMMC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And later we made BOOT_MODE0 to '0' and BOOT_MODE1 to '1' to enter internalboot (through eMMC ) option eventhough we made these settings we are unable to boot the processor through eMMC. and we observed that processor is in serail boot mode only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can any one suggest us, do we need to make any other settings for internal boot option ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Kumaraswamy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jul 2017 02:37:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Regarding-i-MX-6UltraLite-Processor-Booting/m-p/669705#M103123</guid>
      <dc:creator>arvapallykumara</dc:creator>
      <dc:date>2017-07-14T02:37:12Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding  i.MX 6UltraLite Processor  Booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Regarding-i-MX-6UltraLite-Processor-Booting/m-p/669706#M103124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; It is necessary to configure the BOOT_CFG options, using section 8.5.3.1 (Expansion Device eFUSE Configuration) &amp;nbsp;&lt;/P&gt;&lt;P&gt;of i.MX 6UltraLite Applications Processor Reference Manual, Rev. 1, 04/2016.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf" title="http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf"&gt;http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jul 2017 07:03:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Regarding-i-MX-6UltraLite-Processor-Booting/m-p/669706#M103124</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-07-18T07:03:24Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding  i.MX 6UltraLite Processor  Booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Regarding-i-MX-6UltraLite-Processor-Booting/m-p/669707#M103125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We will configure and check once again as per your suggestion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kumar.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jul 2017 07:59:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Regarding-i-MX-6UltraLite-Processor-Booting/m-p/669707#M103125</guid>
      <dc:creator>arvapallykumara</dc:creator>
      <dc:date>2017-07-18T07:59:46Z</dc:date>
    </item>
  </channel>
</rss>