<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLCD issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LCD-issue/m-p/669655#M103116</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I am working on a custom board which is based on i.MX6 solo board.Linux yocto is being used to boot the board . The kernel version is 3.14.38.The issue being faced is ,image size is larger.It is not fitting correctly on LCD.&lt;/P&gt;&lt;P&gt;LCD resolution is 320*240.&lt;/P&gt;&lt;P&gt;modified the dts file based on LCD datasheet.&lt;/P&gt;&lt;P&gt;i have seen the below thread, which tells change pll2 to pll5.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="jivelink1" href="https://community.nxp.com/message/833716?commentID=833716#comment-833716" title="https://community.nxp.com/message/833716?commentID=833716#comment-833716"&gt;https://community.nxp.com/message/833716?commentID=833716#comment-833716&lt;/A&gt;&lt;/P&gt;&lt;P&gt;am not understanding where to change the clock to pll5.am not using sabre board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Rizwan Syed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Jul 2017 11:34:54 GMT</pubDate>
    <dc:creator>rizwan_s</dc:creator>
    <dc:date>2017-07-14T11:34:54Z</dc:date>
    <item>
      <title>LCD issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-issue/m-p/669655#M103116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I am working on a custom board which is based on i.MX6 solo board.Linux yocto is being used to boot the board . The kernel version is 3.14.38.The issue being faced is ,image size is larger.It is not fitting correctly on LCD.&lt;/P&gt;&lt;P&gt;LCD resolution is 320*240.&lt;/P&gt;&lt;P&gt;modified the dts file based on LCD datasheet.&lt;/P&gt;&lt;P&gt;i have seen the below thread, which tells change pll2 to pll5.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="jivelink1" href="https://community.nxp.com/message/833716?commentID=833716#comment-833716" title="https://community.nxp.com/message/833716?commentID=833716#comment-833716"&gt;https://community.nxp.com/message/833716?commentID=833716#comment-833716&lt;/A&gt;&lt;/P&gt;&lt;P&gt;am not understanding where to change the clock to pll5.am not using sabre board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Rizwan Syed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jul 2017 11:34:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-issue/m-p/669655#M103116</guid>
      <dc:creator>rizwan_s</dc:creator>
      <dc:date>2017-07-14T11:34:54Z</dc:date>
    </item>
    <item>
      <title>Re: LCD issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-issue/m-p/669656#M103117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rizwan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please follow the following document &lt;A href="https://community.nxp.com/docs/DOC-172312"&gt;Porting LVDS LCD With Low Resolution to i.MX6&lt;/A&gt; ,&amp;nbsp;&amp;nbsp; In this document you can see that you need to modify the DTS file and also make some changes in the&amp;nbsp; &lt;SPAN style="font-size: 12pt;"&gt;/arch/arm/mach-mx6/clock.c,&amp;nbsp; there you can modify&amp;nbsp; 3 ldb's clock source : &lt;/SPAN&gt;&lt;STRONG&gt;&amp;amp;pll5_video_main_clk,&lt;/STRONG&gt; &lt;SPAN lang="EN-US" style="font-size: 10.5pt; font-family: 'Times New Roman','serif';"&gt;&amp;amp;&lt;STRONG&gt;pll2_pfd_352M, &lt;/STRONG&gt;&lt;/SPAN&gt;&amp;amp;&lt;STRONG&gt;pll2_pfd_400M,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jul 2017 15:55:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-issue/m-p/669656#M103117</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2017-07-14T15:55:01Z</dc:date>
    </item>
  </channel>
</rss>