<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Read verification error in Serial Flash in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Read-verification-error-in-Serial-Flash/m-p/669411#M103024</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is regarding iMX6Q, SST26VF032B Serial Flash base custom board design and following error message shows on console (Red highlighted in log file) while doing the run upgradeu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;Total of 0 byte(s) were the same&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;Read verification error&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In order to configure the SPI Flash and RAM&amp;nbsp;I have done all the changes related to DDR calibration values in .cfg file and SPI flash configurations in spi param.c file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;{"SST26VF032B", 0xbf2642, 0x0, 64 * 1024, 64, RD_NORM, SECT_4K},&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Could you please tell me the reason for this issue ? Any idea regarding this ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Console log file --------&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2016.03-20600-g0dbffd3-dirty (Jun 21 2017 - 13:29:09 +0100)&amp;nbsp;base custom board design&amp;nbsp;&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6Q rev1.2 at 792 MHz&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: Nitrogen6_max&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;SF: Detected SST26VF032B with page size 256 Bytes, erase size 4 KiB, total 4 MiB&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;Display: hdmi:1280x720M@60 (1280x720)&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Net: FEC [PRIME]&lt;BR /&gt;Error: FEC address not set.&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;=&amp;gt; run upgradeu&lt;BR /&gt;AHCI 0000.0000 1 slots 1 ports ? Gbps 0x0 impl SATA mode&lt;BR /&gt;flags:&lt;BR /&gt;No port device detected!&lt;BR /&gt;** Bad device size - sata 0 **&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;1808 bytes read in 37 ms (46.9 KiB/s)&lt;BR /&gt;## Executing script at 10008000&lt;BR /&gt;check U-Boot&lt;BR /&gt;490496 bytes read in 159 ms (2.9 MiB/s)&lt;BR /&gt;read 77c00 bytes from SD card&lt;BR /&gt;SF: Detected SST26VF032B with page size 256 Bytes, erase size 4 KiB, total 4 MiB&lt;BR /&gt;probed SPI ROM&lt;BR /&gt;device 0 offset 0x400, size 0x77c00&lt;BR /&gt;SF: 490496 bytes @ 0x400 Read: OK&lt;BR /&gt;byte at 0x12000000 (0xd1) != byte at 0x12400000 (0xff)&lt;BR /&gt;Total of 0 byte(s) were the same&lt;BR /&gt;Need U-Boot upgrade&lt;BR /&gt;Program in 5 seconds&lt;BR /&gt;5&lt;BR /&gt;4&lt;BR /&gt;3&lt;BR /&gt;2&lt;BR /&gt;1&lt;BR /&gt;erasing&lt;BR /&gt;SF: 786432 bytes @ 0x0 Erased: OK&lt;BR /&gt;programming&lt;BR /&gt;device 0 offset 0x400, size 0x77c00&lt;BR /&gt;SF: 490496 bytes @ 0x400 Written: OK&lt;BR /&gt;verifying&lt;BR /&gt;device 0 offset 0x400, size 0x77c00&lt;BR /&gt;SF: 490496 bytes @ 0x400 Read: OK&lt;BR /&gt;byte at 0x12000000 (0xd1) != byte at 0x12400000 (0xff)&lt;BR /&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;Total of 0 byte(s) were the same&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;Read verification error&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;timeout irqstat=10000&lt;BR /&gt;timeout irqstat=10000&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1(part 0) is current device&lt;BR /&gt;** No partition table - mmc 1 **&lt;BR /&gt;starting USB...&lt;BR /&gt;USB0: USB EHCI 1.00&lt;BR /&gt;scanning bus 0 for devices... 1 USB Device(s) found&lt;BR /&gt;USB1: USB EHCI 1.00&lt;BR /&gt;scanning bus 1 for devices... 1 USB Device(s) found&lt;BR /&gt; scanning usb for storage devices... 0 Storage Device(s) found&lt;BR /&gt; scanning usb for ethernet devices... 0 Ethernet Device(s) found&lt;/P&gt;&lt;P&gt;USB device 0: unknown device&lt;BR /&gt;** Bad device usb 0 **&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Jun 2017 07:37:16 GMT</pubDate>
    <dc:creator>peteramond</dc:creator>
    <dc:date>2017-06-22T07:37:16Z</dc:date>
    <item>
      <title>Read verification error in Serial Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Read-verification-error-in-Serial-Flash/m-p/669411#M103024</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is regarding iMX6Q, SST26VF032B Serial Flash base custom board design and following error message shows on console (Red highlighted in log file) while doing the run upgradeu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;Total of 0 byte(s) were the same&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;Read verification error&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In order to configure the SPI Flash and RAM&amp;nbsp;I have done all the changes related to DDR calibration values in .cfg file and SPI flash configurations in spi param.c file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;{"SST26VF032B", 0xbf2642, 0x0, 64 * 1024, 64, RD_NORM, SECT_4K},&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Could you please tell me the reason for this issue ? Any idea regarding this ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Console log file --------&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2016.03-20600-g0dbffd3-dirty (Jun 21 2017 - 13:29:09 +0100)&amp;nbsp;base custom board design&amp;nbsp;&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6Q rev1.2 at 792 MHz&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: Nitrogen6_max&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;SF: Detected SST26VF032B with page size 256 Bytes, erase size 4 KiB, total 4 MiB&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;Display: hdmi:1280x720M@60 (1280x720)&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Net: FEC [PRIME]&lt;BR /&gt;Error: FEC address not set.&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;=&amp;gt; run upgradeu&lt;BR /&gt;AHCI 0000.0000 1 slots 1 ports ? Gbps 0x0 impl SATA mode&lt;BR /&gt;flags:&lt;BR /&gt;No port device detected!&lt;BR /&gt;** Bad device size - sata 0 **&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;1808 bytes read in 37 ms (46.9 KiB/s)&lt;BR /&gt;## Executing script at 10008000&lt;BR /&gt;check U-Boot&lt;BR /&gt;490496 bytes read in 159 ms (2.9 MiB/s)&lt;BR /&gt;read 77c00 bytes from SD card&lt;BR /&gt;SF: Detected SST26VF032B with page size 256 Bytes, erase size 4 KiB, total 4 MiB&lt;BR /&gt;probed SPI ROM&lt;BR /&gt;device 0 offset 0x400, size 0x77c00&lt;BR /&gt;SF: 490496 bytes @ 0x400 Read: OK&lt;BR /&gt;byte at 0x12000000 (0xd1) != byte at 0x12400000 (0xff)&lt;BR /&gt;Total of 0 byte(s) were the same&lt;BR /&gt;Need U-Boot upgrade&lt;BR /&gt;Program in 5 seconds&lt;BR /&gt;5&lt;BR /&gt;4&lt;BR /&gt;3&lt;BR /&gt;2&lt;BR /&gt;1&lt;BR /&gt;erasing&lt;BR /&gt;SF: 786432 bytes @ 0x0 Erased: OK&lt;BR /&gt;programming&lt;BR /&gt;device 0 offset 0x400, size 0x77c00&lt;BR /&gt;SF: 490496 bytes @ 0x400 Written: OK&lt;BR /&gt;verifying&lt;BR /&gt;device 0 offset 0x400, size 0x77c00&lt;BR /&gt;SF: 490496 bytes @ 0x400 Read: OK&lt;BR /&gt;byte at 0x12000000 (0xd1) != byte at 0x12400000 (0xff)&lt;BR /&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;Total of 0 byte(s) were the same&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;Read verification error&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;timeout irqstat=10000&lt;BR /&gt;timeout irqstat=10000&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1(part 0) is current device&lt;BR /&gt;** No partition table - mmc 1 **&lt;BR /&gt;starting USB...&lt;BR /&gt;USB0: USB EHCI 1.00&lt;BR /&gt;scanning bus 0 for devices... 1 USB Device(s) found&lt;BR /&gt;USB1: USB EHCI 1.00&lt;BR /&gt;scanning bus 1 for devices... 1 USB Device(s) found&lt;BR /&gt; scanning usb for storage devices... 0 Storage Device(s) found&lt;BR /&gt; scanning usb for ethernet devices... 0 Ethernet Device(s) found&lt;/P&gt;&lt;P&gt;USB device 0: unknown device&lt;BR /&gt;** Bad device usb 0 **&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jun 2017 07:37:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Read-verification-error-in-Serial-Flash/m-p/669411#M103024</guid>
      <dc:creator>peteramond</dc:creator>
      <dc:date>2017-06-22T07:37:16Z</dc:date>
    </item>
    <item>
      <title>Re: Read verification error in Serial Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Read-verification-error-in-Serial-Flash/m-p/669412#M103025</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;upgradeu was developed by BD and one can look at its sources:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fboundarydevices.com%2Fswitching-u-boot-versions-on-i-mx6%2F" rel="nofollow" target="_blank"&gt;https://boundarydevices.com/switching-u-boot-versions-on-i-mx6/&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://boundarydevices.com/compiling-latest-u-boot-for-i-mx6-2015-edition/"&gt;https://boundarydevices.com/compiling-latest-u-boot-for-i-mx6-2015-edition/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;seems data is not written correctly to flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jun 2017 23:12:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Read-verification-error-in-Serial-Flash/m-p/669412#M103025</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-22T23:12:40Z</dc:date>
    </item>
    <item>
      <title>Re: Read verification error in Serial Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Read-verification-error-in-Serial-Flash/m-p/669413#M103026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="206296" data-username="igorpadykov" href="https://community.nxp.com/people/igorpadykov" style="color: #5e89c1; background-color: #ffffff; border: 0px; font-weight: 200; text-decoration: underline; font-size: 1.286rem;"&gt;igorpadykov&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now the custom&amp;nbsp;boot from flash correctly and when it start the kernel shows the following error messages.&lt;/P&gt;&lt;P&gt;I have done the changes to all the imx6qdl.dtsi, imx6qd.dtsi and etc files and compiled and generated the dtb file as well. &lt;STRONG&gt;Could you please tell me the reason for following error messages.&lt;/STRONG&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;----------- trying to load /initrd.img&lt;BR /&gt;6556084 bytes read in 637 ms (9.8 MiB/s)&lt;BR /&gt;5791064 bytes read in 663 ms (8.3 MiB/s)&lt;BR /&gt;Kernel image @ 0x10800000 [ 0x000000 - 0x585d58 ]&lt;BR /&gt;## Flattened Device Tree blob at 13000000&lt;BR /&gt;Booting using the fdt blob at 0x13000000&lt;BR /&gt;reserving fdt memory region: addr=13000000 size=b000&lt;BR /&gt;Using Device Tree in place at 13000000, end 1300dfff&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/iomuxc-imx6q-nitrogen6-maxgrp/audmuxgrp&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/iomuxc-imx6q-nitrogen6-maxgrp/hoggrp&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/iomuxc-imx6q-nitrogen6-maxgrp/i2c1-sgtl5000grp&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/iomuxc-imx6q-nitrogen6-maxgrp/i2c2muxgrp&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/iomuxc-imx6q-nitrogen6-maxgrp/i2c3muxgrp&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: no fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/iomuxc-imx6q-nitrogen6-maxgrp/i2c3-ov5640grp&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/iomuxc-imx6q-nitrogen6-maxgrp/reg-wlan-engrp&lt;BR /&gt;i2c-mux-gpio i2cmux@2: Missing mux-gpios property in the DT.&lt;BR /&gt;i2c-mux-gpio i2cmux@3: Missing mux-gpios property in the DT.&lt;BR /&gt;ldb 2000000.aips-bus:ldb@020e0008: failed to find valid LVDS channel&lt;BR /&gt;m25p80 spi0.0: unrecognized JEDEC id bytes: bf, 26, 42&lt;BR /&gt;imx-sgtl5000 sound: ASoC: CODEC DAI sgtl5000 not registered&lt;BR /&gt;imx-sgtl5000 sound: snd_soc_register_card failed (-517)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Jun 2017 06:10:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Read-verification-error-in-Serial-Flash/m-p/669413#M103026</guid>
      <dc:creator>peteramond</dc:creator>
      <dc:date>2017-06-24T06:10:18Z</dc:date>
    </item>
  </channel>
</rss>