<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Custom Device Tree Blob Target</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Custom-Device-Tree-Blob-Target/m-p/669095#M102959</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi danielbujak,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Device tree is an extensive topic. The following document explains how to customize a device tree. In this case the Udoo board is used.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329664"&gt;Basic Device Tree for the Udoo Board&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For general information about device Tree you may take a look to the links provided at the end of this post:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/450118"&gt;32Khz clock on CCM_CLKO2 (SD1_WP)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Jul 2017 17:07:47 GMT</pubDate>
    <dc:creator>Carlos_Musich</dc:creator>
    <dc:date>2017-07-13T17:07:47Z</dc:date>
    <item>
      <title>Custom Device Tree Blob Target</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-Device-Tree-Blob-Target/m-p/669094#M102958</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I build the images for my custom board based on the imx6ul, I still get a imx6ul-14x14-evk.dtb file generated. I'd like to change the target to create a imx6ul-customboard.dtb and be able to modify the source files to match my board layout. I think I should create a copy of all the imx6ul-14x14-*.dts files and rename them imx6ul-customboard-*.dts and then modify those to meet my needs. However, I'm unsure where in the build configs I should be specifying which device tree source to build into the image. Do I just set the BR2_LINUX_KERNEL_INTREE_DTS_NAME?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any device tree customization guide available, or can anyone point me in the right direction?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jul 2017 14:49:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-Device-Tree-Blob-Target/m-p/669094#M102958</guid>
      <dc:creator>danielbujak</dc:creator>
      <dc:date>2017-07-13T14:49:03Z</dc:date>
    </item>
    <item>
      <title>Re: Custom Device Tree Blob Target</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-Device-Tree-Blob-Target/m-p/669095#M102959</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi danielbujak,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Device tree is an extensive topic. The following document explains how to customize a device tree. In this case the Udoo board is used.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329664"&gt;Basic Device Tree for the Udoo Board&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For general information about device Tree you may take a look to the links provided at the end of this post:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/450118"&gt;32Khz clock on CCM_CLKO2 (SD1_WP)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jul 2017 17:07:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-Device-Tree-Blob-Target/m-p/669095#M102959</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-07-13T17:07:47Z</dc:date>
    </item>
  </channel>
</rss>