<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMx6 - MIPI CSI camera raw10 format support in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMx6-MIPI-CSI-camera-raw10-format-support/m-p/668760#M102898</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;I am working on imx6 camera driver development for MIPI camera which supports RAW10 pixelformat only. So I want to add support for RAW10 format. &lt;BR /&gt;For example &lt;BR /&gt;#define V4l2_PIX_FMT_SBGGR10P v4l2_fourcc('P', 'B', 'A', 'A')&lt;/P&gt;&lt;P&gt;I saw the latest BSP , seems it doesn't support RAW10 pixelformat, so can you please tell us the IPU driver changes or patches or any reference link who did the RAW10 for imx6.&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;BR /&gt;Thalapushpam,.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Aug 2017 12:46:49 GMT</pubDate>
    <dc:creator>sivasiva</dc:creator>
    <dc:date>2017-08-07T12:46:49Z</dc:date>
    <item>
      <title>iMx6 - MIPI CSI camera raw10 format support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMx6-MIPI-CSI-camera-raw10-format-support/m-p/668760#M102898</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;I am working on imx6 camera driver development for MIPI camera which supports RAW10 pixelformat only. So I want to add support for RAW10 format. &lt;BR /&gt;For example &lt;BR /&gt;#define V4l2_PIX_FMT_SBGGR10P v4l2_fourcc('P', 'B', 'A', 'A')&lt;/P&gt;&lt;P&gt;I saw the latest BSP , seems it doesn't support RAW10 pixelformat, so can you please tell us the IPU driver changes or patches or any reference link who did the RAW10 for imx6.&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;BR /&gt;Thalapushpam,.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Aug 2017 12:46:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMx6-MIPI-CSI-camera-raw10-format-support/m-p/668760#M102898</guid>
      <dc:creator>sivasiva</dc:creator>
      <dc:date>2017-08-07T12:46:49Z</dc:date>
    </item>
    <item>
      <title>Re: iMx6 - MIPI CSI camera raw10 format support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMx6-MIPI-CSI-camera-raw10-format-support/m-p/668761#M102899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi siva&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in L4.1.15 BSP release, there is ov5647_mipi driver:&amp;nbsp; drivers/media/platform/mxc/subdev/ov5647_mipi.c.&lt;/P&gt;&lt;P&gt;also one can refer to ov5647 in :&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fforum.solid-run.com%2Flinux-kernel-and-bootloaders-on-cubox-i-and-hummin-f10%2Fov5647-driver--t1740.html" rel="nofollow" target="_blank"&gt;http://forum.solid-run.com/linux-kernel-and-bootloaders-on-cubox-i-and-hummin-f10/ov5647-driver--t1740.html&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.freescale.com/message/309833#309833"&gt;https://community.freescale.com/message/309833#309833&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Aug 2017 23:14:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMx6-MIPI-CSI-camera-raw10-format-support/m-p/668761#M102899</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-08-07T23:14:01Z</dc:date>
    </item>
  </channel>
</rss>