<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックReading Processor Variant and Fusemap from the console</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Reading-Processor-Variant-and-Fusemap-from-the-console/m-p/668122#M102783</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using the DART 6UL board from Varascite and their Yocto-generated 4.1.15 distribution. I have the following questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is there a way to read the processor variant (G0, G1, etc.), e.g., from the /proc file system (from the console)?&lt;/LI&gt;&lt;LI&gt;How do you read the fuse map from the console? We want to read fuse map location 0x430, bits 21:20, "TAMPER_PIN_DISABLE[1:0]" (from the imx6 applications processor reference manual).&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Namely I want to find out if the tamper inputs have been fused so that they cannot be used as GPIO outputs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for any pointers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Aug 2017 17:07:52 GMT</pubDate>
    <dc:creator>yates</dc:creator>
    <dc:date>2017-08-07T17:07:52Z</dc:date>
    <item>
      <title>Reading Processor Variant and Fusemap from the console</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reading-Processor-Variant-and-Fusemap-from-the-console/m-p/668122#M102783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using the DART 6UL board from Varascite and their Yocto-generated 4.1.15 distribution. I have the following questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is there a way to read the processor variant (G0, G1, etc.), e.g., from the /proc file system (from the console)?&lt;/LI&gt;&lt;LI&gt;How do you read the fuse map from the console? We want to read fuse map location 0x430, bits 21:20, "TAMPER_PIN_DISABLE[1:0]" (from the imx6 applications processor reference manual).&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Namely I want to find out if the tamper inputs have been fused so that they cannot be used as GPIO outputs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for any pointers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Aug 2017 17:07:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reading-Processor-Variant-and-Fusemap-from-the-console/m-p/668122#M102783</guid>
      <dc:creator>yates</dc:creator>
      <dc:date>2017-08-07T17:07:52Z</dc:date>
    </item>
    <item>
      <title>Re: Reading Processor Variant and Fusemap from the console</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reading-Processor-Variant-and-Fusemap-from-the-console/m-p/668123#M102784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Randy&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems one can read the fuse map with: cat /sys/fsl_otp/&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/450573"&gt;i.mx6ull GP3 &amp;amp;amp; GP4 burning issue&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Aug 2017 23:57:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reading-Processor-Variant-and-Fusemap-from-the-console/m-p/668123#M102784</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-08-07T23:57:59Z</dc:date>
    </item>
  </channel>
</rss>