<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: UART1_RTS_B boot pin configuration</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/UART1-RTS-B-boot-pin-configuration/m-p/668045#M102770</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok thanks.&lt;/P&gt;&lt;P&gt;My doubt is mainly about the fact that in the datasheet (table 8-7 &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;i.MX6 UL RM&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&amp;nbsp;) I read that to boot from a specific device (SD, NAND, NOR ecc) you simply configure some GPIO pins and I don't understand how&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;UART1_RTS_B pin is involved in this process.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Jacopo&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Jun 2017 09:19:22 GMT</pubDate>
    <dc:creator>jacopoagostini</dc:creator>
    <dc:date>2017-06-22T09:19:22Z</dc:date>
    <item>
      <title>UART1_RTS_B boot pin configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART1-RTS-B-boot-pin-configuration/m-p/668041#M102766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a question about boot mode and pin configuration. Is it correct that when the pin&amp;nbsp;UART1_RTS_B is low the system reboot from SD Card. What about if this pin is high?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jun 2017 08:31:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART1-RTS-B-boot-pin-configuration/m-p/668041#M102766</guid>
      <dc:creator>jacopoagostini</dc:creator>
      <dc:date>2017-06-21T08:31:57Z</dc:date>
    </item>
    <item>
      <title>Re: UART1_RTS_B boot pin configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART1-RTS-B-boot-pin-configuration/m-p/668042#M102767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; UART1_RTS_B is configured as SD CD_B signal during SD boot : &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Table 8-18 (SD/MMC IOMUX Pin Configuration) of the i.MX6 UL RM (Rev. 1, 04/2016).&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;When internal boot failed, “SD or MMC card will be scanned on uSDHC1. If card is detected&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;and valid boot image is found in card, then boot image will be loaded then executed. Pad&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;of SD1_CD is used to detect whether card is inserted” - section 8.12 (SD/MMC Manufacture Mode) &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;of the i.MX6 UL RM.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; So, the UART1_RTS_B pulled low may cause SD boot, if proper card is inserted to SD1&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;port, even if the SD1 is not default boot device. If the UART1_RTS_B is pulled high - no SD boot occurs. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jun 2017 09:13:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART1-RTS-B-boot-pin-configuration/m-p/668042#M102767</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-06-21T09:13:33Z</dc:date>
    </item>
    <item>
      <title>Re: UART1_RTS_B boot pin configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART1-RTS-B-boot-pin-configuration/m-p/668043#M102768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What about if I configure a simple GPIO pin for the card detection and so I don't choose one of the possible pin listed in datasheet? Is SD Card detection still possible after a software configuration?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jun 2017 08:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART1-RTS-B-boot-pin-configuration/m-p/668043#M102768</guid>
      <dc:creator>jacopoagostini</dc:creator>
      <dc:date>2017-06-22T08:33:45Z</dc:date>
    </item>
    <item>
      <title>Re: UART1_RTS_B boot pin configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART1-RTS-B-boot-pin-configuration/m-p/668044#M102769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; boot options / pin configurations are provided by boot ROM during &amp;nbsp;boot.&lt;/P&gt;&lt;P&gt;After that it is possible to reconfigure pins as needed. And, yes, &amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;SD Card detection &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;still possible after a software configuration (under OS) in Your case.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jun 2017 08:51:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART1-RTS-B-boot-pin-configuration/m-p/668044#M102769</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-06-22T08:51:10Z</dc:date>
    </item>
    <item>
      <title>Re: UART1_RTS_B boot pin configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART1-RTS-B-boot-pin-configuration/m-p/668045#M102770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok thanks.&lt;/P&gt;&lt;P&gt;My doubt is mainly about the fact that in the datasheet (table 8-7 &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;i.MX6 UL RM&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&amp;nbsp;) I read that to boot from a specific device (SD, NAND, NOR ecc) you simply configure some GPIO pins and I don't understand how&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;UART1_RTS_B pin is involved in this process.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Jacopo&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jun 2017 09:19:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART1-RTS-B-boot-pin-configuration/m-p/668045#M102770</guid>
      <dc:creator>jacopoagostini</dc:creator>
      <dc:date>2017-06-22T09:19:22Z</dc:date>
    </item>
  </channel>
</rss>