<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX53 gstreamer on framebuffer?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194955#M10276</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You maybe simply comment these sentences to see what happened.&amp;nbsp;&lt;/P&gt;&lt;P&gt;maybe the some macro is not defined, it should defined&amp;nbsp;_MX51&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 17 Dec 2011 15:29:45 GMT</pubDate>
    <dc:creator>KanHU</dc:creator>
    <dc:date>2011-12-17T15:29:45Z</dc:date>
    <item>
      <title>i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194939#M10260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are there examples on how to use the gstreamer codec plugins on the i.MX53 without X Windows running on the target?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has someone played decoded video to the framebuffer?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Leon.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2011 23:18:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194939#M10260</guid>
      <dc:creator>sidebranch</dc:creator>
      <dc:date>2011-12-13T23:18:13Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194940#M10261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leon,&lt;/P&gt;&lt;P&gt;I only tried with gplay lately, but this one works flawlessly without any X running. Have to check with gst-launch tomorrow, but AFAIR it also worked without X. Only thing is that I did not yet figure out how to set up overlay correctly (blinking cursor of the framebuffer visible on the video...)&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Wolfgang&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2011 00:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194940#M10261</guid>
      <dc:creator>WolfgangW</dc:creator>
      <dc:date>2011-12-14T00:45:20Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194941#M10262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Short update:&lt;/P&gt;&lt;P&gt;Playback on raw framebuffer (actually: overlay via v4l) works with gst-launch as well as gplay in the same way.&lt;/P&gt;&lt;P&gt;With my self-compiled filesystem image, the overlay is also used without transparency, so the framebuffer contents is not visible while playing video - I remember this was different with the original Freescale image.&lt;/P&gt;&lt;P&gt;However, on second reading I am not sure if this is what you mean by "played decoded video to the framebuffer"?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2011 15:57:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194941#M10262</guid>
      <dc:creator>WolfgangW</dc:creator>
      <dc:date>2011-12-14T15:57:39Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194942#M10263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you. To answer your last question first: Yes, this is exactly what I mean with framebuffer playout. I was unsure if the V4L2 output used the fb device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tested the following on the supplied Ubuntu SD image:&lt;/P&gt;&lt;P&gt;time gst-launch filesrc location=/trailer_1080p.mov ! qtdemux ! mfw_vpudecoder ! mfw_v4lsink&lt;/P&gt;&lt;P&gt;I see the video play correctly in the background, even when I kill the X Windows server at the same time. This is OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my self-built image, I think I have an issue with the transparency, but opposite to your situation, in my case the framebuffer remains visible, but the video is invisible.&lt;/P&gt;&lt;P&gt;Where can this transparency be set?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MFW_GST_V4LSINK_PLUGIN&amp;nbsp; build on Dec 14 2011 13:56:30.&lt;BR /&gt;Setting pipeline to PAUSED ...&lt;BR /&gt;[INFO]&amp;nbsp;&amp;nbsp; &amp;nbsp;Product Info: i.MX53&lt;BR /&gt;VPU Version: firmware 13.4.41; libvpu: 5.3.2 &lt;BR /&gt;MFW_GST_VPU_DECODER_PLUGIN&amp;nbsp; build on Dec 14 2011 13:56:16.&lt;BR /&gt;Pipeline is PREROLLING ...&lt;BR /&gt;&amp;gt;&amp;gt;V4L_SINK: Actually buffer status:&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;hardware buffer : 0&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;software buffer : 0&lt;BR /&gt;Pipeline is PREROLLED ...&lt;BR /&gt;Setting pipeline to PLAYING ...&lt;BR /&gt;full screen size:1024x768&lt;BR /&gt;[V4L Update Display]: left=0, top=0, width=1024, height=768&lt;BR /&gt;New clock: GstSystemClock&lt;BR /&gt;Got EOS from element "pipeline0".&lt;BR /&gt;Execution ended after 32461977000 ns.&lt;BR /&gt;Setting pipeline to PAUSED ...&lt;BR /&gt;total time:0:00:32.480843375 ,Render fps:0&lt;BR /&gt;Setting pipeline to READY ...&lt;BR /&gt;Setting pipeline to NULL ...&lt;BR /&gt;Total rendered:0&lt;BR /&gt;&lt;BR /&gt;&amp;gt;&amp;gt;VPU_DEC: State: Ready to Null&lt;BR /&gt;Freeing pipeline ...&lt;BR /&gt;[---&amp;gt;FINALIZE vpu_dec&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2011 16:09:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194942#M10263</guid>
      <dc:creator>sidebranch</dc:creator>
      <dc:date>2011-12-14T16:09:26Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194943#M10264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, I didn't find out where to set transparency either.&lt;/P&gt;&lt;P&gt;Trying with gst-launch, my output looks mostly similar:&lt;/P&gt;&lt;P&gt;root@freescale ~$ gst-launch filesrc location=/mnt/cdrom/hd_other_samsung_led_motion.m2ts ! ffdemux_mpegts ! mfw_vpudecoder ! mfw_v4lsink&lt;BR /&gt;MFW_GST_V4LSINK_PLUGIN 2.0.3 build on Nov 25 2011 23:46:26.&lt;BR /&gt;Setting pipeline to PAUSED ...&lt;BR /&gt;[INFO] Product Info: i.MX53&lt;BR /&gt;VPU Version: firmware 13.4.41; libvpu: 5.3.2 &lt;BR /&gt;MFW_GST_VPU_DECODER_PLUGIN 2.0.3 build on Nov 25 2011 23:45:31.&lt;BR /&gt;Pipeline is PREROLLING ...&lt;BR /&gt;&amp;gt;&amp;gt;V4L_SINK: Actually buffer status:&lt;BR /&gt; hardware buffer : 11&lt;BR /&gt; software buffer : 0&lt;BR /&gt;Pipeline is PREROLLED ...&lt;BR /&gt;Setting pipeline to PLAYING ...&lt;BR /&gt;full screen size:1920x1080&lt;BR /&gt;[V4L Update Display]: left=0, top=0, width=1920, height=1080&lt;BR /&gt;New clock: GstSystemClock&lt;BR /&gt;video4linux video16: Bypassing IC&lt;BR /&gt;mxc_ipu mxc_ipu: Channel already disabled 10&lt;BR /&gt;mxc_ipu mxc_ipu: Channel already uninitialized 10&lt;BR /&gt;mxc_ipu mxc_ipu: Channel already disabled 10&lt;BR /&gt;mxc_ipu mxc_ipu: Channel already uninitialized 10&lt;BR /&gt;VPU blocking: timeout.&lt;BR /&gt;VPU blocking: timeout.&lt;BR /&gt;...&lt;/P&gt;&lt;P&gt;I am not sure if the number of hardware buffers at this point is meaningful? And, in my case, there is the message " video4linux video16: Bypassing IC" - what is IC? Might be image combiner...?&lt;BR /&gt;&lt;BR /&gt;BTW, this is a full HD video you're playing... Did you see and follow&amp;nbsp;&lt;A href="http://imxcommunity.org/group/imx53quickstartboard/forum/topics/playing-1080p-video-on-a-1080p-panel" target="_self"&gt;this post&lt;/A&gt;?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2011 16:34:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194943#M10264</guid>
      <dc:creator>WolfgangW</dc:creator>
      <dc:date>2011-12-14T16:34:44Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194944#M10265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;v4l sink is default output to fb2&lt;/P&gt;&lt;P&gt;composite for fb0 and fb2 is controlled by alpha value or colorkey&amp;nbsp;&lt;/P&gt;&lt;P&gt;there's ioctl for alpha setting&amp;nbsp;&lt;/P&gt;&lt;P&gt;struct mxcfb_gbl_alpha g_alpha;&amp;nbsp;&lt;/P&gt;&lt;P&gt;fd = open("/dev/fb0", O_RDWR, 0);&lt;/P&gt;&lt;P&gt;g_alpha.alpha = 128;&lt;BR /&gt; g_alpha.enable = 1;&lt;BR /&gt;ioctl(fd, MXCFB_SET_GBL_ALPHA, done, &amp;amp;g_alpha);&lt;/P&gt;&lt;P&gt;the alpha is from 0 to 255.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;the hardware buffer number is for internal debug only, you can ignore the information.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 02:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194944#M10265</guid>
      <dc:creator>KanHU</dc:creator>
      <dc:date>2011-12-15T02:17:38Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194945#M10266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My own build gives "hardware buffer : 0" and gives no codec video output to the screen.&lt;/P&gt;&lt;P&gt;The Ubuntu SD card gives "hardware buffer : 12" and works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be the reason for this difference?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have built and executed the alpha tool just to be sure it is no alpha/colorkey issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 03:03:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194945#M10266</guid>
      <dc:creator>sidebranch</dc:creator>
      <dc:date>2011-12-15T03:03:20Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194946#M10267</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;where you build from?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;can you post log with "export GST_DEBUG=mfw_vpudecoder:4,GST_CAPS:4"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 03:06:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194946#M10267</guid>
      <dc:creator>KanHU</dc:creator>
      <dc:date>2011-12-15T03:06:50Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194947#M10268</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for looking along. I build from the meta-freescale repository at GitHub, this is for OpenEmbedded.&amp;nbsp; I know this is not LTIB, but I am working with the Freescale team to bring this upstream. This should match the 11.09.01 source code release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached is the log for&lt;/P&gt;&lt;P&gt;export GST_DEBUG=mfw_vpudecoder:4,GST_CAPS:4&lt;/P&gt;&lt;P&gt;time gst-launch filesrc location=/trailer_1080p.mov ! qtdemux ! mfw_vpudecoder ! mfw_v4lsink&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 03:26:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194947#M10268</guid>
      <dc:creator>sidebranch</dc:creator>
      <dc:date>2011-12-15T03:26:09Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194948#M10269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;really strange, like the vpu did not set good caps to v4lsink&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;btw, I'm wondering which team you are with for upstream to which project? linaro? &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 03:32:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194948#M10269</guid>
      <dc:creator>KanHU</dc:creator>
      <dc:date>2011-12-15T03:32:08Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194949#M10270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry the log was not complete. I've deleted the old log and attached the new log instead.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 03:34:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194949#M10270</guid>
      <dc:creator>sidebranch</dc:creator>
      <dc:date>2011-12-15T03:34:23Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194950#M10271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No this is independent of Linaro. We are working on the Yocto Project and the OpenEmbedded Core.&lt;/P&gt;&lt;P&gt;This is mainly voluntary work by me in the community as I need this for a project, whilst Alonso Lazcano Adrian (B38018) is working to get Freescale teams to work on mainlining.&lt;/P&gt;&lt;P&gt;Freescale has already taken over my work for PowerPC mainlining in Yocto.&lt;/P&gt;&lt;P&gt;We can re-use the Linaro work. We mostly work on the build infrastructure for Yocto, not necessarely on kernel/user space fixes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However I do want to verify that what I check in and bring up stream actually works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 03:40:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194950#M10271</guid>
      <dc:creator>sidebranch</dc:creator>
      <dc:date>2011-12-15T03:40:56Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194951#M10272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;could you try "export GST_DEBUG=mfw_vpudecoder:4,mfw_v4lsink:4,GST_CAPS:4",&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need more information for analysis.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 05:30:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194951#M10272</guid>
      <dc:creator>KanHU</dc:creator>
      <dc:date>2011-12-15T05:30:06Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194952#M10273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have included the log for that.&lt;/P&gt;&lt;P&gt;I think it goes wrong at this point, I just cannot figure out why yet. The full log is in the attachment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0:00:03.544888354&amp;nbsp; 1233&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xd2fc0 ERROR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4l.c:1130:mfw_gst_v4l2_set_fmt: Error in mfw_gst_v4lsink_output_setup&lt;BR /&gt;&amp;gt;&amp;gt;V4L_SINK: Actually buffer status:&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;hardware buffer : 0&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;software buffer : 0&lt;BR /&gt;0:00:03.545144729&amp;nbsp; 1233&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xd2fc0 ERROR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4l_buffer.c:630:mfw_gst_v4l2_buffer_init: Failed to allocate buffer pool container&lt;BR /&gt;0:00:03.545243854&amp;nbsp; 1233&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xd2fc0 WARN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4l_buffer.c:400:mfw_gst_v4l2_new_buffer: Try new buffer failed, ret 2 No such file or directory queued 0&lt;BR /&gt;0:00:03.545417854&amp;nbsp; 1233&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xd2fc0 DEBUG&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4l_buffer.c:404:mfw_gst_v4l2_new_buffer: Finally assign a sw buffer from queue, left:0.&lt;BR /&gt;0:00:03.575604104&amp;nbsp; 1233&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xd2fc0 DEBUG&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4l_buffer.c:69:mfw_gst_v4lsink_buffer_finalize: Buffer 0 maybe dropped.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 15:22:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194952#M10273</guid>
      <dc:creator>sidebranch</dc:creator>
      <dc:date>2011-12-15T15:22:34Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194953#M10274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have continued my analysis why no video is played out from my build:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the "gst-fsl-plugin-2.0.3.tar.gz" package, the source file "mfw_gst_v4lsink.c" and the function "mfw_gst_v4lsink_buffer_alloc()":&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; max_frames = MAX_V4L_ALLOW_SIZE_IN_BYTE / frame_buffer_size;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (v4l_info-&amp;gt;buffers_required &amp;gt; max_frames) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; v4l_info-&amp;gt;buffers_required = max_frames;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;resulted in v4l_info-&amp;gt;buffers_required = 2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which resulted in mfw_gst_v4l.c: mfw_gst_v4l2_output_setup() to not allocate any buffers at all; this loop condition was never true:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (v4l_info-&amp;gt;buffers_required &amp;gt;= MIN_BUFFER_NUM) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have added extra Gstreamer debugging prints to demonstrate what happens. I do not have a clue yet why the Ubuntu provided image behaves differently. Unfortunately I am running into LTIB problems I have to solve, as that would provide a third basis.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0:00:01.058964251&amp;nbsp; 1231&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xf39c0 DEBUG&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4lsink.c:1890:mfw_gst_v4lsink_buffer_alloc: Decoded Width = 1920, Decoded Height = 1088&lt;BR /&gt;0:00:01.059034001&amp;nbsp; 1231&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xf39c0 WARN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4lsink.c:1213:mfw_gst_v4lsink_set_format: set to nv12 mode&lt;BR /&gt;0:00:01.059086376&amp;nbsp; 1231&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xf39c0 DEBUG&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4lsink.c:1902:mfw_gst_v4lsink_buffer_alloc: Decoder maximal reserved 12 buffers.&lt;BR /&gt;0:00:01.059323751&amp;nbsp; 1231&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xf39c0 INFO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4lsink.c:1933:mfw_gst_v4lsink_buffer_alloc: MAX_V4L_ALLOW_SIZE_IN_BYTE / frame_buffer_size = max_frames (7340032 / 3133440 = 2)&lt;BR /&gt;0:00:01.059380376&amp;nbsp; 1231&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xf39c0 DEBUG&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4lsink.c:1936:mfw_gst_v4lsink_buffer_alloc: Decoder maximal support 2 buffers.&lt;BR /&gt;0:00:01.059429626&amp;nbsp; 1231&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xf39c0 DEBUG&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4lsink.c:1940:mfw_gst_v4lsink_buffer_alloc: v4l_info-&amp;gt;buffers_required reduced to max_frames = 2&lt;BR /&gt;0:00:01.059703626&amp;nbsp; 1231&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xf39c0 INFO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4l.c:1007:mfw_gst_v4l2_set_fmt: mfw_gst_v4l2_set_fmt()&lt;BR /&gt;0:00:01.059797751&amp;nbsp; 1231&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xf39c0 INFO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4l.c:1137:mfw_gst_v4l2_set_fmt: v4l_info-&amp;gt;buffers_required = 2&lt;BR /&gt;0:00:01.059887126&amp;nbsp; 1231&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xf39c0 INFO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4l.c:942:mfw_gst_v4l2_output_setup: v4l_info-&amp;gt;buffers_required = 2&lt;BR /&gt;0:00:01.059941126&amp;nbsp; 1231&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xf39c0 INFO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4l.c:943:mfw_gst_v4l2_output_setup: MIN_BUFFER_NUM = 5&lt;BR /&gt;0:00:01.059990126&amp;nbsp; 1231&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xf39c0 INFO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4l.c:974:mfw_gst_v4l2_output_setup: v4l_info-&amp;gt;swbuffer_max = 0&lt;BR /&gt;0:00:01.060038751&amp;nbsp; 1231&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xf39c0 ERROR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mfw_v4lsink mfw_gst_v4l.c:1141:mfw_gst_v4l2_set_fmt: Error in mfw_gst_v4lsink_output_setup&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Dec 2011 18:04:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194953#M10274</guid>
      <dc:creator>sidebranch</dc:creator>
      <dc:date>2011-12-16T18:04:52Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194954#M10275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I disable this piece of code, the decoding suddenly works:&lt;/P&gt;&lt;P&gt;if (v4l_info-&amp;gt;buffers_required &amp;gt; max_frames) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; v4l_info-&amp;gt;buffers_required = max_frames;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder why I need this change in my build, as nobody else seems to have this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leon.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Dec 2011 13:31:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194954#M10275</guid>
      <dc:creator>sidebranch</dc:creator>
      <dc:date>2011-12-17T13:31:49Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194955#M10276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You maybe simply comment these sentences to see what happened.&amp;nbsp;&lt;/P&gt;&lt;P&gt;maybe the some macro is not defined, it should defined&amp;nbsp;_MX51&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Dec 2011 15:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194955#M10276</guid>
      <dc:creator>KanHU</dc:creator>
      <dc:date>2011-12-17T15:29:45Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 gstreamer on framebuffer?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194956#M10277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes it seems you are right that _MX51 must be defined. However, the configure user message suggests otherwise:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;configure.ac:251:&amp;nbsp; AC_MSG_ERROR(No target platform specified! Use ./configure PLATFORM=(MX28/MX233/MX25/MX27/MX31/MX35/MX37/MX51/MX53/MX50/MX5X/MX6) to retry)&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;If specifying PLATFORM=MX53 this will define _MX53 as a preprocessor symbol during compilation. However, there is no check for _MX53, only for MX51 and smaller platforms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I think MX53/MX50/MX5X/MX6 will fail (and possible are Freescale internal new developments).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks Kan HU, this fixed my problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Dec 2011 01:56:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-gstreamer-on-framebuffer/m-p/194956#M10277</guid>
      <dc:creator>sidebranch</dc:creator>
      <dc:date>2011-12-18T01:56:51Z</dc:date>
    </item>
  </channel>
</rss>