<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6 adding new display resolutions</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-adding-new-display-resolutions/m-p/667828#M102736</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could you tell me is the HDMI display well on your board? Or you only have VGA monitor?&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Rita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 May 2017 07:57:08 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2017-05-12T07:57:08Z</dc:date>
    <item>
      <title>IMX6 adding new display resolutions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-adding-new-display-resolutions/m-p/667827#M102735</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. I am using a Solid Run Humming Boar Quad (imx6) dev board.&lt;/P&gt;&lt;P&gt;2. I am running the Solid Run officially supported / release of Debian Jessie mate 20170413, Linux kernel 3.14.79-fslc-imx6-sr&lt;/P&gt;&lt;P&gt;3. No additional Hw/SW&lt;/P&gt;&lt;P&gt;4. No changes to HW/SW&lt;/P&gt;&lt;P&gt;5, 6, 7, 8:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to adjust the screen resolution with xrandr to support 1024x768-60&amp;nbsp; resolution&lt;/P&gt;&lt;P&gt;I follow the normal sequence of :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; a. gtf&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; b. xrandr --newmode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; c. xrandr --addmode&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Step c above xrandr complains that the new mode is an invalid option.&lt;/P&gt;&lt;P&gt;The connect device correctly shows up as "DISP3 BG"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried this with an HDMI monitor and a VGA monitor (using an HDMI to VGA dongle).&lt;/P&gt;&lt;P&gt;What is the correct method to change my screen resolution to support the application I will be using this board with?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2017 23:32:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-adding-new-display-resolutions/m-p/667827#M102735</guid>
      <dc:creator>vaheavedissian</dc:creator>
      <dc:date>2017-05-04T23:32:37Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 adding new display resolutions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-adding-new-display-resolutions/m-p/667828#M102736</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could you tell me is the HDMI display well on your board? Or you only have VGA monitor?&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Rita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 May 2017 07:57:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-adding-new-display-resolutions/m-p/667828#M102736</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2017-05-12T07:57:08Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 adding new display resolutions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-adding-new-display-resolutions/m-p/667829#M102737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If the display is well on your board, when the board boot up ,you need to use the cat command to confirm which display resolutions are support. If the 1024x768-60 is support, you can use the echo command to change the display resolutions of the screen.&lt;/P&gt;&lt;H1&gt;&lt;/H1&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 May 2017 08:10:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-adding-new-display-resolutions/m-p/667829#M102737</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2017-05-12T08:10:10Z</dc:date>
    </item>
  </channel>
</rss>