<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックEIM on M4, while using Linux on i.MX7D</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/EIM-on-M4-while-using-Linux-on-i-MX7D/m-p/667769#M102722</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to use the EIM on the Cortex-M4 of a i.MX7D to access an FPGA. Deploying my program to M4 using u-boot without starting Linux on the A7 works perfectly fine. I am already able to use EIM for communication when I manually reconfigure&amp;nbsp; the pins in iomuxc registers to use EIM. &lt;/P&gt;&lt;P&gt;However, when the program is running and I boot Linux on the A7, EIM stops working on the M4 and memory accesses to EIM memory space can take up to five seconds. I already tried to disable EIM on the Linux side changing the device-tree. I also tried to load the program for the M4 directly from Linux considering AN5317, which works fine (if I had a program running on M4 already previously, starting it from u-boot), but as soon as I access EIM memory space, Linux and the M4 freeze.&lt;/P&gt;&lt;P&gt;So, could there still be any conflict with EIM at the M4 running Linux? Can you give me some suggestions how to configure Linux in order to avoid those conflicts or do you have in case some example configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Jul 2017 11:14:29 GMT</pubDate>
    <dc:creator>dominiksteinhau</dc:creator>
    <dc:date>2017-07-13T11:14:29Z</dc:date>
    <item>
      <title>EIM on M4, while using Linux on i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-on-M4-while-using-Linux-on-i-MX7D/m-p/667769#M102722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to use the EIM on the Cortex-M4 of a i.MX7D to access an FPGA. Deploying my program to M4 using u-boot without starting Linux on the A7 works perfectly fine. I am already able to use EIM for communication when I manually reconfigure&amp;nbsp; the pins in iomuxc registers to use EIM. &lt;/P&gt;&lt;P&gt;However, when the program is running and I boot Linux on the A7, EIM stops working on the M4 and memory accesses to EIM memory space can take up to five seconds. I already tried to disable EIM on the Linux side changing the device-tree. I also tried to load the program for the M4 directly from Linux considering AN5317, which works fine (if I had a program running on M4 already previously, starting it from u-boot), but as soon as I access EIM memory space, Linux and the M4 freeze.&lt;/P&gt;&lt;P&gt;So, could there still be any conflict with EIM at the M4 running Linux? Can you give me some suggestions how to configure Linux in order to avoid those conflicts or do you have in case some example configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jul 2017 11:14:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-on-M4-while-using-Linux-on-i-MX7D/m-p/667769#M102722</guid>
      <dc:creator>dominiksteinhau</dc:creator>
      <dc:date>2017-07-13T11:14:29Z</dc:date>
    </item>
    <item>
      <title>Re: EIM on M4, while using Linux on i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-on-M4-while-using-Linux-on-i-MX7D/m-p/667770#M102723</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dominik&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;issue may be caused by linux clock reinitialization during start-up, in such process&lt;BR /&gt;it is necesary to gate some clocks. This is described in sect.1.2.4 PFD restrictions&lt;BR /&gt;EB790 Configuration of Phase Fractional Dividers&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.nxp.com%2Fdocs%2Fen%2Fengineering-bulletin%2FEB790.pdf" rel="nofollow" target="_blank"&gt;http://cache.nxp.com/docs/en/engineering-bulletin/EB790.pdf&lt;/A&gt;&lt;BR /&gt;So EIM can stop working even not using by linux, if its parent clock source&lt;BR /&gt;needs to be used by some other peripheral (used by linux). One can try to debug it&lt;BR /&gt;using AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors&lt;BR /&gt;&lt;A href="http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf"&gt;http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Jul 2017 23:11:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-on-M4-while-using-Linux-on-i-MX7D/m-p/667770#M102723</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-16T23:11:21Z</dc:date>
    </item>
    <item>
      <title>Re: EIM on M4, while using Linux on i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-on-M4-while-using-Linux-on-i-MX7D/m-p/667771#M102724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor, &lt;/P&gt;&lt;P&gt;thank you very much, that was indeed the problem, now it works!&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Dominik&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jul 2017 16:19:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-on-M4-while-using-Linux-on-i-MX7D/m-p/667771#M102724</guid>
      <dc:creator>dominiksteinhau</dc:creator>
      <dc:date>2017-07-20T16:19:01Z</dc:date>
    </item>
    <item>
      <title>Re: EIM on M4, while using Linux on i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-on-M4-while-using-Linux-on-i-MX7D/m-p/667772#M102725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,Dominik&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Could you share your solution ? I have&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;reconfigure&amp;nbsp; the pins in iomuxc registers to use EIM on M4,and also clk.&amp;nbsp;but I don't know how to access the addr of EIM(when in A9,I can use &lt;STRONG&gt;mmap&lt;/STRONG&gt;).&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Dec 2017 08:36:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-on-M4-while-using-Linux-on-i-MX7D/m-p/667772#M102725</guid>
      <dc:creator>jingyangxie</dc:creator>
      <dc:date>2017-12-18T08:36:20Z</dc:date>
    </item>
    <item>
      <title>Re: EIM on M4, while using Linux on i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-on-M4-while-using-Linux-on-i-MX7D/m-p/667773#M102726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know this is a bit offtopic, but could you maybe tell me how you loaded the code to the M4 from Linux?&lt;/P&gt;&lt;P&gt;I am trying to write a script but I am quiet new to loading files to the memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you eventually share your code with me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Aug 2018 13:48:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-on-M4-while-using-Linux-on-i-MX7D/m-p/667773#M102726</guid>
      <dc:creator>erikfriedel</dc:creator>
      <dc:date>2018-08-21T13:48:21Z</dc:date>
    </item>
  </channel>
</rss>