<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックToolchain for i.mx28</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Toolchain-for-i-mx28/m-p/667754#M102720</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to get a build going for i.mx28. &amp;nbsp;I've downreved Ubuntu to 10.10 which allows me to install LTIB, which seems to be required, but I can't get a g++ install for the old version of Ubuntu. &amp;nbsp;If I use a more recent version of Ubuntu, I can't get LTIB installed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's the current toolchain setup I should be using for a linux application for i.mx28?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Jun 2017 20:20:11 GMT</pubDate>
    <dc:creator>tomhanks</dc:creator>
    <dc:date>2017-06-20T20:20:11Z</dc:date>
    <item>
      <title>Toolchain for i.mx28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Toolchain-for-i-mx28/m-p/667754#M102720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to get a build going for i.mx28. &amp;nbsp;I've downreved Ubuntu to 10.10 which allows me to install LTIB, which seems to be required, but I can't get a g++ install for the old version of Ubuntu. &amp;nbsp;If I use a more recent version of Ubuntu, I can't get LTIB installed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's the current toolchain setup I should be using for a linux application for i.mx28?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 20:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Toolchain-for-i-mx28/m-p/667754#M102720</guid>
      <dc:creator>tomhanks</dc:creator>
      <dc:date>2017-06-20T20:20:11Z</dc:date>
    </item>
    <item>
      <title>Re: Toolchain for i.mx28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Toolchain-for-i-mx28/m-p/667755#M102721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for new ubuntu one can look at suggestions provided on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/437371"&gt;imx6q build LTIB problems&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or use some third party yocto releases, like:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.digi.com%2Fsupport%2Fproductdetail%3Fpid%3D5587%26type%3Ddocumentation" rel="nofollow" target="_blank"&gt;http://www.digi.com/support/productdetail?pid=5587&amp;amp;type=documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 23:40:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Toolchain-for-i-mx28/m-p/667755#M102721</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-20T23:40:39Z</dc:date>
    </item>
  </channel>
</rss>