<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 4.9 kernel for imx6slevk in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/4-9-kernel-for-imx6slevk/m-p/667697#M102706</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How to build latest 4.9 kernel for the Imx6slevk board using Freescale yocto project?&lt;/P&gt;&lt;P&gt;Can anyone share the documents?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Susan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 May 2017 13:49:00 GMT</pubDate>
    <dc:creator>susangracerapak</dc:creator>
    <dc:date>2017-05-30T13:49:00Z</dc:date>
    <item>
      <title>4.9 kernel for imx6slevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4-9-kernel-for-imx6slevk/m-p/667697#M102706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How to build latest 4.9 kernel for the Imx6slevk board using Freescale yocto project?&lt;/P&gt;&lt;P&gt;Can anyone share the documents?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Susan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 May 2017 13:49:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4-9-kernel-for-imx6slevk/m-p/667697#M102706</guid>
      <dc:creator>susangracerapak</dc:creator>
      <dc:date>2017-05-30T13:49:00Z</dc:date>
    </item>
    <item>
      <title>Re: 4.9 kernel for imx6slevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4-9-kernel-for-imx6slevk/m-p/667698#M102707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Susangrace Rapaka,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a recipe in place for 4.9 on the latest Community BSP for the Morty branch of the Yocto Project. However, it’s not a complete recipe and as I imagined I couldn’t bake it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I added the following on the conf/local.conf file and tried baking linux-fslc-imx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PREFERRED_VERSION_linux-fslc-imx = "4.9"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I got the following warnings:&lt;/P&gt;&lt;P&gt;NOTE: preferred version 4.9 of linux-fslc-imx not available (for item linux-fslc-imx)&lt;/P&gt;&lt;P&gt;NOTE: versions of linux-fslc-imx available: 4.1-2.0.x+gitAUTOINC+ee67fc7e07&lt;/P&gt;&lt;P&gt;NOTE: Resolving any missing task queue dependencies&lt;/P&gt;&lt;P&gt;NOTE: preferred version 4.9 of linux-fslc-imx not available (for item kernel-base)&lt;/P&gt;&lt;P&gt;NOTE: versions of linux-fslc-imx available: 4.1-2.0.x+gitAUTOINC+ee67fc7e07&lt;/P&gt;&lt;P&gt;NOTE: preferred version 4.9 of linux-fslc-imx not available (for item kernel-image-zimage)&lt;/P&gt;&lt;P&gt;NOTE: versions of linux-fslc-imx available: 4.1-2.0.x+gitAUTOINC+ee67fc7e07&lt;/P&gt;&lt;P&gt;NOTE: preferred version 4.9 of linux-fslc-imx not available (for item kernel-image)&lt;/P&gt;&lt;P&gt;NOTE: versions of linux-fslc-imx available: 4.1-2.0.x+gitAUTOINC+ee67fc7e07&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently the supported kernel for both the BSP release and Community BSP is 4.X (verion varies depending on the BSP). I would recommend using these kernels unless you absolutely need a feature from kernel 4.9 that’s not available on previous versions, in which case you would need to adapt the mainline kernel to work for your MACHINE.&lt;/P&gt;&lt;P&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 May 2017 17:01:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4-9-kernel-for-imx6slevk/m-p/667698#M102707</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-05-30T17:01:47Z</dc:date>
    </item>
    <item>
      <title>Re: 4.9 kernel for imx6slevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4-9-kernel-for-imx6slevk/m-p/667699#M102708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi gusarambula,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your information. I have tried the same earlier but it wasn't working.&lt;/P&gt;&lt;P&gt;I have brought up the latest kernel 4.1 successfully but, I need 4.9 now. Do you have any idea which Machine has the build with 4.9 kernel[Imx platfrom]?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Susan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 May 2017 04:57:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4-9-kernel-for-imx6slevk/m-p/667699#M102708</guid>
      <dc:creator>susangracerapak</dc:creator>
      <dc:date>2017-05-31T04:57:19Z</dc:date>
    </item>
    <item>
      <title>Re: 4.9 kernel for imx6slevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4-9-kernel-for-imx6slevk/m-p/667700#M102709</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Susan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From what I see there are no machines using Kernel 4.9 on the Community BSP, which makes sense as it's too recent. I think you would need to work on the mainline kernel and adapt it for the i.MX family, which would be a lot of work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 May 2017 20:49:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4-9-kernel-for-imx6slevk/m-p/667700#M102709</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-05-31T20:49:25Z</dc:date>
    </item>
    <item>
      <title>Re: 4.9 kernel for imx6slevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4-9-kernel-for-imx6slevk/m-p/667701#M102710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi gusarambula,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the update.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Susan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2017 07:07:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4-9-kernel-for-imx6slevk/m-p/667701#M102710</guid>
      <dc:creator>susangracerapak</dc:creator>
      <dc:date>2017-06-02T07:07:27Z</dc:date>
    </item>
  </channel>
</rss>