<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX7 Use SDMA ROM Script with FTM or GPT</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX7-Use-SDMA-ROM-Script-with-FTM-or-GPT/m-p/666811#M102590</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Running in Linux 4.1.15, we would like to use the SDMA to get input capture value from the FlexTimer (FTM) or General Purpose Timer.&lt;/P&gt;&lt;P&gt;Is it possible using the existing SDMA ROM script ?&amp;nbsp;For example app_2_mcu one ?&lt;/P&gt;&lt;P&gt;Is there an example or a document to explain how to do it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jerome&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 May 2017 15:33:54 GMT</pubDate>
    <dc:creator>jeromemathieu</dc:creator>
    <dc:date>2017-05-04T15:33:54Z</dc:date>
    <item>
      <title>IMX7 Use SDMA ROM Script with FTM or GPT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7-Use-SDMA-ROM-Script-with-FTM-or-GPT/m-p/666811#M102590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Running in Linux 4.1.15, we would like to use the SDMA to get input capture value from the FlexTimer (FTM) or General Purpose Timer.&lt;/P&gt;&lt;P&gt;Is it possible using the existing SDMA ROM script ?&amp;nbsp;For example app_2_mcu one ?&lt;/P&gt;&lt;P&gt;Is there an example or a document to explain how to do it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jerome&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2017 15:33:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7-Use-SDMA-ROM-Script-with-FTM-or-GPT/m-p/666811#M102590</guid>
      <dc:creator>jeromemathieu</dc:creator>
      <dc:date>2017-05-04T15:33:54Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7 Use SDMA ROM Script with FTM or GPT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7-Use-SDMA-ROM-Script-with-FTM-or-GPT/m-p/666812#M102591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jerome&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in general this is possible however current nxp linux does not support that.&lt;/P&gt;&lt;P&gt;One can contact NXP Professional Services to develop it&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fsupport%2Fnxp-professional-services%3APROFESSIONAL-SERVICE" rel="nofollow" target="_blank"&gt;http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2017 23:41:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7-Use-SDMA-ROM-Script-with-FTM-or-GPT/m-p/666812#M102591</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-05-04T23:41:41Z</dc:date>
    </item>
  </channel>
</rss>