<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6ULL CAN Connection</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6ULL-CAN-Connection/m-p/666739#M102585</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Soumya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe you are right, for loop back just connect L-L and H-H of Can0-Can1 respectively.&lt;/P&gt;&lt;P&gt;For test one can use imx-test&lt;BR /&gt;&lt;A href="https://community.nxp.com/www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz" target="test_blank"&gt;www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Jul 2017 08:44:32 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-07-13T08:44:32Z</dc:date>
    <item>
      <title>imx6ULL CAN Connection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ULL-CAN-Connection/m-p/666738#M102584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using imx6.ULL EVK board. There is a CAN connector on the board which has pins for both CAN0(L/H) and CAN1(L/H).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to do a loop back from CAN0 to CAN1. How should I connect these pins? Is it enough if I just wire it up from L-L and H-H of Can0-Can1 respectively? There was a continuity seen in the other pins when I do that.&lt;/P&gt;&lt;P&gt;Is there a cable which can be procured anywhere particularly for this EVK?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any leads will be of atmost help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Soumya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jul 2017 06:58:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ULL-CAN-Connection/m-p/666738#M102584</guid>
      <dc:creator>soumyaks</dc:creator>
      <dc:date>2017-07-13T06:58:12Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ULL CAN Connection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ULL-CAN-Connection/m-p/666739#M102585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Soumya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe you are right, for loop back just connect L-L and H-H of Can0-Can1 respectively.&lt;/P&gt;&lt;P&gt;For test one can use imx-test&lt;BR /&gt;&lt;A href="https://community.nxp.com/www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz" target="test_blank"&gt;www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jul 2017 08:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ULL-CAN-Connection/m-p/666739#M102585</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-13T08:44:32Z</dc:date>
    </item>
  </channel>
</rss>