<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Secure boot log imx7 if boot fails in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Secure-boot-log-imx7-if-boot-fails/m-p/666230#M102513</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Abdallah&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for security boot details one can refer to AN4581 Secure Boot&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/docs/en/application-note/AN4581.pdf" title="http://www.nxp.com/docs/en/application-note/AN4581.pdf"&gt;http://www.nxp.com/docs/en/application-note/AN4581.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;in particular on p.8 it states&lt;/P&gt;&lt;P&gt;"When built with this configuration [secure], U-Boot provides extra functions for HAB, one&lt;/P&gt;&lt;P&gt;of those being access to HAB status logs."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Aug 2017 10:53:32 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-08-04T10:53:32Z</dc:date>
    <item>
      <title>Secure boot log imx7 if boot fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-boot-log-imx7-if-boot-fails/m-p/666229#M102512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Folks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not a secure boot guru but after checking the boot security settings on&amp;nbsp;Security Reference Manual for i.MX 7D. I found the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case of boot mode set to closed;&amp;nbsp;All detected errors are logged, and the boot flow is aborted with the control being passed to the serial downloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I&amp;nbsp;gain access to these log files if the flow is aborted? There is no point of&amp;nbsp;logging if we don't have access to these logs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Aug 2017 10:35:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-boot-log-imx7-if-boot-fails/m-p/666229#M102512</guid>
      <dc:creator>agalal</dc:creator>
      <dc:date>2017-08-04T10:35:04Z</dc:date>
    </item>
    <item>
      <title>Re: Secure boot log imx7 if boot fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-boot-log-imx7-if-boot-fails/m-p/666230#M102513</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Abdallah&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for security boot details one can refer to AN4581 Secure Boot&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/docs/en/application-note/AN4581.pdf" title="http://www.nxp.com/docs/en/application-note/AN4581.pdf"&gt;http://www.nxp.com/docs/en/application-note/AN4581.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;in particular on p.8 it states&lt;/P&gt;&lt;P&gt;"When built with this configuration [secure], U-Boot provides extra functions for HAB, one&lt;/P&gt;&lt;P&gt;of those being access to HAB status logs."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Aug 2017 10:53:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-boot-log-imx7-if-boot-fails/m-p/666230#M102513</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-08-04T10:53:32Z</dc:date>
    </item>
    <item>
      <title>Re: Secure boot log imx7 if boot fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-boot-log-imx7-if-boot-fails/m-p/666231#M102514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; You can create request / ticket to get more details about Secure boot (under NDA).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu" title="http://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu"&gt;Support|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Aug 2017 06:17:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-boot-log-imx7-if-boot-fails/m-p/666231#M102514</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-08-07T06:17:20Z</dc:date>
    </item>
  </channel>
</rss>