<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Can we use SDIO interface [not USB]Wifi Card for Android ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-we-use-SDIO-interface-not-USB-Wifi-Card-for-Android/m-p/666172#M102500</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; We are not using BCM Driver. But Generally if we insert the SDIO Card it should get detected by kernel. But here SDIO Card is detected and immediately card removed.&lt;/P&gt;&lt;P&gt;================================================================================================&lt;/P&gt;&lt;P&gt;LOG:&lt;/P&gt;&lt;P&gt;================================================================================================&lt;/P&gt;&lt;P&gt;8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;Key type dns_resolver registered&lt;BR /&gt;dhd_module_init in&lt;BR /&gt;Power-up adapter 'DHD generic adapter'&lt;BR /&gt;wifi_platform_bus_enumerate device present 1&lt;BR /&gt;&lt;STRONG&gt;mmc1: new high speed SDIO card at address fffd&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;failed to power up DHD generic adapter, 3 retry left&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;wifi_platform_bus_enumerate device present 0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;mmc1: card fffd removed&lt;/STRONG&gt;&lt;BR /&gt;wifi_platform_bus_enumerate device present 1&lt;BR /&gt;&lt;STRONG&gt;mmc1: new high speed SDIO card at address fffd&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;failed to power up DHD generic adapter, 2 retry left&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;wifi_platform_bus_enumerate device present 0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;mmc1: card fffd removed&lt;/STRONG&gt;&lt;BR /&gt;wifi_platform_bus_enumerate device present 1&lt;BR /&gt;&lt;STRONG&gt;mmc1: new high speed SDIO card at address fffd&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;failed to power up DHD generic adapter, 1 retry left&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;wifi_platform_bus_enumerate device present 0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;mmc1: card fffd removed&lt;/STRONG&gt;&lt;BR /&gt;wifi_platform_bus_enumerate device present 1&lt;BR /&gt;&lt;STRONG&gt;mmc1: new high speed SDIO card at address fffd&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;failed to power up DHD generic adapter, 0 retry left&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;wifi_platform_bus_enumerate device present 0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;mmc1: card fffd removed&lt;/STRONG&gt;&lt;BR /&gt;failed to power up DHD generic adapter, max retry reached**&lt;BR /&gt;input: gpio-keys as /devices/soc0/gpio-keys/input/input12&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;=========================================================================================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anything we need to enable from host controller side or in kernel menuconfig ?&lt;/P&gt;&lt;P&gt;Please suggest idea to fix this..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Thanaraj.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 May 2017 07:26:49 GMT</pubDate>
    <dc:creator>ThanarajS</dc:creator>
    <dc:date>2017-05-29T07:26:49Z</dc:date>
    <item>
      <title>Can we use SDIO interface [not USB]Wifi Card for Android ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-we-use-SDIO-interface-not-USB-Wifi-Card-for-Android/m-p/666170#M102498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; We have SDIO Interface supported wifi card, Can we use that module for android driver porting ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; We tried but wifi card is not detecting in Android Kernel.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Please help me to use SDIO Interface based Wi-Fi Card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Thanaraj.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 May 2017 04:33:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-we-use-SDIO-interface-not-USB-Wifi-Card-for-Android/m-p/666170#M102498</guid>
      <dc:creator>ThanarajS</dc:creator>
      <dc:date>2017-05-29T04:33:22Z</dc:date>
    </item>
    <item>
      <title>Re: Can we use SDIO interface [not USB]Wifi Card for Android ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-we-use-SDIO-interface-not-USB-Wifi-Card-for-Android/m-p/666171#M102499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thanaraj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes it can be used, please refer to attached Linux Manual&lt;/P&gt;&lt;P&gt;Chapter 46 Wi-Fi BCM4339 Driver, the same is for Android as&lt;/P&gt;&lt;P&gt;described in Release Notes Table 2. Features. Usually porting&lt;/P&gt;&lt;P&gt;guidelines are provided by chip vendor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 May 2017 05:09:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-we-use-SDIO-interface-not-USB-Wifi-Card-for-Android/m-p/666171#M102499</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-05-29T05:09:07Z</dc:date>
    </item>
    <item>
      <title>Re: Can we use SDIO interface [not USB]Wifi Card for Android ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-we-use-SDIO-interface-not-USB-Wifi-Card-for-Android/m-p/666172#M102500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; We are not using BCM Driver. But Generally if we insert the SDIO Card it should get detected by kernel. But here SDIO Card is detected and immediately card removed.&lt;/P&gt;&lt;P&gt;================================================================================================&lt;/P&gt;&lt;P&gt;LOG:&lt;/P&gt;&lt;P&gt;================================================================================================&lt;/P&gt;&lt;P&gt;8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;Key type dns_resolver registered&lt;BR /&gt;dhd_module_init in&lt;BR /&gt;Power-up adapter 'DHD generic adapter'&lt;BR /&gt;wifi_platform_bus_enumerate device present 1&lt;BR /&gt;&lt;STRONG&gt;mmc1: new high speed SDIO card at address fffd&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;failed to power up DHD generic adapter, 3 retry left&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;wifi_platform_bus_enumerate device present 0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;mmc1: card fffd removed&lt;/STRONG&gt;&lt;BR /&gt;wifi_platform_bus_enumerate device present 1&lt;BR /&gt;&lt;STRONG&gt;mmc1: new high speed SDIO card at address fffd&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;failed to power up DHD generic adapter, 2 retry left&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;wifi_platform_bus_enumerate device present 0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;mmc1: card fffd removed&lt;/STRONG&gt;&lt;BR /&gt;wifi_platform_bus_enumerate device present 1&lt;BR /&gt;&lt;STRONG&gt;mmc1: new high speed SDIO card at address fffd&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;failed to power up DHD generic adapter, 1 retry left&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;wifi_platform_bus_enumerate device present 0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;mmc1: card fffd removed&lt;/STRONG&gt;&lt;BR /&gt;wifi_platform_bus_enumerate device present 1&lt;BR /&gt;&lt;STRONG&gt;mmc1: new high speed SDIO card at address fffd&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;failed to power up DHD generic adapter, 0 retry left&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;wifi_platform_bus_enumerate device present 0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;mmc1: card fffd removed&lt;/STRONG&gt;&lt;BR /&gt;failed to power up DHD generic adapter, max retry reached**&lt;BR /&gt;input: gpio-keys as /devices/soc0/gpio-keys/input/input12&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;=========================================================================================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anything we need to enable from host controller side or in kernel menuconfig ?&lt;/P&gt;&lt;P&gt;Please suggest idea to fix this..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Thanaraj.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 May 2017 07:26:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-we-use-SDIO-interface-not-USB-Wifi-Card-for-Android/m-p/666172#M102500</guid>
      <dc:creator>ThanarajS</dc:creator>
      <dc:date>2017-05-29T07:26:49Z</dc:date>
    </item>
  </channel>
</rss>