<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How VBS scripts is used in MFGtool in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-VBS-scripts-is-used-in-MFGtool/m-p/666015#M102479</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aditya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at ucl2.xml file and use for example mfgtool2-yocto-mx-sabresd-nand.vbs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;CMD state="BootStrap" type="load" file="firmware/zImage-imx6q%plus%-%board%-%nanddtb%.dtb" address="0x18000000"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;parameters in "" are taken from *.vbs file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-s ""board=sabreauto"" -s ""sxuboot=sabreauto"" -s ""sxdtb=sabreauto"" -s ""nand=nand"" -s ""nanddtb=gpmi-weim"" -s ""part_uboot=0"" -s ""part_kernel=1"" -s ""part_dtb=2"" -s ""part_rootfs=3""&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Jun 2017 11:14:14 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-06-20T11:14:14Z</dc:date>
    <item>
      <title>How VBS scripts is used in MFGtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-VBS-scripts-is-used-in-MFGtool/m-p/666014#M102478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I am using MFGTool for flashing the NAND Flash over my custom board . I want to know how VBS script is used in the MFGtool. I believe , this script is having certain arguments , but how these arguments are processed in MFGtool , I have no clue. Please suggest.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aditya Nagal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 07:55:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-VBS-scripts-is-used-in-MFGtool/m-p/666014#M102478</guid>
      <dc:creator>adityanagal</dc:creator>
      <dc:date>2017-06-20T07:55:20Z</dc:date>
    </item>
    <item>
      <title>Re: How VBS scripts is used in MFGtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-VBS-scripts-is-used-in-MFGtool/m-p/666015#M102479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aditya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at ucl2.xml file and use for example mfgtool2-yocto-mx-sabresd-nand.vbs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;CMD state="BootStrap" type="load" file="firmware/zImage-imx6q%plus%-%board%-%nanddtb%.dtb" address="0x18000000"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;parameters in "" are taken from *.vbs file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-s ""board=sabreauto"" -s ""sxuboot=sabreauto"" -s ""sxdtb=sabreauto"" -s ""nand=nand"" -s ""nanddtb=gpmi-weim"" -s ""part_uboot=0"" -s ""part_kernel=1"" -s ""part_dtb=2"" -s ""part_rootfs=3""&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 11:14:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-VBS-scripts-is-used-in-MFGtool/m-p/666015#M102479</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-20T11:14:14Z</dc:date>
    </item>
    <item>
      <title>Re: How VBS scripts is used in MFGtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-VBS-scripts-is-used-in-MFGtool/m-p/666016#M102480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor , &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your response. One confusion is , in the MFGtool we have many VBS scripts , I want to use a particular VBS script for example the mfgtool2-yocto-mx-sabresd-nand.vbs . How to pass this mfgtool2-yocto-mx-sabresd-nand.vbs as input to the MFGtool ? Please suggest.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 11:45:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-VBS-scripts-is-used-in-MFGtool/m-p/666016#M102480</guid>
      <dc:creator>adityanagal</dc:creator>
      <dc:date>2017-06-20T11:45:04Z</dc:date>
    </item>
    <item>
      <title>Re: How VBS scripts is used in MFGtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-VBS-scripts-is-used-in-MFGtool/m-p/666017#M102481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aditya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;just click mouse on vbs script and it will launch mfg tools with all necessary parameters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 12:42:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-VBS-scripts-is-used-in-MFGtool/m-p/666017#M102481</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-20T12:42:56Z</dc:date>
    </item>
  </channel>
</rss>