<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Gen2wbfParser can't work for imx6sl</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Gen2wbfParser-can-t-work-for-imx6sl/m-p/665969#M102464</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As per the i.MX6SoloLite Reference Manual document, its EPD Controller hardware itself supports the 5-bit pixel format. However, the current framebuffer driver seems to be supporting only 4-bit format. So, only 4-bit EP displays can be supported in Linux at present.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 May 2017 09:56:46 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2017-05-30T09:56:46Z</dc:date>
    <item>
      <title>Gen2wbfParser can't work for imx6sl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gen2wbfParser-can-t-work-for-imx6sl/m-p/665968#M102463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a Gen2wbfParser tool,which &amp;nbsp;convert waveform from *.wbf to *.fw .&lt;/P&gt;&lt;P&gt;I convert a *.fw for imx6sl use the command as follow:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Gen2wbfParser -o imx6sl.fw mywbf.wbf &amp;nbsp; //mywbf.wbf is 5bit format&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;but&amp;nbsp;&lt;EM&gt;imx6sl.fw&lt;/EM&gt;&amp;nbsp;can't work well, the epdc_E060SCM.fw(old format 4bit) can work,&lt;/P&gt;&lt;P&gt;Is the convert tool Incorrect ?&lt;/P&gt;&lt;P&gt;or the my sourecode for imx6sl waveform set is wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks &amp;amp; best regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 27 May 2017 03:22:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gen2wbfParser-can-t-work-for-imx6sl/m-p/665968#M102463</guid>
      <dc:creator>yan2anfei</dc:creator>
      <dc:date>2017-05-27T03:22:06Z</dc:date>
    </item>
    <item>
      <title>Re: Gen2wbfParser can't work for imx6sl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gen2wbfParser-can-t-work-for-imx6sl/m-p/665969#M102464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As per the i.MX6SoloLite Reference Manual document, its EPD Controller hardware itself supports the 5-bit pixel format. However, the current framebuffer driver seems to be supporting only 4-bit format. So, only 4-bit EP displays can be supported in Linux at present.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 May 2017 09:56:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gen2wbfParser-can-t-work-for-imx6sl/m-p/665969#M102464</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-05-30T09:56:46Z</dc:date>
    </item>
    <item>
      <title>Re: Gen2wbfParser can't work for imx6sl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gen2wbfParser-can-t-work-for-imx6sl/m-p/665970#M102465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi Artur,&lt;/P&gt;&lt;P&gt;imx7d can supported the 5-bit &amp;nbsp;EP displays, &amp;nbsp;Is the framebuffer driver &amp;nbsp;different with imx6sl?&lt;/P&gt;&lt;P&gt;Is it possible port&amp;nbsp;&lt;SPAN&gt;imx7d framebuffer&amp;nbsp;&lt;/SPAN&gt;to imx6sl ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks ！&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 May 2017 15:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gen2wbfParser-can-t-work-for-imx6sl/m-p/665970#M102465</guid>
      <dc:creator>yan2anfei</dc:creator>
      <dc:date>2017-05-30T15:10:02Z</dc:date>
    </item>
  </channel>
</rss>