<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: GPIO set value and get value</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GPIO-set-value-and-get-value/m-p/665624#M102384</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which board and which version BSP are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Aug 2017 07:46:37 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2017-08-04T07:46:37Z</dc:date>
    <item>
      <title>GPIO set value and get value</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPIO-set-value-and-get-value/m-p/665623#M102383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp; I'm &lt;SPAN style="font-size: 11.0pt;"&gt;confused for the gpio control. Here is my step:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; 1: &amp;nbsp;&amp;nbsp; int pin_num = of_get_named_gpio(np, "345-en,fsl", 0);&amp;nbsp;&amp;nbsp; //GPIO2 IO03&amp;nbsp; pin_num = 35;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; 2:&amp;nbsp;&amp;nbsp;&amp;nbsp; gpio_direction_output(pin_num, 1);&amp;nbsp;&amp;nbsp; //Voltage high&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 3: &amp;nbsp;&amp;nbsp; gpiod_get_value(gpio_to_desc(pin_num));&amp;nbsp;&amp;nbsp; //get "0"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; 4:&amp;nbsp;&amp;nbsp;&amp;nbsp; gpiod_set_value(gpio_to_desc(pin_num),0);&amp;nbsp;&amp;nbsp; //voltage low&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; 5: &amp;nbsp;&amp;nbsp; gpiod_get_value(gpio_to_desc(pin_num));&amp;nbsp; //get "0"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; 6: &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;gpiod_set_value(gpio_to_desc(pin_num),1);&amp;nbsp; //voltage high&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; 7: &amp;nbsp; gpiod_get_value(gpio_to_desc(pin_num)); //get "0"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Every time I get the gpio value is &lt;SPAN&gt;"0"&lt;/SPAN&gt;&lt;/SPAN&gt;, &amp;nbsp;but the pin voltage is the same(high/low) what I set.&amp;nbsp; how can i get the GPIO value after i set.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Aug 2017 06:54:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPIO-set-value-and-get-value/m-p/665623#M102383</guid>
      <dc:creator>cilymo</dc:creator>
      <dc:date>2017-08-04T06:54:24Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO set value and get value</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPIO-set-value-and-get-value/m-p/665624#M102384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which board and which version BSP are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Aug 2017 07:46:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPIO-set-value-and-get-value/m-p/665624#M102384</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2017-08-04T07:46:37Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO set value and get value</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPIO-set-value-and-get-value/m-p/665625#M102385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I use imx6dl, and BSP version is 4.1.15_2.0.1.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Aug 2017 07:49:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPIO-set-value-and-get-value/m-p/665625#M102385</guid>
      <dc:creator>cilymo</dc:creator>
      <dc:date>2017-08-04T07:49:46Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO set value and get value</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPIO-set-value-and-get-value/m-p/665626#M102386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The GPIO module provides general-purpose pins that can be configured as either inputs&lt;BR /&gt;or outputs.&lt;BR /&gt;When configured as an output, the pin state (high or low) can be controlled by writing to&lt;BR /&gt;an internal register. When configured as an input, the pin input state can be read from an&lt;BR /&gt;internal register.&lt;/P&gt;&lt;P&gt;If a pin is configured as GPIO by the IOMUX, the state of the pin should also be set since&lt;BR /&gt;it is not initialized by a dedicated hardware module. Setting the pad pull-up, pull-down,&lt;BR /&gt;slew rate and so on, with the pad control function may be required as well.&lt;BR /&gt;Detail you can refer to the i.MX_Linux_Reference_Manual.pdf,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Aug 2017 08:29:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPIO-set-value-and-get-value/m-p/665626#M102386</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2017-08-04T08:29:19Z</dc:date>
    </item>
  </channel>
</rss>