<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックQuestions about eLCDIF register of i.MX7D</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Questions-about-eLCDIF-register-of-i-MX7D/m-p/664872#M102191</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have several questions about eLCDIF register of i.MX7D.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q1. Question about DATA_SELECT field of eLCDIF General Control Register in P3657.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1-1&lt;/P&gt;&lt;P&gt;I read section 13.2 but can't understand a difference of "Command mode" and "Data mode".&lt;BR /&gt;Is there any description for it ?&lt;BR /&gt;Could you explain the "Command mode" and "Data mode" ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1-2&lt;/P&gt;&lt;P&gt;There are following description.&lt;/P&gt;&lt;P&gt;""Command Mode. DCn signal is Low""&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, there are no description about "DCn".&lt;BR /&gt;What is DCn signal ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2. Question about MASTER field of eLCDIF General Control Register in P3658.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2-1&lt;/P&gt;&lt;P&gt;My understanding is as below. Am I correct ?&lt;/P&gt;&lt;P&gt;In MPU i8080 mode, user set MASTER field to "1" when Write.&lt;BR /&gt;In MPU i8080 mode, user set MASTER field to "0" when Read.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;2-2&lt;/P&gt;&lt;P&gt;Does the "PIO mode" mean "program I/O mode" ?&lt;/P&gt;&lt;P&gt;If above understanding is uncorrect, please explain the meaning and function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q3. Question about OUTSTANDING_REQS field of eLCDIF General Control2 Register in P3662.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1&lt;/P&gt;&lt;P&gt;Let me confirm the meaning of "Number of outstanding transaction".&lt;/P&gt;&lt;P&gt;The meaning of "Number of outstanding transaction" is that how many untransmitted data can be held of the transmission data in Master mode (default is 2 data) ? &lt;BR /&gt;Is it like an internal buffer?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ko-hey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Feb 2017 02:18:48 GMT</pubDate>
    <dc:creator>ko-hey</dc:creator>
    <dc:date>2017-02-03T02:18:48Z</dc:date>
    <item>
      <title>Questions about eLCDIF register of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Questions-about-eLCDIF-register-of-i-MX7D/m-p/664872#M102191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have several questions about eLCDIF register of i.MX7D.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q1. Question about DATA_SELECT field of eLCDIF General Control Register in P3657.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1-1&lt;/P&gt;&lt;P&gt;I read section 13.2 but can't understand a difference of "Command mode" and "Data mode".&lt;BR /&gt;Is there any description for it ?&lt;BR /&gt;Could you explain the "Command mode" and "Data mode" ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1-2&lt;/P&gt;&lt;P&gt;There are following description.&lt;/P&gt;&lt;P&gt;""Command Mode. DCn signal is Low""&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, there are no description about "DCn".&lt;BR /&gt;What is DCn signal ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2. Question about MASTER field of eLCDIF General Control Register in P3658.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2-1&lt;/P&gt;&lt;P&gt;My understanding is as below. Am I correct ?&lt;/P&gt;&lt;P&gt;In MPU i8080 mode, user set MASTER field to "1" when Write.&lt;BR /&gt;In MPU i8080 mode, user set MASTER field to "0" when Read.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;2-2&lt;/P&gt;&lt;P&gt;Does the "PIO mode" mean "program I/O mode" ?&lt;/P&gt;&lt;P&gt;If above understanding is uncorrect, please explain the meaning and function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q3. Question about OUTSTANDING_REQS field of eLCDIF General Control2 Register in P3662.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1&lt;/P&gt;&lt;P&gt;Let me confirm the meaning of "Number of outstanding transaction".&lt;/P&gt;&lt;P&gt;The meaning of "Number of outstanding transaction" is that how many untransmitted data can be held of the transmission data in Master mode (default is 2 data) ? &lt;BR /&gt;Is it like an internal buffer?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ko-hey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 02:18:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Questions-about-eLCDIF-register-of-i-MX7D/m-p/664872#M102191</guid>
      <dc:creator>ko-hey</dc:creator>
      <dc:date>2017-02-03T02:18:48Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about eLCDIF register of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Questions-about-eLCDIF-register-of-i-MX7D/m-p/664873#M102192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ko-hey&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q1.&amp;nbsp; DCn signal is LCD_RS, selects between command and data mode of mpu lcd interface.&lt;BR /&gt;Description of "Command mode" and "Data mode" can be found in LCD datasheets.&lt;BR /&gt;From sect.13.2.4.6 MPU Interface&amp;nbsp; i.MX7D&amp;nbsp; RM:&lt;BR /&gt;"LCD_RS signal is typically used to switch between command and data modes."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;2-1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;right&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;2-2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;right&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q3. &amp;gt;The meaning of "Number of outstanding transaction" is that how many untransmitted &lt;BR /&gt;data can be held of the transmission data in Master mode (default is 2 data) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this is right understanding, note "outstanding transaction" may refer not only to data but also commands.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Is it like an internal buffer?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 05:53:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Questions-about-eLCDIF-register-of-i-MX7D/m-p/664873#M102192</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-06T05:53:39Z</dc:date>
    </item>
  </channel>
</rss>