<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx6 DDR3 test in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-DDR3-test/m-p/664835#M102180</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found out there is "mtest" command in u-boot, which can do the basic memory test as expected. Kind of solved my problem!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Feb 2017 19:42:52 GMT</pubDate>
    <dc:creator>yzhang</dc:creator>
    <dc:date>2017-02-03T19:42:52Z</dc:date>
    <item>
      <title>imx6 DDR3 test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-DDR3-test/m-p/664834#M102179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am new to imx6 and linux as well. As I am trying to test the hardware connection between DDR3 and imx6, I need to run a basic functional test program. But I have no idea of where to start from. I wonder if there is any example test code that helps. Any advice or help is welcome. Really appreciate it. The schematic is shown below for your reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Feb 2017 20:23:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-DDR3-test/m-p/664834#M102179</guid>
      <dc:creator>yzhang</dc:creator>
      <dc:date>2017-02-02T20:23:18Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 DDR3 test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-DDR3-test/m-p/664835#M102180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found out there is "mtest" command in u-boot, which can do the basic memory test as expected. Kind of solved my problem!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 19:42:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-DDR3-test/m-p/664835#M102180</guid>
      <dc:creator>yzhang</dc:creator>
      <dc:date>2017-02-03T19:42:52Z</dc:date>
    </item>
  </channel>
</rss>