<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem testing modifs in yocto in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problem-testing-modifs-in-yocto/m-p/664726#M102150</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am facing a problem modifying and testing for remapping my debug uart, so I am modifying .config, device tree and u-boot include files, below the location of files modified:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/home/aaron/fsl-arm-yocto-bsp_2/build-x11/tmp/work/imx6dqscm_1gb_qwks-poky-linux-gnueabi/linux-imx/3.14.52-r0/build/.config&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/home/aaron/fsl-arm-yocto-bsp_2/build-x11/tmp/work/imx6dqscm_1gb_qwks-poky-linux-gnueabi/u-boot-imx/2015.04-r0/git/include/configs/mx6dqscmqwks.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/home/aaron/fsl-arm-yocto-bsp_2/build-x11/tmp/work-shared/imx6dqscm-1gb-qwks/kernel-source/arch/arm/boot/dts/imx6dqscm-1gb-qwks-rev2-fix-ldo.dts&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Buy the problem is at compilation time, if I run a&amp;nbsp; bitbake image compilation like:&lt;/P&gt;&lt;P&gt;bitbake core-image-minimal or bitbake -f core-image-base&lt;/P&gt;&lt;P&gt;Nothing changes in the deploy folder, then if I run a forced clean compilation&lt;/P&gt;&lt;P&gt;bitbake -c clean core-image-base&lt;/P&gt;&lt;P&gt;bitbake -f core-image-base&lt;/P&gt;&lt;P&gt;the generated .sdcard file is updated but I think that my modifications are not compiled&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I modify something in the source/somelayer/conf... the bitbake image ovverrides my modifications&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried too with the fsl-image-qt5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, what is the correct procedure to modify some things like uboot, device tree, kernel config in the build folder and then force a compilation without update the files from the source?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Aaron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Feb 2017 22:09:16 GMT</pubDate>
    <dc:creator>aaronpadilla</dc:creator>
    <dc:date>2017-02-02T22:09:16Z</dc:date>
    <item>
      <title>Problem testing modifs in yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-testing-modifs-in-yocto/m-p/664726#M102150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am facing a problem modifying and testing for remapping my debug uart, so I am modifying .config, device tree and u-boot include files, below the location of files modified:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/home/aaron/fsl-arm-yocto-bsp_2/build-x11/tmp/work/imx6dqscm_1gb_qwks-poky-linux-gnueabi/linux-imx/3.14.52-r0/build/.config&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/home/aaron/fsl-arm-yocto-bsp_2/build-x11/tmp/work/imx6dqscm_1gb_qwks-poky-linux-gnueabi/u-boot-imx/2015.04-r0/git/include/configs/mx6dqscmqwks.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/home/aaron/fsl-arm-yocto-bsp_2/build-x11/tmp/work-shared/imx6dqscm-1gb-qwks/kernel-source/arch/arm/boot/dts/imx6dqscm-1gb-qwks-rev2-fix-ldo.dts&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Buy the problem is at compilation time, if I run a&amp;nbsp; bitbake image compilation like:&lt;/P&gt;&lt;P&gt;bitbake core-image-minimal or bitbake -f core-image-base&lt;/P&gt;&lt;P&gt;Nothing changes in the deploy folder, then if I run a forced clean compilation&lt;/P&gt;&lt;P&gt;bitbake -c clean core-image-base&lt;/P&gt;&lt;P&gt;bitbake -f core-image-base&lt;/P&gt;&lt;P&gt;the generated .sdcard file is updated but I think that my modifications are not compiled&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I modify something in the source/somelayer/conf... the bitbake image ovverrides my modifications&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried too with the fsl-image-qt5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, what is the correct procedure to modify some things like uboot, device tree, kernel config in the build folder and then force a compilation without update the files from the source?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Aaron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Feb 2017 22:09:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-testing-modifs-in-yocto/m-p/664726#M102150</guid>
      <dc:creator>aaronpadilla</dc:creator>
      <dc:date>2017-02-02T22:09:16Z</dc:date>
    </item>
    <item>
      <title>Re: Problem testing modifs in yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-testing-modifs-in-yocto/m-p/664727#M102151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can compile the kernel only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your reference.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94953"&gt;Useful bitbake commands&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95045"&gt;https://community.nxp.com/docs/DOC-95045&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Feb 2017 09:25:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-testing-modifs-in-yocto/m-p/664727#M102151</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2017-02-04T09:25:57Z</dc:date>
    </item>
  </channel>
</rss>