<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Does MX6ULL support Serial/SPI NAND?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Does-MX6ULL-support-Serial-SPI-NAND/m-p/664589#M102130</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Scott&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;supported serial memory devices, such as EEPROM and serial flash, using the SPI,&lt;/P&gt;&lt;P&gt;Serial/SPI NAND not supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Feb 2017 23:40:37 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-02-02T23:40:37Z</dc:date>
    <item>
      <title>Does MX6ULL support Serial/SPI NAND?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-MX6ULL-support-Serial-SPI-NAND/m-p/664588#M102129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Serial/SPI NAND Flash offers advantages for lower memory densities, but it's not clear in the datasheet if it supports Serial/SPI NAND?&amp;nbsp; eMMC is supported and desirable because of the error management built inside.&amp;nbsp; Since Serial/SPI NAND can be used reliably in systems that provide bad-block management and error-correction algorithms, it looks like I have to this management in the i.MX6ULL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the MX6ULL support Serial/SPI NAND with 8-bit ECC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Feb 2017 19:41:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-MX6ULL-support-Serial-SPI-NAND/m-p/664588#M102129</guid>
      <dc:creator>ScottKerstein</dc:creator>
      <dc:date>2017-02-02T19:41:57Z</dc:date>
    </item>
    <item>
      <title>Re: Does MX6ULL support Serial/SPI NAND?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-MX6ULL-support-Serial-SPI-NAND/m-p/664589#M102130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Scott&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;supported serial memory devices, such as EEPROM and serial flash, using the SPI,&lt;/P&gt;&lt;P&gt;Serial/SPI NAND not supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Feb 2017 23:40:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-MX6ULL-support-Serial-SPI-NAND/m-p/664589#M102130</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-02T23:40:37Z</dc:date>
    </item>
  </channel>
</rss>