<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Loading Yocto(3.10.17) To eMMC for iMX6SL based custom board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Loading-Yocto-3-10-17-To-eMMC-for-iMX6SL-based-custom-board/m-p/663998#M101995</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hai all,&lt;/P&gt;&lt;P&gt;we designed a custom board same as iMX6SLEVK board .it has both sdcard and eMMC boot selection and flashed images of&amp;nbsp; Android4.4.2 to&amp;nbsp; eMMC &amp;amp; sdcard successfully.&lt;/P&gt;&lt;P&gt;Then we tried Yocto(3.10.17) core-minimal-images and successfully flashed&amp;nbsp; to the sdcard but unable to flash to eMMC.&lt;/P&gt;&lt;P&gt;Now inorder to flash yocto images to eMMC what are the changes we have to do in the kernel and uboot level.&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;D.jansirani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Sep 2016 08:46:31 GMT</pubDate>
    <dc:creator>jansirani</dc:creator>
    <dc:date>2016-09-30T08:46:31Z</dc:date>
    <item>
      <title>Loading Yocto(3.10.17) To eMMC for iMX6SL based custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Loading-Yocto-3-10-17-To-eMMC-for-iMX6SL-based-custom-board/m-p/663998#M101995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hai all,&lt;/P&gt;&lt;P&gt;we designed a custom board same as iMX6SLEVK board .it has both sdcard and eMMC boot selection and flashed images of&amp;nbsp; Android4.4.2 to&amp;nbsp; eMMC &amp;amp; sdcard successfully.&lt;/P&gt;&lt;P&gt;Then we tried Yocto(3.10.17) core-minimal-images and successfully flashed&amp;nbsp; to the sdcard but unable to flash to eMMC.&lt;/P&gt;&lt;P&gt;Now inorder to flash yocto images to eMMC what are the changes we have to do in the kernel and uboot level.&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;D.jansirani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Sep 2016 08:46:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Loading-Yocto-3-10-17-To-eMMC-for-iMX6SL-based-custom-board/m-p/663998#M101995</guid>
      <dc:creator>jansirani</dc:creator>
      <dc:date>2016-09-30T08:46:31Z</dc:date>
    </item>
    <item>
      <title>Re: Loading Yocto(3.10.17) To eMMC for iMX6SL based custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Loading-Yocto-3-10-17-To-eMMC-for-iMX6SL-based-custom-board/m-p/663999#M101996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jansi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can use Mfg Tools for eMMC programming&lt;/P&gt;&lt;P&gt;i.MX 6Family Manufacturing Toolkit for L3.10.17 (REV L3.10.17_1.0.0) &lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX_6_MFG_L3.10.17_1.0.0_TOOL&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337695836026701499367&amp;amp;Parent_pageType=product"&gt;https://www.nxp.com/webapp/Download?colCode=IMX_6_MFG_L3.10.17_1.0.0_TOOL&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337695836026701499367&amp;amp;Parent_pageType=product&lt;/A&gt;&lt;/P&gt;&lt;P&gt;or erase partitions as suggested on&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/435725"&gt;https://community.nxp.com/thread/435725&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Sep 2016 09:41:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Loading-Yocto-3-10-17-To-eMMC-for-iMX6SL-based-custom-board/m-p/663999#M101996</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-09-30T09:41:03Z</dc:date>
    </item>
    <item>
      <title>Re: Loading Yocto(3.10.17) To eMMC for iMX6SL based custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Loading-Yocto-3-10-17-To-eMMC-for-iMX6SL-based-custom-board/m-p/664000#M101997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the quick reply.&lt;/P&gt;&lt;P&gt;we are already using i.MX 6Family Manufacturing Toolkit for L3.10.17 (REV L3.10.17_1.0.0)&amp;nbsp; to flash yocto images to the sdcard without any problem.&lt;/P&gt;&lt;P&gt;As the yocto default source code for iMX6SL&amp;nbsp; compiles images for&amp;nbsp; sdcard .&lt;/P&gt;&lt;P&gt;now we want to know what are the changes we have to do in kernel and uboot source code inorder to compile images (rootfs+uImage+uboot) to flash to eMMC Flash?&lt;/P&gt;&lt;P&gt;Note :&lt;/P&gt;&lt;P&gt;just to update i.MX 6Family Manufacturing Toolkit for L3.10.17 (REV L3.10.17_1.0.0) downloaded one will have the Mfgfirmware images&amp;nbsp; for sdcard so we have to compile the uboot and uImage for the Mfg firmware also inorder to flash to eMMC.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Sep 2016 12:57:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Loading-Yocto-3-10-17-To-eMMC-for-iMX6SL-based-custom-board/m-p/664000#M101997</guid>
      <dc:creator>jansirani</dc:creator>
      <dc:date>2016-09-30T12:57:45Z</dc:date>
    </item>
    <item>
      <title>Re: Loading Yocto(3.10.17) To eMMC for iMX6SL based custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Loading-Yocto-3-10-17-To-eMMC-for-iMX6SL-based-custom-board/m-p/664001#M101998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;as there is no script for i.MX6SL EVK for eMMC one can create&lt;BR /&gt;it using mfgtool2-mx6-sabresd-yocto-emmc.vbs as example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Oct 2016 00:16:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Loading-Yocto-3-10-17-To-eMMC-for-iMX6SL-based-custom-board/m-p/664001#M101998</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-01T00:16:57Z</dc:date>
    </item>
  </channel>
</rss>